Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents New Raspberry Pi Zero 2 W - 5 x Faster!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14phil
  • Date Created: 20 Oct 2021 2:50 PM Date Created
  • Last Updated Last Updated: 28 Oct 2021 12:57 PM
  • Views 16881 views
  • Likes 4 likes
  • Comments 7 comments
Related
Recommended

New Raspberry Pi Zero 2 W - 5 x Faster!

Meet the New Raspberry Pi Zero 2 W

image

Raspberry Pi Zero W 2Raspberry Pi Zero W 2

 

Introducing the New Raspberry Pi Zero 2 W.

 

The second version of the tiny and powerful fan favorite, building on the success of the current Zero family, Raspberry Pi Zero 2 W is built around a Raspberry Pi-designed System-in-Package, which integrates the BCM2710A1 die used in Raspberry Pi 3 with 512MB of RAM. The exact performance uplift over Zero varies across workloads, but for multi-threaded sysbench it is almost exactly five times faster.

 

Key features:

• 1GHz quad-core, 64-bit ARM Cortex-A53 CPU

• VideoCore IV GPU • 512MB LPDDR2 DRAM

• 802.11b/g/n wireless LAN

•Bluetooth 4.2 / Bluetooth Low Energy (BLE)

• MicroSD card slot

• Mini HDMI and USB 2.0 OTG ports

• Micro USB power

• HAT-compatible 40-pin header

• Composite video and reset pins via solder test points

• CSI camera connector

 

image

Foot Print

 

image

The Raspbery Pi Zero 2 W uses the same Footprint as the previous Raspberry Pi Zero W model.
65mm x 30mm (x 5.2mm maximum z-height)

image

Like Raspberry Pi 1, Raspberry Pi Zero and Zero W are built around the Broadcom BCM2835 SoC. This neatly sidesteps the problem by using package-on-package (PoP) technology, in which the SDRAM package sits directly on top of the SoC. - Raspberry Pi 2021

 

Secrets of the Raspberry Pi Zero 2 W

Simon Martin, who designed the Raspberry Pi Zero 2 W and the RP3A0 package that powers it,  even managed to squeeze a very low-resolution Raspberry Pi logo into the package ball-out, as you can see from this package and X-ray image.

image

 

Modular Radio Certification for Using Raspberry Pi Zero V2 in your own product design

Zero 2 W has FCC modular certification!

The Raspberry Pi Zero 2 W has a large metal shield can, which covers the wireless circuitry on the board and protects it from external interference.

Like all Raspberry Pi products since 3B+, Zero 2 W has FCC modular certification, which reduces the compliance workload involved in incorporating it into an end product. - Raspberry Pi

 

Raspberry Pi Zero V2 Power Supply

The Raspberry Pi Zero uses a Micro USB Power supply, the official power supply comes in US, EU, UK, AU and IN sockets.

image

 

RPI ZERO V2, 12.5W PSU (US)RPI ZERO V2, 12.5W PSU (US)

RPI ZERO V2, 12.5W PSU (EU)RPI ZERO V2, 12.5W PSU (EU)

RPI ZERO V2, 12.5W PSU (UK)RPI ZERO V2, 12.5W PSU (UK)

RPI ZERO V2, 12.5W PSU (AU)RPI ZERO V2, 12.5W PSU (AU)

RPI ZERO V2, 12.5W PSU (IN)RPI ZERO V2, 12.5W PSU (IN)

 

Raspberry Pi Zero W 2Raspberry Pi Zero W 2

  • raspberry pi zero
  • raspberry pi
  • raspberry pi zero 2
  • raspberry pi zero v2
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
  • scottiebabe
    scottiebabe over 5 years ago

    Schematic is available: https://datasheets.raspberrypi.com/rpizero2/raspberry-pi-zero-2-w-reduced-schematics.pdf , I hope this model will be able to operate off an ordinary 5V/2A powerbank. I hope they continue to include Wifi as standard on all models going forward.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 5 years ago

    At somewhere around $15 it looks like a great price/performance ratio, and I like the small form factor

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 5 years ago

    It will be interesting to see what people do with the new board.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • luislabmo
    luislabmo over 5 years ago

    Surprising and very good news!.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14phil
    e14phil over 5 years ago in reply to feiticeir0

    Not bad for a Thursday morning in October!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 5 years ago

    I always like a new member in the RPI family,
    I'm stil la fan of the A+ and for small form factor I moved on to using the Compute Module 4...but I can see myselve using the Zer2W in case I only need to embedd it with GPIO usage, not USB or other preripherals.
    The naming of the prcessor combinatory package RP3A0 makes me hope its going a similar route like the RP2040--> available as a SOC for our own boards.

    Which would give me some amaaaaaazing posssibilities for highly integrated embedded linux things.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • feiticeir0
    feiticeir0 over 5 years ago

    One of the first things I do when I wake up, besides shutting down the alarm, is check the email... Maybe something happened during the night - and today something did.

     

    For my delight, a new Raspberry PI W was launched.  This week we saw Eben Upton talk about increasing the price of the Raspberry PI 4B 2GB (because of components shortage) and today they launch a new Raspberry PI.

    Those guys are full of surprises.  Already bought one. Let's wait and see the power of this one !