Raspberry Pi
  • Products
  • More
Raspberry Pi
Documents Pi Desktop: Booting from the SSD (aka booting from USB devices on a Pi 3)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: cstanton
  • Date Created: 3 Jul 2017 2:38 PM Date Created
  • Last Updated Last Updated: 10 May 2021 8:50 PM
  • Views 13628 views
  • Likes 8 likes
  • Comments 66 comments
Related
Recommended

Pi Desktop: Booting from the SSD (aka booting from USB devices on a Pi 3)

Amazingly, the Raspberry Pi booting from a USB device is a huge point of controversy. A great deal many people believe that you still require the SDCard to be able to do it. This is definitely no longer the case, especially with the Raspberry Pi 3. So even though with the Pi Desktop you're going to be connecting a Solid State Drive via a SATA to USB 2.0 interface, where you're going to lose some speed, overall, it's still an improvement. If for nothing else, the capacity of what you can store on it. The add-on HAT board will take an mSATA SSD up to 1 Terabyte in size, and for that to be faster to boot and access than an SDCard and for some USB 'sticks' or 'drives' then that is a significant improvement in itself, and I know a lot of people out there want a dedicated Pi NAS box after all.

 

So why isn't this straight forward for a lot of people? Why can't you simply plug in your mSATA SSD, format it and get going? Well, I've identified are a few areas that people are mainly struggling with on this:

 

  • You have to enable the 'USB Boot bit' on the Raspberry Pi 3 first (this is permanent)
  • Your SSD has to be imaged in the 'right way'
  • Some have the impression that you still need the SDCard in, and that you need to mount the SSD (you can do this, though, you don't strictly have to use the SSD as a boot device)
  • The mSATA SSD has to be supported by the add-on HAT (I'm not actually sure of any that aren't and there's no reference list at the moment, this is mostly hypothetical).
  • There are/were problems with the PiDesktop debian file supplied by Embest (these are being worked on and there is an official github repo here).

 

On the SSD being imaged in 'the right way', you can end up encountering problems imaging your SSD card as you likely do with your SDCard, especially with Microsoft Windows. Windows has a terrible interface to the SDCard readers with the various software that's available. This is either because the software can only refer to the device via the 'drive letter' or by the 'hardware device ID'. Unfortunately most software (eg. Win32DiskImager, I'm looking at you) can only handle imaging drives when it has a drive letter. This totally fails if you haven't even partitioned your device yet and assigned it a drive letter, and some people feel forced to format it to FAT32, this can break things even further. You don't need to format or pre-partition your device, merely assign it a drive letter. There're two useful pieces of software I use to handle this, one is the free software 'Active Partition Manager' and the other is the Disk Management Snapin for Management Console.

 

Let's go through some steps on setting this up. By all means comment on this with your experiences or software you've used that has been successful. What you're about to read is my except from the user manual.

 

image

 

Connecting an mSATA SSD

 

Inside the Pi Desktop we can access the data stored onto the mSATA SSD in one of two ways. Either via USB from the add-on board and then into the attached Raspberry Pi (where we can also boot from it), or connect it to an external computer via USB without having to open up the Pi Desktop case (though you still need to 'turn on' the Pi Desktop for this to work).

 

If the mSATA SSD that you have connected is pre-formatted with a partition using a FAT32 file system (FS), then this FS is typically accessible by all known modern operating systems (OS), and easily accessible. Though if it uses a typical Linux FS such as ext2/3/4, this is trickier to access by all OSs.

 

Note: If you’re connecting the mSATA SSD add-on board to a computer other than the Raspberry Pi inside the Pi Desktop, then you will need the appropriate cable, and you will also have to power the add-on board/Pi Desktop and press the power-on switch. This will also power on the Raspberry Pi if it is still connected.

 

Imaging and Setting Up Partitions

An easy to use utility for managing the partitions on the drive is ‘gparted’ from the Raspbian (OS) (for example if you booted from the SDCard):

 

> http://gparted.org/

 

This is a graphical user interface (GUI) tool that can be used to manage the partitions on your drives, connected via USB or otherwise. It can be installed via the apt package manager from the command line interface (CLI) :

 

> sudo apt-get update

> sudo apt-get install gparted

 

Then you can either run it from the menu of your Raspbian OS, or from the CLI:

 

> sudo gparted

 

From here you can (re)partition your mSATA SSD if it’s running a supported file system. If you are using the CLI, then you will want to issue the following command:

 

> sudo fdisk /dev/<identifier>

 

Where <identifier> is the mount point for the mSATA SSD.

 

Alternatively, you can simply write an image to the mSATA SSD, just as you would write an image to an SDCard. The Raspberry Pi Foundation have instructions on how you write images here:

 

https://www.raspberrypi.org/documentation/installation/installing-images/

 

Note: if you write an image to your mSATA SSD then the data used and accessible from the OS will only be of the size of the image written, unless you resize the partitions.

 

Mounting the mSATA SSD to Access Files

 

Raspbian

The Raspbian OS is based upon Debian Linux, and as such supports the majority of commands and functions that you would use to mount drives within that OS (these typically involve fstab - https://wiki.debian.org/fstab, and pmount - https://wiki.debian.org/pmount ).

 

From the GUI

Depending on your version of Raspbian, and how you have it configured, when you boot your Raspberry Pi to the GUI and then connect the attached mSATA SSD, you will be prompted what to do with your “Removable media” that has been inserted, and the drive will be automatically mounted.

 

It is possible that the GUI will not behave in this way, and instead you will have a transparent icon representing the drive on your desktop, which you can then double-click with the left mouse button and Raspbian will attempt to mount it.

 

From the CLI

When mounting the drive from the GUI, you will have made the drive accessible from the CLI. Typically this is located within the following folder:

 

/media

 

However, sometimes we can’t use the GUI, or merely we don’t want to. To mount the drive we must first know how Linux is referring to it. Linux has the majority of its hardware listed under the ‘/dev’ folder structure, with connected devices typically using the format of ‘/dev/sd<x>’ where <x> is a letter. These can even extend further with ‘/dev/sd<x><y>’ where <y> is the number of the partition(s) on the device.

 

There are a few commands in which we can determine what the device is of a USB device we connect, first, connect the USB device, and then type the following:

 

> dmesg

 

This will tell you basically the contents of a system log which gives you information about the device you have just plugged in. You can also issue the following commands:

 

> lsusb

 

Which will tell you about the device identifiers, and also:

 

> lsblk

 

This command will tell you the /dev/ mount points.

 

Note: If you have problems running a command, try typing ‘sudo’ before it.

 

Now, you will need somewhere to mount the drive to. Let’s make a directory and set the permissions onto it:

 

> sudo mkdir /media/ssd

> sudo chmod 755 /media/ssd

 

Once you know the device mount point, you can then issue the following command:

 

> sudo mount /dev/sd<x><y> /media/ssd

 

Note: Mounting will only work if the mSATA SSD has a file system and partitions setup (see ‘Imaging and Setting Up Partitions’ in this document.), you will want to mount the relevant partition (which has a number, such as /dev/sdb1) as opposed to the device itself (/dev/sdb).

 

The Raspberry Pi Foundation’s official magazine, The Mag Pi has a good article on this:

 

https://www.raspberrypi.org/magpi/connecting-disks-with-the-command-line/

 

 

Microsoft Windows

Thanks to an open source project called Ext2Fsd (Ext2 File System Driver) it is now possible to very easily mount linux FS onto Microsoft Windows OS.

 

You can download and install the software from these websites:

 

http://www.ext2fsd.com/

https://sourceforge.net/projects/ext2fsd/

 

To install the software you will need to have administrative rights on the computer you’re installing it onto, and the ability to install the required system drivers. Afterwards you will likely have to reboot.

 

After you have connected the mSATA SSD HAT board to your computer, you will see it in Windows device manager as a USB Mass Storage Device and also as a drive:

 

imageimage

 

 

From the start menu, you will want to open the ‘Ext2Fsd’ folder and then ‘Ext2 Volume Manager’:

 

image

 

From the software we can then see the partitions of all of the drives listed, including the identified ext FS:

 

image

 

Since in this example, we have already imaged the mSATA SSD with Raspbian, a FAT32x partition is listed (drive E:). it is the EXT4, Linux FS we want below it:

 

image

 

image

 

 

 

Make sure we want to give it a drive letter so we can access it, there are various mounting options you can choose from.

 

image

 

Windows Explorer then has the new drive listed, which we can then open and view the Linux EXT FS:

 

image

 

You can now alter the files and unmount them as necessary.

 

Boot from the mSATA SSD

Configuring your Raspberry Pi to boot from a USB device is a one-way setting. You are configuring a ‘flag’ or a ‘bit’ on your Raspberry Pi chip that you cannot revert.

 

The Raspberry Pi will always prioritise booting from the SDCard when one is present.

 

To set this up, you will need an SDCard in your Raspberry Pi that has the Raspbian OS on it. Inside the file located in:

 

/boot/config.txt

 

You need to set this option to the value ‘1’ :

 

program_usb_boot_mode=1

 

Then power on your Raspberry Pi with the SDCard inserted. That’s all there is to it. Once you’re in Raspbian, you can run the following command from the CLI:

 

> vcgencmd otp_dump | grep 17:

 

This should output the following:

 

17:3020000a

 

Now all you need to do is ensure your mSATA SSD has an OS on it, that it’s connected via USB and power up your Pi Desktop. If you’re unsure about these steps then you can read the following guide on the Raspberry Pi Foundation site:

 

https://www.raspberrypi.org/documentation/hardware/raspberrypi/bootmodes/msd.md

 

You can write the same Raspbian image to your mSATA SSD as you have done to your SDCard. You now no longer need the SDCard to boot your Raspberry Pi once this flag is set.

 

I've got a Pi Desktop sat on my desk here, if there's any further information you need, or believe I should elaborate on any part of this, then go ahead and ask by adding a comment and I'll do my best.

  • raspberry pi 3 ssd
  • rpiintermediate
  • ssd
  • raspberry pi 3 hard drive
  • raspberry_pi
  • setup ssd
  • pi desktop
  • raspberry pi 3
  • raspberry pi 3 setup
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • cstanton
    cstanton over 9 years ago in reply to DAB +3
    Both fortunately, and unfortunately, DAB, that's exactly what you have to do. Dive in. The hardware in its current state isn't going to change from needing the config file altering on the SDCard for that…
  • fvan
    fvan over 9 years ago in reply to DAB +2
    I agree with DAB, ease of use (or installation) is key. Look at the recurrent issues on Raspberry Pi, a lot of cases are about incorrectly flashed SD cards etc ... If that's already too difficult, this…
  • DAB
    DAB over 9 years ago +1
    Nice post, but what most of us want is to be able to just add the SSD and reboot. Until you can make it that easy, most of us are just too scared to dive in with our limited Linux skills. DAB
  • cstanton
    cstanton over 9 years ago in reply to trlaing

    Thanks trlaing , so have you tried the latest version of the debian package, having uninstalled the currently installed one and checked if you still have a problem?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • trlaing
    trlaing over 9 years ago in reply to cstanton

    Hi Christopher

    First of all, thank you for looking into this for me. I have the latest release of Raspbian installed on a brand new Raspberry Pi 3 purchased at the same time from CPC.

     

    Raspbian Jessie with desktop

    Image with desktop based on Debian Jessie

    Version: July 2017

    Release date: 2017-07-05

    Kernel version: 4.9

     

    Image file: 2017-07-05-raspbian-jessie.img

     

    The image was backed up from the SD card after running "sudo apt-get update && sudo apt-get upgrade -y" then written to a Sandisk mSata drive which it is now booting from without an SD card installed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 9 years ago in reply to trlaing

    Hi trlaing , I fed this back to the developers and they're not seeing the same issue as you are, at least with the most recent debian package which is available here https://github.com/pi-desktop/deb-make/releases

     

    They've asked what version of raspbian you're using / what image you're using, too. If you're able to supply that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • trlaing
    trlaing over 9 years ago

    Is it possible to completely bypass the power button features of the PiDesktop? In the event of a power-cut, it does not restart. If I plug the power cable into the Pi instead of the PiDesktop, will I still have access to the mSata drive? Or is it possible to set it to start the Pi without pressing the button once the power is switched on?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 9 years ago in reply to tedvan

    Have you tried connecting the SSD Hat via USB to your Mac and then writing the card image to the SSD? This is mentioned in the manual, you will need to press the power button to power on the hat.

     

    Also, unless you need to run a different operating system to Raspbian, avoid using NOOBS and use the Raspbian image instead.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tedvan
    tedvan over 9 years ago in reply to cstanton

    I use a Mac to copy the NOOBS files to a clean formatted SDcard (using SDFormatter) or a clean disk (formatted with DiskUtility). On my Mac I use Etcher to write an image (or PiBakery for preconfigured Rasbian).

    In this post: http://www.makerspace-uk.co.uk/setting-diy-pi-desktop-kit/  I found some hints that I will try next time. Seems that ppp-hdclone is where many users get lost. Also noticed that some USB drives cannot be booted from with a Pi3 with the bit set...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 9 years ago in reply to tedvan

    What operating system does your other computer run which you're using to write the image to the SDCard?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • trlaing
    trlaing over 9 years ago in reply to trlaing

    I have removed the following files from the "/lib/systemd/system/" folder and rebooted:

    embest.service

    embest-shutdown.service

     

    I presume they are the services installed during the Pi Desktop installation that enables the power button for powering off. The button no longer shuts down the Pi but "sudo reboot" successfully reboots the Pi. This is a temporary fix that I am happy with. Hopefully element14 will update their software to fix this issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • trlaing
    trlaing over 9 years ago

    I have successfully installed my Raspberry Pi 3 / Pi-Desktop / Samsung 32GB mSata drive and have it booting to the mSata without the MicroSD card. However, I have noticed that it will not reboot using the command 'sudo reboot' or 'sudo shutdown -r now' - it does start to reboot, but after the first 4 lines of text after the "rainbow" box screen it just powers off. It successfully boots when pressing the power button to power back on, shuts down when holding the button for 2 seconds, then starts up again fine when pressing the power button again, but the reboot command does not boot up again. I need to be able to reboot this Pi remotely, so need the reboot facility.

     

    Any ideas anyone?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tedvan
    tedvan over 9 years ago in reply to cstanton

    I tried two other ways but I still can not get my Pi3 to boot without SDCard :-(

     

    I made sure the bit was set first and then put NOOBS on the mSATA SSD and rebooted: it does not want to start from that

     

    Then I started with NOOBS on the SDcard and Raspbian installed fine: After that connected the SSD and tried to duplicate everything to the SSD following the steps from the manual: but the ppp-hdclone does not work (all options greyed) Instead I used the SDcopy from the menu, which finished successfully. Ran ppp-hdclone again to finish the last part of the process, took out the SDCard booted again and got a kernel panic : unable to mount root fs on unknown block.

     

    So now I am back at the procedure to install from a NOOBS SDCard to the SSD. IThis works fine but I have to leave in the SDcard to boot

     

    I hope you can give me a procedure that works: the one in the Manual does not

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>