Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Raspberry Pi Compute Module 3+
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14phil
  • Date Created: 28 Jan 2019 11:24 AM Date Created
  • Last Updated Last Updated: 4 Feb 2019 4:27 PM
  • Views 2716 views
  • Likes 4 likes
  • Comments 4 comments
Related
Recommended

Raspberry Pi Compute Module 3+

Meet the Compute Module 3+ is the latest addition to the Raspberry Pi Compute Module range.

imageimage

Raspberry Pi Compute Module 3+ 8G, 16GB, 32GB

 

For anyone already following the Raspberry Pi foundations work from a developers viewpoint will be very happy to hear that they have released a new Compute Module.
Based on the same chip as Raspberry Pi 3 Model B+ Broadcom BCM2837B0, a 64-bit quad core processor running at 1.4GHz.

For the uninitiated, the compute module range has all the brains and power of the Raspberry Pi but in a form factor that is optimized for being embedded into a design, for example the standard external USB, power and ethernet have been removed and broken out into the fin edge connector.  The Compute Module 3+ is priced lower than the average Pi and has a wider operating temperature range.

In addition to the super fast processor the new Compute Model 3+ comes in three different onboard memory variants; 8GB, 16GB & 32GB, to suits every kind of industrial embedded design applications.

 

But, what if you don't want onboard memory and your prototype has an SD card slot or other type of boot memory else where on its PCB?!?!... then we have you covered with the Compute Module 3+ Lite

Compute Module 3+ Lite

A Lite version of the Compute Module 3+ is also available.

The CM3L brings the SD card interface to the Module pins so a user can wire this up to an eMMC or SD card of their choice.

 

imageimage

Raspberry Pi Compute Module3+ Lite

 

Raspberry Pi Compute Module3+ Lite

The Compute Module 3+ simplifies the design process engineers need to undertake when developing a System on Module (SoM) solution into their final product. Engineers do not need to concern themselves with the complexities of interfacing with the BCM2837B0 processor directly and instead can concentrate on designing the interfaces to their own IO board and their application software. This simplicity fosters rapid development.

 

  • Broadcom BCM2837B0, Cortex-A53 64-bit SoC @ 1.2GHz
  • 1Gbyte LPDDR2 SDRAM
  • Memory Options: 8 Gbytes, 16 Gbytes, 32 Gbytes eMMC Flash or None.
  • Multimedia: H.264, MPEG-4 decode (1080p30), H.264 encode (1080p30), OpenGL ES 1.1, 2.0 graphics
  • SD card support: The CM3+ Lite brings the SD card interface to the module pins so a user can connect this to either an eMMC or SD card.
  • Environment: Operating temperature, -20° to +70°C
  • 35u hard gold plated IO Pins

 

Buy the Raspberry Pi Compute Module 3+

 

Without Flash Memory

Raspberry Pi Compute Module 3+ LiteRaspberry Pi Compute Module 3+ Lite

 

With Flash Memory

Raspberry Pi Compute Module 3+ 8GBRaspberry Pi Compute Module 3+ 8GB

Raspberry Pi Compute Module 3+ 16GBRaspberry Pi Compute Module 3+ 16GB

Raspberry Pi Compute Module 3+ 32GB Raspberry Pi Compute Module 3+ 32GB

 

Development Kit

Raspberry Pi Compute Module 3+ Dev KitRaspberry Pi Compute Module 3+ Dev Kit

 

Want to Discuss Raspberry Pi, Join Built Contents and Enter Give-aways?
Check out the Raspberry Pi Space Here

 

Why join the element14 Community?

CONNECT. LEARN. CREATE. INSPIRE.

Established in 2009, the element14 Community is the industry standard for electronics collaboration. It has popular technical blogs, videos and webinars that provide information on the latest in electronics trends such as the Internet of Things and Wireless Technologies. It also hosts our video project releases in element14 presents on Wednesdays and Fridays. It is a place where you can:

  • CONNECT with a community of thousands of engineers and innovators from all over the world.
  • LEARN about the very latest in new technology from industry experts, suppliers, independent sources and user reviews.
  • CREATE and source your next electronics project with access to 24/7 community support to tackle tough project challenges.
  • INSPIRE and be Inspired; build your next project and help others to create a better connected world.
Our Exclusive Features
imageimageimage

element14 Design Challenge

By connecting engineers to powerful new ideas and to each other, the element14 Design Challenge is creating innovative solutions to everyday problems.

element14 Design Center

Explore our huge selection of hardware development tools and software products, all supported with the technical resources you will need.

EAGLE PCB Design Software

Whether you are a team of one, or part of a large engineering department, EAGLE provides quality PCB design software with the features that get the job done.

Join the ChallengeExplore NowLearn More
imageimageimage

element14 presents

Join the hackers, engineers and makers of element14 presents as they tackle new and fun projects each week using circuitry design, 3D printing, microcontrollers, and much more.

element14 RoadTest

Apply to test new products from top manufacturers like NXP, Microchip, and Rohde & Schwarz. If selected, put that new product through its paces and you'll keep it for free.

Online Learning

Together with our manufacturer partners, we offer Webinars on a wide range of engineering topics. Stay up-to-date on the latest trends and the hottest technologies.

Watch EpisodeEnroll NowStart Now
imageimageimage

Tech Connection

Keep up on the latest tech trends with the element14 Tech Journal or learn about the most current technologies today in Tech Spotlight.

Project14

A monthly project compeition open to all Community members. Apply for a chance to win a $100 shopping spree.

Prototype to Production

Join element14's Business of Engineering and learn how to launch companies successfully from prototype to production.

Learn MoreSubmit ProjectFind out More




  • rpi cm
  • raspberry pi compute module 3
  • raspberry pi
  • compute module
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • Problemchild
    Problemchild over 7 years ago in reply to e14phil +2
    A lot more useful now it has that Flash memory Phil. You can get the entire OS application and a wedge of data without recourse to an external SD card. An HAB balloon board using this would save a load…
  • e14phil
    e14phil over 7 years ago +1
    With the new on-board Flash Memory what will you all be making with this new Compute Module?
  • e14phil
    e14phil over 7 years ago in reply to Problemchild +1
    ohh sounds good John. Its pretty cool and pretty small too
  • tonydbeck
    tonydbeck over 7 years ago

    Great news the Compute Module 3+ has more flash memory options!  One limitation I have found with the original module and a board I was using is the 4GB flash.  This limited me to what OS I could install.  Now with options up to 32GB it is possible to install any of the available OS options.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14phil
    e14phil over 7 years ago in reply to Problemchild

    ohh sounds good John. Its pretty cool and pretty small too

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 7 years ago in reply to e14phil

    A lot more useful now it has that Flash memory Phil. You can get the entire OS application and a wedge of data without recourse to an external SD card.

    An HAB balloon board using this would save a load of space and be a lot more robust than an normal RPI

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14phil
    e14phil over 7 years ago

    With the new on-board Flash Memory what will you all be making with this new Compute Module?