Raspberry Pi
  • Products
  • More
Raspberry Pi
Documents Raspberry Pi High Quality Camera
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14phil
  • Date Created: 30 Apr 2020 7:18 AM Date Created
  • Last Updated Last Updated: 30 Apr 2020 8:47 AM
  • Views 6984 views
  • Likes 13 likes
  • Comments 20 comments
Related
Recommended

Raspberry Pi High Quality Camera

Raspberry Pi High Quality Camera Specs

 

Wildlife photographers, Home CCTV installers, Computer vision pioneers and Astronomy hackers, REJOICE your prayers have been answered.

Today we are excited to introduce to you the new Raspberry Pi High Quality Camera, a High Quality, 12 Megapixel Sony IMX477 Sensor with interchangeable lenses.

image

Raspberry Pi HQ CameraRaspberry Pi HQ Camera

 

The Raspberry Pi High Quality Camera is the latest camera accessory from Raspberry Pi.

It offers higher resolution (12 megapixels, compared to 8 megapixels), and sensitivity (approximately 50% greater area per pixel for improved low-light performance) than the existing Camera Module v2, and is designed to work with interchangeable lenses in both C- and CS-mount form factors. Other lens form factors can be accommodated using third-party lens adapters.

 

The package comprises a circuit board carrying a Sony IMX477 sensor, an FPC cable for connection to a Raspberry Pi computer, a milled aluminium lens mount with integrated tripod mount and focus adjustment ring, and a C- to CS-mount adapter.

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

In addition the the Raspberry Pi HQ Camera, two official Lenses have been releases, The 6mm Wide Angle Lens and the 16mm Telephoto Lens, with compatibility for other 3rd Party Lenses through the integrated C and CS Mount.

 

Raspberry Pi HQ Camera Interchangeable Lenses.

imageimage

Raspberry Pi HQ Camera with 16MM Telephoto Lens

Raspberry Pi HQ CameraRaspberry Pi HQ Camera

RPi 16MM Telephoto LensRPi 16MM Telephoto Lens

Raspberry Pi HQ Camera with 6MM Wide Angle Lens

Raspberry Pi HQ CameraRaspberry Pi HQ Camera

RPi 6MM Wide Angle LensRPi 6MM Wide Angle Lens

 

 

Raspberry Pi HQ Camera FAQ

 

Will this camera work with my Raspberry Pi?

It is compatible with all models of Raspberry Pi computer from Raspberry Pi 1 Model B onwards, using the latest software release from

www.raspberrypi.org.

 

Do I need to buy a lens?

Yes, the same as a DSLR Camera, you need to pair the Raspberry Pi HQ Camera with a lens. You can Buy one of the two listed above or pair it with any 3rd Party C-Mount or CS-Mount Lens.

 

What are the Raspberry Pi HQ Camera Specifications

 

Sensor

Sony IMX477R stacked, back-illuminated sensor

12.3 megapixels

7.9 mm sensor diagonal

1.55 μm × 1.55 μm pixel size

OutputRAW12/10/8, COMP8
Back FocusAdjustable  (12.5mm to 22.4mm)
Lens Mounts

C-Mount

CS-Mount (C-CD Adapter Included)

IR Cut FilterIntegrated
Ribbon Cable Length200mm
Tripod Mound1/4" -20
Compliance

FCC 47 CFR Part 15, Subpart B, Class B Digital Device

 

Electromagnetic Compatibility Directive (EMC)

2014/30/EU

Restriction of Hazardous Substances (RoHS)

Directive 2011/65/EU

Production Lifetime

The Raspberry Pi High Quality Camera will remain

in production until at least January 2026

 

 

What Camera Mount Does the Rapsberry Pi HQ Camera come with?

The Raspberry Pi HQ Camera has a milled aluminium lens mount with integrated tripod mount and focus adjustment ring, and comes with a C- to

CS-mount adapter.

 

image

 

 

How Does the Raspberry Pi HQ Camera connect to my Raspberry Pi?

With an FPC cable, the same as the Raspberry Pi Camera V2. You will need to use the most up to date software for your Raspberry Pi.

 

Raspberry Pi HQ Camera Dimensions

image

 

Can you remove the Raspberry Pi HQ Camera's Infrared IR Filter?

Technically Yes... BUT..  but doing so will void the warranty on the product, and is likely to prove irreversible.

Read more info here.

 

Taking Photos with the Raspberry Pi HQ Camera

 

First, Make sure your raspberry Pi is up to date by connecting your Raspberry Pi to the internetand running:

sudo apt update  and  sudo apt full-upgrade

 

Then enable the camera in Raspbian: in the Raspbian menu, select Preferences, then Raspberry Pi Configuration. Click the Interfaces tab, find the Camera entry in the list, and select Enabled. Click OK, and reboot your Raspberry Pi when prompted.

 

raspistill is a command line tool for capturing camera images.

 

To check your camera is correctly installed, open a terminal window (Raspbian menu > Accessories > Terminal) and take a test photograph by entering the command:

raspistill -o test.jpg

 

When you hit ENTER a live preview image will appear, and after a default period of five seconds, the camera will capture a single still image. This will be saved in your home folder and named test.jpg.

 

To use the camera just as a viewfinder, without saving a photo, use this command:

raspistill -t 0

 

For more detailed information about installing and operating camera software, refer to

https://www.raspberrypi.org/documentation/configuration/camera.md

 

For more advanced information about controlling the camera, see

https://www.raspberrypi.org/documentation/raspbian/applications/camera.md

 

Now the biggest question.... What will you build with a Raspberry Pi HQ Camera?

Attachments:
image20200430 Raspberry Pi High Quality Camera Getting Started.pdf
  • raspberry pi hq camera
  • raspberry pi camera computer vision
  • rpi cctv
  • raspberry pi 4
  • raspberry pi
  • raspberry pi camera for cctv
  • computer vision camera
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • Workshopshed
    Workshopshed over 6 years ago +5
    Would definitely be interested to see how this captures video and if you need to fit out your Pi with additional storage.
  • Problemchild
    Problemchild over 6 years ago in reply to shabaz +5
    Yes Shabaz handy but a tad expensive for what it is then again everyone else charges more for that sensor so maybe they think it can support that price. One thing it does need is some dust protection as…
  • beacon_dave
    beacon_dave over 6 years ago in reply to beacon_dave +5
    8 MegaPixel Sony IMX219 imager with CS mount lens on the left and M12 mount lens on the right.
  • colporteur
    colporteur over 6 years ago in reply to dougw

    Sweet! The RoadTest application would need to be resolved with a Thunderdome competition!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 6 years ago

    This camera would make a great road test.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 6 years ago in reply to beacon_dave

    Most warrantees are useless, but getting to the full range of the sensor is worth a little risk.

     

    DAB

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 6 years ago in reply to DAB

    Do you consider yourself an 'adventurous type who laughs in the face of a voided warranty' ?

     

    https://www.raspberrypi.org/blog/new-product-raspberry-pi-high-quality-camera-on-sale-now-at-50/#comment-1527936

     

     

    Removing the infrared (IR) filter from the Raspberry Pi High Quality Camera

    https://www.raspberrypi.org/documentation/hardware/camera/hqcam_filter_removal.md

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 6 years ago

    I like it.

    Are they going to do a no IR version?

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 6 years ago in reply to ipv1

    If not, then ArduCam have some Jetson Nano solutions that may be of interest:

    https://www.arducam.com/jetson-nano-one-arducam-driver-support-all-camera-sensor/

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ipv1
    ipv1 over 6 years ago

    I wonder if these work with the NVIDIA Jetson Nano and the like. Seem like something that would kick things up a notch.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 6 years ago in reply to beacon_dave


    8 MegaPixel Sony IMX219 imager with CS mount lens on the left and M12 mount lens on the right.image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 6 years ago in reply to shabaz

    Me too. I have stopped the path to arducam for this.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 6 years ago in reply to shabaz

    Have they ever been in stock as of yet Shabaz?? I've seen this and Pimoroni's ad today only and they both have no stock.

    On another note I have a spare unused Unicorn if any one wants to buy ?

    ;-)

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
>