Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Raspberry Pi 7” Touchscreen Display
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: joeman
  • Date Created: 11 Aug 2015 6:55 PM Date Created
  • Last Updated Last Updated: 16 May 2022 10:17 AM
  • Views 116534 views
  • Likes 20 likes
  • Comments 478 comments
Related
Recommended

Raspberry Pi 7” Touchscreen Display

image

Raspberry Pi 7” Touchscreen Display

Buy Here  Display Installation Guide

Install Virtual Keyboard* Other Pi Accessories  image

The 7” Touchscreen Monitor for Raspberry Pi gives users the ability to create all-in-one, integrated projects such as tablets, infotainment systems and embedded projects. The 800 x 480 display connects via an adapter board which handles power and signal conversion. Only two connections to the Pi are required; power from the Pi’s GPIO port and a ribbon cable that connects to the DSI port present on all Raspberry Pi’s.  Touchscreen drivers with support for 10-finger touch and an on-screen keyboard will be integrated into the latest Raspbian OS for full functionality without the need for a physical keyboard or mouse.

*Note: Your NEW Rasp Pi 7.0 needs you to Add a Virtual Keyboard….

imageimage

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Raspberry Pi Sense HAT

image

Learn More  image

Technical Specification:

image  7” Touchscreen Display

image  Screen Dimensions: 194mm x 110mm x 20mm (including standoffs)

image  Viewable screen size: 155mm x 86mm

image  Screen Resolution 800 x 480 pixels

image  10 finger capacitive touch

image  Connects to the Raspberry Pi board using a ribbon cable connected to the DSI port

image  Adapter board is used to power the display and convert the parallel signals from the display to the serial (DSI) port on the Raspberry Pi

image  Will require the latest version of Raspbian OS to operate correctly

 

Features and Benefits

image  Turn your Raspberry Pi into a touch screen tablet, infotainment system, or standalone device.

image  Truly Interactive - the latest software drivers will support a virtual ‘on screen’ keyboard, so there is no need to plug in a keyboard and mouse.

image  Make your own ‘Internet of Things’ (IoT) devices including a visual display. Simply connect your Raspberry Pi, develop a Python script to interact with the display, and you’re ready to create your own home automation devices with touch screen capability.

image  A range of educational software and programs available on the Raspberry Pi will be touch enabled, making learning and programming easier on the Raspberry Pi.

Kit Contents

image  7” Touchscreen Display

image  Adapter Board

image  DSI Ribbon cable

image  4 x stand-offs and screws (used to mount the adapter board and Raspberry Pi board to the back of the display

image  4 x jumper wires (used to connect the power from the Adapter Board and the GPIO pins on the Pi so the 2Amp power is shared across both units)

NOTE: THE RASPBERRY PI AND POWER SUPPLY ARE NOT INCLUDED IN THIS KIT AND ARE SOLD SEPARATELY.

Compatible With:

Raspberry Pi 3 Model B

Raspberry Pi 2 Model B

Raspberry Pi Model B+

Raspberry Pi Model A+

The display will technically work with the Model A and Model B boards (connecting it to the DSI port on the Pi board), however the mounting holes on the back of the display will only line up with the newer board design (A+, B+, Pi 2 and Pi 3).

 

How to Install the Matchbox-Keyboard for your Pi

image

1. Connect a physical keyboard to the Raspberry Pi (or SSH into it if that’s your thing.)

2. Connect to the internet via WiFi or Ethernet.

3. Open the terminal.

4. Type sudo apt-get install matchbox-keyboard

5. Let the program download & install (takes 30s-1min depending on your connection.)

6. Exit the terminal & reboot your Pi.

7. The keyboard can be found by clicking the Menu -> Accessories -> Keyboard.

 

Operating System Support

In order to be sure you’re running the latest version of Raspbian, connect your Raspberry Pi to the Internet and then open LX Terminal.  Type ‘sudo apt-get update’ to download the latest version of the OS.  Once that’s complete, type ‘sudo apt-get upgrade’ to apply the download to your Raspberry Pi.  That way you’ll have all of the latest drivers and software needed to support the touch screen display.

Step 1

image

Step 2

image

Step 3

image

Step 4

image

Step 5

image

Step 6

image

Step 7

image

Step 8

image

Step 9

image
  • pi_guide
  • raspberry
  • pi
  • pi_display
  • raspberry_pi
  • matchbox_keyboard
  • display
  • touchscreen
  • 7”
  • guide
  • installation
  • 7_inches
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 9 years ago in reply to idometeor +3
    Jason Does Meteor wrote: As mentioned, I tried that. Actually you didn't, you stated: I have tried everything and I cannot get the display to rotate in Raspbian. I have written many X configuration files…
  • softweyr
    softweyr over 11 years ago in reply to ejohnfel +2
    Yeah, this is not a bad price for a 7" display, plus you get the touchscreen, integrated keyboard, etc. And tomorrow is my birthday!
  • bwelsby
    bwelsby over 11 years ago in reply to phantomski +2
    The reduced screen size is because Overscan settings are enabled. you can either comment out the settings in /boot/config.txt or just run raspi-config and select the advanced options then Overscan , Disable…
  • jack.chaney56
    jack.chaney56 over 10 years ago in reply to e14 Contributor

    Careful of your diagnostic wording.  Creating a PDF is making the file, presenting the PDF is putting it on a screen.

     

    Jack.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    FYI: PDF generation is a little broken with images rolling off page.

    It still very useable though.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cmdshft4
    cmdshft4 over 10 years ago

    Couple questions:

    Why is the bezel so large and is it removable?

    Are there plans to produce a model with higher resolution? It would be great to have an official RPi display with something like 1024x600 support.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cmdshft4
    cmdshft4 over 10 years ago

    Couple questions:

    Why is the bezel so large and is it removable?

    Are there plans to produce a model with higher resolution? It would be great to have an official RPi display with something like 1024x600 support.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jack.chaney56
    jack.chaney56 over 10 years ago in reply to e14 Contributor

    I love the expectations brought on by plug-n-play (he says sarcastically). Great hardware is only part of the story, if the device drivers aren't working properly, then the hardware becomes an expensive paper weight.  I think a few of the responses in this thread have covered the Python code to test the interface,

     

    Jack

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hi!  Just got my touch panel.  I've got it working as a display, but no touch interface.  I did the apt-get update, upgrade and rebooted more than once.

     

    Any ideas?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to roberto.romero

    if you follow my or many other tutorials on getting the display assembled, connected and configured you should have no issues.

     

    see here:-

    Create Boot SD Card

    Install Raspbian and test without display

    Assemble Display

    Test Display

     

    Now if you have added your display to an earlier version of Raspbian I would suggest downloading hte latest and trying that, it needs nothing added to get display and touch to work as you will see in my video tutorials

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • roberto.romero
    roberto.romero over 10 years ago

    Hello everyone.

    I have bought a brand new raspberry pi 2 B model and also the display. I attached the display as per video instructions, but nothing comes up in the display.

    Is there a specific command that I need to run in order to get this going?

    Another thing...since i have not downloaded any updates of the operating systems... how can I check if my new pi 2 has the latest software?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to e14 Contributor

    It should work right off the bat as far as the display is concerned, this is the case with Windows 10 IoT too. The only issue may be if the Touch part of the display will work, you may need an additional driver added for that (And that is beyond my skill set with Linux based systems)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Not sure if I missed this in another post......

     

    How in the world do you get the 7" Touchscreen to work with a different OS? For Example Kali Linux. I've used Kali on my Pi 2 for a long time now, sure would be nice to get this thing working with it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>