Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Raspberry Pi 7” Touchscreen Display
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: joeman
  • Date Created: 11 Aug 2015 6:55 PM Date Created
  • Last Updated Last Updated: 16 May 2022 10:17 AM
  • Views 116560 views
  • Likes 20 likes
  • Comments 478 comments
Related
Recommended

Raspberry Pi 7” Touchscreen Display

image

Raspberry Pi 7” Touchscreen Display

Buy Here  Display Installation Guide

Install Virtual Keyboard* Other Pi Accessories  image

The 7” Touchscreen Monitor for Raspberry Pi gives users the ability to create all-in-one, integrated projects such as tablets, infotainment systems and embedded projects. The 800 x 480 display connects via an adapter board which handles power and signal conversion. Only two connections to the Pi are required; power from the Pi’s GPIO port and a ribbon cable that connects to the DSI port present on all Raspberry Pi’s.  Touchscreen drivers with support for 10-finger touch and an on-screen keyboard will be integrated into the latest Raspbian OS for full functionality without the need for a physical keyboard or mouse.

*Note: Your NEW Rasp Pi 7.0 needs you to Add a Virtual Keyboard….

imageimage

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Raspberry Pi Sense HAT

image

Learn More  image

Technical Specification:

image  7” Touchscreen Display

image  Screen Dimensions: 194mm x 110mm x 20mm (including standoffs)

image  Viewable screen size: 155mm x 86mm

image  Screen Resolution 800 x 480 pixels

image  10 finger capacitive touch

image  Connects to the Raspberry Pi board using a ribbon cable connected to the DSI port

image  Adapter board is used to power the display and convert the parallel signals from the display to the serial (DSI) port on the Raspberry Pi

image  Will require the latest version of Raspbian OS to operate correctly

 

Features and Benefits

image  Turn your Raspberry Pi into a touch screen tablet, infotainment system, or standalone device.

image  Truly Interactive - the latest software drivers will support a virtual ‘on screen’ keyboard, so there is no need to plug in a keyboard and mouse.

image  Make your own ‘Internet of Things’ (IoT) devices including a visual display. Simply connect your Raspberry Pi, develop a Python script to interact with the display, and you’re ready to create your own home automation devices with touch screen capability.

image  A range of educational software and programs available on the Raspberry Pi will be touch enabled, making learning and programming easier on the Raspberry Pi.

Kit Contents

image  7” Touchscreen Display

image  Adapter Board

image  DSI Ribbon cable

image  4 x stand-offs and screws (used to mount the adapter board and Raspberry Pi board to the back of the display

image  4 x jumper wires (used to connect the power from the Adapter Board and the GPIO pins on the Pi so the 2Amp power is shared across both units)

NOTE: THE RASPBERRY PI AND POWER SUPPLY ARE NOT INCLUDED IN THIS KIT AND ARE SOLD SEPARATELY.

Compatible With:

Raspberry Pi 3 Model B

Raspberry Pi 2 Model B

Raspberry Pi Model B+

Raspberry Pi Model A+

The display will technically work with the Model A and Model B boards (connecting it to the DSI port on the Pi board), however the mounting holes on the back of the display will only line up with the newer board design (A+, B+, Pi 2 and Pi 3).

 

How to Install the Matchbox-Keyboard for your Pi

image

1. Connect a physical keyboard to the Raspberry Pi (or SSH into it if that’s your thing.)

2. Connect to the internet via WiFi or Ethernet.

3. Open the terminal.

4. Type sudo apt-get install matchbox-keyboard

5. Let the program download & install (takes 30s-1min depending on your connection.)

6. Exit the terminal & reboot your Pi.

7. The keyboard can be found by clicking the Menu -> Accessories -> Keyboard.

 

Operating System Support

In order to be sure you’re running the latest version of Raspbian, connect your Raspberry Pi to the Internet and then open LX Terminal.  Type ‘sudo apt-get update’ to download the latest version of the OS.  Once that’s complete, type ‘sudo apt-get upgrade’ to apply the download to your Raspberry Pi.  That way you’ll have all of the latest drivers and software needed to support the touch screen display.

Step 1

image

Step 2

image

Step 3

image

Step 4

image

Step 5

image

Step 6

image

Step 7

image

Step 8

image

Step 9

image
  • pi_guide
  • raspberry
  • pi
  • pi_display
  • raspberry_pi
  • matchbox_keyboard
  • display
  • touchscreen
  • 7”
  • guide
  • installation
  • 7_inches
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 9 years ago in reply to idometeor +3
    Jason Does Meteor wrote: As mentioned, I tried that. Actually you didn't, you stated: I have tried everything and I cannot get the display to rotate in Raspbian. I have written many X configuration files…
  • softweyr
    softweyr over 11 years ago in reply to ejohnfel +2
    Yeah, this is not a bad price for a 7" display, plus you get the touchscreen, integrated keyboard, etc. And tomorrow is my birthday!
  • bwelsby
    bwelsby over 11 years ago in reply to phantomski +2
    The reduced screen size is because Overscan settings are enabled. you can either comment out the settings in /boot/config.txt or just run raspi-config and select the advanced options then Overscan , Disable…
  • shabaz
    shabaz over 11 years ago in reply to e14 Contributor

    Just curious, is there a polyfuse on the board? Or is the microUSB directly wired to the 5V pin on the header?

    It could be a poor contact with the jumper cable, but I guess you've already tried to move it a bit to ensure contact. The pins will in theory support the load, but perhaps there is a fault in the contact, or the interface between the wire and the crimp. I have in the past seen some poor quality cables (from e-bay) where the wire has been incorrectly stripped, causing most of the strands of wire to have been cut. That shouldn't occur here, but nevertheless you could try swapping out the jumper cables for the power with different ones temporarily to see if it makes a difference.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    Hi, everyone. I was having power problems when I first assembled my screen (to a RP2). I tried connecting power to the lcd interface board and using a short usb cable to go from the usb out on the interface board to the RP2, but I would have the low voltage symbol constantly on the screen. I tested the voltage at the interface board input: 5VDC dead on. I then tested the voltage at the interface board output: 4.74VDC. My PS is a 5V 3A PS. So I figured a work around. I have the RP2 plugged directly into the PS and I use the GPIO pins  4 & 6 to jump to the pins on the interface board. Now RP2 has full voltage and the screen works great. AND NO MORE ANNOYING UNDERVOLTAGE SYMBOL ON SCREEN! I've used a borrowed FLIR camera for before and after pics and no hot spots show up - so should be good. I plan to eventually directly solder the wires to the pads under the pins so that I can invert the RP2 on the mounting stands for a lower profile. I am not sure why there is such a voltage drop across the interface board, but hopefully this might help someone else.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to e14 Contributor

    Hi Bruce,

     

    There may be differences (e.g. there may be reliability, quality of display differences) between the two, but I couldn't say in favour of which one (not seen the touchscreen display nor the tablet). But, I suspect "charge what the market will bear" applies too, same as most products unfortunately. (Also, I think you meant 32Gbyte Flash memory, not RAM, right?).

    There are some alternative options if you need a display for a Raspberry Pi.

    Firstly, if you are already using a PC then you can remotely control (and view) the Raspberry Pi screen from your PC (see here). Even with the 7" display the best option for general programming would still be a higher-resolution PC used remotely, or a HDMI monitor or TV and keyboard/mouse.

    Another option is a (much) smaller display such as the 2.4 inch display2.4 inch display. You won't get much text or graphics on it (and not possible to write code with it, it is too small for that) but it could be useful for some tasks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    Why is it that I can buy a cheap (but functional) 7" Chinese tablet for as little as $36 including shipping but these 7" screens cost $60 plus shipping? By the time I buy the Pi, add the screen and all of the rest of the bits & pieces I have invested at least $100. I just bought a 9.7" tablet with a HD retina screen 32Gb of ram, a 4 core Intel 64 bit processor and has android & windows 10 on it for $156 and it has an aluminum case to boot. I know that a lot of people that shop here are young tech types with well paying jobs to whom $100 is 1 less night on the town but I am a retired fixed income person who finally has some time to play with these wonderful devices but struggles to come up with the cash. Just sayin.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    I got one.  Was working great but there appears to be no reverse polarity protection.  MAKE SURE you attach your power jumpers correctly,  I fried mine.  Otherwise it is pretty slick.  Anyone know if you can by the controller card separately?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    Hi,

    I will use this display with the Raspi2 as a jukebox. So I  installed the Openelec / Kodi distribution in the latest version and works well.

    Connecting the display  => it works also without matters.

    But the touchscreen won't work in any way. Mouse and keyboard are connected via usb.

     

    Must I install a driver? How can I install the driver? Did I have the possibility to open the lx terminal?

    How can I execute the described sudo apt-get install matchbox-keyboard?

    Does there exist other way's / workarounds?

    The separate cable connection between Raspi and display are only two cables. (+5V and GND). The I²C are not connected together.

     

    thanks a lot for a good description for a non-linux user .... ;-)

     

    R.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Sorry, my English is not good.

    You can move/rotate the board for a "minimum depth" but yo need a other power cable for the Pi.

    PiDisp3.JPG

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    what that means???

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Och nöö... oczko.gif

    Use this direction...

    PiDisp_u.JPG

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    My first try...

    Kiste1.JPG

    Kiste2.JPG

    Kiste3.JPG

    Any things to do but I missing additional technical information. No RISC OS lobby here oczko.gif

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>