RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Review Blogs Arduino nano r4 review
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: neerajrd82
  • Date Created: 11 Apr 2026 5:31 AM Date Created
  • Views 2322 views
  • Likes 9 likes
  • Comments 13 comments
Related
Recommended
  • RoadTest
  • cortex-m4
  • nano r4
  • arduino ide
  • arduino_projects
  • review
  • arm keil mdk

Arduino nano r4 review

neerajrd82
neerajrd82
11 Apr 2026

Section: Unboxing, Initial Setup & Failure Analysis – Arduino Nano R4

image

1. Unboxing & First Impressions

The Arduino Nano R4 was received in standard Arduino packaging with the board securely enclosed in an anti-static cover.

Package Contents:

  • Arduino Nano R4 board
  • Berg strip headers (unsoldered)

Initial Observations:

  • Compact Nano form factor retained
  • High-quality PCB finish
  • Clearly labeled pinout
  • USB Type-C interface for modern connectivity

The inclusion of unsoldered headers allows flexibility depending on application (breadboard vs embedded use).

2. Header Soldering Procedure

To prepare the board for testing, the supplied Berg strip headers were manually soldered.

Tools Used:

  • Temperature-controlled soldering iron
  • Lead-free solder wire
  • Flux (for clean joints)

Procedure Followed:

  1. Headers were aligned with PCB through-holes
  2. Board was placed on a flat surface to maintain perpendicular alignment
  3. Each pin was soldered carefully to ensure:
    • Proper wetting
    • No cold joints
    • No bridging between adjacent pins

image

Result:

  • Clean and mechanically stable solder joints
  • Board ready for breadboard and test setup integration



3. Initial Power-Up & Arduino IDE Detection

After soldering, the board was connected to the system using a USB Type-C cable.

Expected Behavior:

  • Automatic USB detection
  • COM port visibility in Arduino IDE
  • Board ready for programming

Observed Symptoms:

  •  No COM port visible in Arduino IDE
  •  Device shown as “Unknown USB Device” in Windows Device Manager
  •  Upload attempts failed completely
  •  No LED indication of bootloader activity

 At this stage, the board appeared non-functional and inaccessible

4. Initial Diagnosis Using Community Reference

To investigate the issue, the following troubleshooting resource was referred:

  • Element14 Community guide on USB detection issues on this link: 
    https://community.element14.com/products/arduino/b/blog/posts/arduino-uno-r4-minima-troubleshooting-unknown-usb-device

Key Insight:

  • USB failure is commonly caused by:
    • Improper firmware initialization
    • Clock misconfiguration
    • Bootloader not executing

Engineering Interpretation:

Since USB depends on correct timing:

Any misconfiguration in system clock or startup code can completely disable USB communication.

5. Attempt to Restore Bootloader Mode

Method Used:

  • Double-press reset button to force bootloader entry

Expected Outcome:

  • Board should enumerate as a valid USB device
  • COM port should reappear

Actual Result:

  •  Bootloader entry was inconsistent
  •  USB remained unstable or undetected

6. Bootloader Recovery Attempt Using Official Procedure

Next, the official Arduino recovery guide was followed:

  • Arduino Nano R4 Bootloader Flashing Procedure on given link: https://docs.arduino.cc/tutorials/nano-r4/bootloader-flashing/

Intended Goal:

  • Reprogram bootloader
  • Restore USB functionality
  • Re-enable Arduino IDE connectivity

7. Practical Challenges Encountered

 No Active Communication Interface

  • USB stack was non-functional
  • No serial interface available

 Result:

  • Bootloader flashing could not proceed

 Limited Hardware Access

  • No exposed SPI/ISP interface (unlike classic Arduino)
  • SWD/JTAG not readily accessible

 This prevented low-level recovery

 Documentation Limitations

The official guide assumes:

  • Functional USB connection
  • Arduino IDE workflow

It does not fully address:

  • Bare-metal firmware corruption
  • Complete USB failure scenarios

8. Root Cause Analysis

Based on experimentation, the failure was attributed to:

 Clock Misconfiguration

  • Incorrect system clock setup disrupted USB timing

 Bootloader Interference

  • Custom firmware may have overridden bootloader execution

 USB Stack Failure

  • USB requires precise timing → deviation leads to “Unknown Device”

9. Key Engineering Insight

The Arduino Nano R4 behaves like a professional MCU platform, but without equivalent recovery infrastructure.

Parameter Observation
USB dependency High
Recovery ease Limited
Bare-metal tolerance Sensitive
Debug accessibility Restricted

10. Lessons Learned For those Engineers who use Arduino IDE without any other options: 

  • Avoid modifying critical startup configuration without validation
  • Preserve bootloader region
  • Maintain backup firmware


11. Switching over to SWD debug access to recover the target chip R7FA4M1AB3CFM mounted on Arduino Nano R4 board:  

Now, i would like to refer to official schematics of Arduino Nano R4 given on this link: 
https://docs.arduino.cc/resources/schematics/ABX00142-schematics.pdf

image
Here are 3 important observations about above picture are given below required for SWD bebug access: 

1. MD pin of MCU given on JP1 connector pin no 13. -> This pin should be connected with SWCLK pin of debugger.

2. RESET pin of MCU given on JP2 connector pin no 3. -> This pin should be connected with RESET pin of debugger.  

3. VUSB pin of MCU given on JP1 connector pin no 12 -> This pin should be given +5VDC from debugger USB power supply.  
image

Here are some important observations about above picture are given below required for SWD bebug access: 

1. P108_SWDIO & P300_SWCLK are required to connected with any compatible debugger -> Jlink / CMSIS-DAP / Renesas made Emulator  

2. Very-very important point :  P300_SWCLK & MD pin of MCU given on JP1 connector pin no 13 should be shorted with each other & connected to SWCLK line from debugger side.  

Again by chance, i already possess this evaluation kit made by renesas: 

image  

This board already have onboard Jlink OB lite debugger mounted on this kit. So, i decided to connect this debugger to Arduino Nano r4 while totally disconnecting on board target chip. 

Now, referring to schematics of this kit which are found in ek-ra2l1-v1-designpackage.zip , these are important points everybody needs to consider for connections given below: 

Please! download ek-ra2l1-v1-designpackage.zip from Renesas website.

Now, given below is important section of debugger to get connected with external target chip  

 


image 

Important Note: all jumpers shown in this diagram needs to taken out totally, to cut off the onboard target chip for debugger connections.

 image

J13 connector shown above is not populated in actual kit, so all the connector pads are exposed which were directly soldered for debugger connection with Arduino Nano r4 board. 

image

In above picture, 5V power supply can be easily seen which was connected with Arduino Nano R4 board to get power up using debugger USB power supply. 

J-link Commander after getting correct connection from debugger will give below message corresponding to Arduino Nano R4 board:  

Device "R7FA4M1AB" selected.

Connecting to target via SWD
InitTarget() start
Identifying target device...
SWD selected. Executing JTAG -> SWD switching sequence...
Initializing DAP...
DAP initialized successfully.
Low power mode detected. Waking device from low power mode.
InitTarget() end - Took 14.5ms
Found SW-DP with ID 0x5BA02477
DPIDR: 0x5BA02477
CoreSight SoC-400 or earlier
Scanning AP map to find all available APs
AP[2]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x24770011, ADDR: 0x00000000)
AP[1]: APB-AP (IDR: 0x44770002, ADDR: 0x01000000)
Iterating through AP map to find AHB-AP to use
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FF000
CPUID register: 0x410FC241. Implementer code: 0x41 (ARM)
Found Cortex-M4 r0p1, Little endian.
FPUnit: 6 code (BP) slots and 2 literal slots
CoreSight components:
ROMTbl[0] @ E00FF000
[0][0]: E000E000 CID B105E00D PID 000BB00C SCS-M7
[0][1]: E0001000 CID B105E00D PID 003BB002 DWT
[0][2]: E0002000 CID B105E00D PID 002BB003 FPB
[0][3]: E0000000 CID B105E00D PID 003BB001 ITM
[0][4]: E0040000 CID B105900D PID 000BB9A1 TPIU
[0][5]: E0041000 CID B105900D PID 000BB925 ETM
[0][6]: E0042000 CID B105900D PID 002BB908 CSTF
[0][7]: E0043000 CID B105900D PID 001BB961 TMC
[0][8]: E0044000 CID B105F00D PID 001BB101 TSG
Memory zones:
Zone: "Default" Description: Default access mode
Cortex-M4 identified.

So, SEGGER J-FLASH LITE was able to program Arduino Nano r4 board successfully, below picture demonstrates that:  


 image

So, SEGGER J-FLASH LITE was able to erase Arduino Nano r4 board successfully, below picture demonstrates that:  

image

 

I m showing the picture of actual physical connections with debugger & Arduino Nano R4 board given below: 
 

image


Important observation noted: I was able to recover original preloaded program which was actually loaded in Arduino Nano R4 at time of arrival using jlink debugger. 

12. Switching over the development of  target chip R7FA4M1AB3CFM mounted on Arduino Nano R4 board from Arduino IDE into Keil MDK ARM :  

Here you have to use Renesas smart configurator with Output configured for Keil MDK ARM.

Select the clock settings given below in Renesas smart configurator in given screenshot: 

image

Select Board : Custom User board (Any Device) as shown in screenshot given below: 

image

Pin function select is shown in given screenshot :


image

BSP options are shown in  below screenshot:

image

In bsp options, just select bare metal & No RTOS to include. Also select "Generate Project option" option to generate Blinky program in this configurator as shown below:

image

Below given picture demonstrates the output given by Renesas smart configurator for Keil MDK ARM: 

 image

To run this program correctly, Please! do the following steps: 

Search & comment  this line given below: 

FSP_HARDWARE_REGISTER_WAIT(R_RTC->RCR2_b.RESET, 0);   -> This line is found in bsp_clocks.c

Important observation: Debugger gets stuck on above line. 

Update on 31/03/2026: 

Keil screenshot on C/C++ tab: 

image

Keil screenshot on Asm tab:

image
 

Keil screenshot on Linker tab:

image

Configure the below settings in Flash download of keil as shown screenshot given below: 

image 

Apply the above settings, then follow the below given steps:


Generate the hex file.

Completely erase the chip.

Then program the chip using download button in keil.

Expected result: You should be able to RGB LED as single white LED glowing brightly but without blinking.

Now, after resolving settings issues, renesas flash programmer is also working, screenshots are given below: 

image

Programming messages by Renesas Flash Programmer are given below: 

Loading File (E:\Arduino-nano-r4\led.hex) CRC-32=8D56F9F1

Target device : RA

Connecting the tool
J-Link Firmware: J-Link OB-S124 compiled Dec 10 2025 15:52:46
Tool : J-Link (SEGGER J-Link-OB-S124), Interface : SWD
Connecting to the target device
Connecting to the target device
Communication speed : 6.0 MHz
Signature:
Device: RA
Device Code: 00160447

Erasing the selected blocks
[Code Flash 1] 0x00000000 - 0x0003FFFF size : 256 K
[Data Flash 1] 0x40100000 - 0x40101FFF size : 8 K

Erasing the selected blocks
[Code Flash 1] 0x00000000 - 0x0003FFFF size : 256 K
[Data Flash 1] 0x40100000 - 0x40101FFF size : 8 K

Writing data to the target device
[Code Flash 1] 0x00000000 - 0x0003FFFF size : 256 K
[Data Flash 1] 0x40100000 - 0x40101FFF size : 8 K
[Config Area 1] 0x01010008 - 0x01010033 size : 44

Verifying data
[Code Flash 1] 0x00000000 - 0x0003FFFF size : 256 K
[Data Flash 1] 0x40100000 - 0x40101FFF size : 8 K
[Config Area 1] 0x01010008 - 0x01010033 size : 44
Setting the target device

Disconnecting the tool
Operation completed.

Important observation: This tool should be used to production programming rather than for development.   

 

13. Build the whole project in keil bypassing Renesas smart configurator   

 If you do not want to use code generated by Renesas smart configurator -> then it is still long learning curve, but some how i managed to reduce the number of files to taken from smart configurator & managed to write in register direct format. Also i have followed the steps given just above this section.

End result of above exercise is shown below screenshot: 

image    

Of course, result was fabulous: I was able to blink RGB LED & AMBER LED independently bypassing the HAL library as mandated by Renesas.


What other parts i should consider comparable to this product?

Ans: STM32F373CCT6,MK40DX256VLK10,ATSAM4LC8C,EFM32GG11B420F2048GL64


What were the biggest problems encountered?

Complete USB failure – Board not detected (no COM port), blocking normal development via Arduino IDE
Ineffective standard recovery methods – Bootloader reset and typical Arduino fixes did not work
Complex root cause – Clock misconfiguration impacting USB initialization required deep MCU-level analysis
Limited low-level documentation – Insufficient clarity on register-level configuration and clock dependencies for debugging such failures
Shift to hardware-level debugging – Required use of SWD + J-Link, full chip erase, and reflash to recover the system

Final Verdict: 

When the Arduino Nano R4 loses USB functionality due to low-level firmware issues, recovery becomes complex and not be achievable using standard Arduino tools alone.

It requires the assistance of JLINK/ CMSIS DAP / Renesas EMULATOR to recover from all types of firmware issues.

Also this board requires the erase of whole chip to prevent the hang-up. 

The Arduino Nano R4 delivers powerful Renesas-based performance, but its recovery mechanisms need significant improvement to support advanced embedded development workflows.

Renesas flash programmer is not reliable at all, it does not connect with Jlink reliably to sense the chip. 

There is steep learning curve for bare metal development on register direct access bypassing HAL layer by Renesas.

Renesas needs to improve on all these parameters. 

MY SINCERE THANKS FOR ELEMENT 14 Community to give me to chance to test the arduino nano R4 board.   

  • Sign in to reply

Top Comments

  • shabaz
    shabaz 7 months ago +3
    Hi, Just to be clear: The section 8 "Root cause analysis" refers to: Clock Misconfiguration / Bootloader Interference / USB Stack Failure but how could it have been any of those, unless Arduino shipped…
  • dougw
    dougw 7 months ago +2
    Yikes. I am about to fire up my Nano R4. I'll let you know if it fares better.
  • neerajrd82
    neerajrd82 7 months ago in reply to misaz +1
    Dear misaz, you can refer the schematics of ek-ra2l1 using ek-ra2l1-v1-designpackage.zip. I have already shown that renesas designed debug section where by default MD pin was shorted with SWDCLK using…
  • neerajrd82
    neerajrd82 7 months ago in reply to shabaz

    Hi shabaz, 
                     long time, no news. I m not saying that : Arduino shipped it with the incorrect firmware or no firmware. I m trying to convey that firmware shipped is not stable enough to give you the access of USB to serial which is required to give the access of re-programming using arduino IDE. Even i have tried to burn "dfu-nano.hex" using SWD debugger using mentioned procedure but still this firmware was not working correctly at all to give access for arduino IDE. Moreover, tried to re-program several times using arduino IDE but it failed miserably several times. that is why this has to be written clearly that it is ARM based chip so the development is going to very complicated as absence of ecosystem by Arduino if any thing goes bad.      

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 7 months ago

    Hi,

    Just to be clear: The section 8 "Root cause analysis" refers to:

    Clock Misconfiguration / Bootloader Interference / USB Stack Failure

    but how could it have been any of those, unless Arduino shipped it with the incorrect firmware or no firmware?

    Is that the case, or is there something missing in the review (i.e. was the board firmware modified by you?). I think it's important to know, because all the rest of the review refers to a far more complicated method of working with that board, rather than using the Arduino IDE. I know you were fine using the more complicated method, but most users will expect (and want) to use the Arduino IDE with the Arduino board. Any clarification would be great. I would want to know, if I buy that board, will it come with the Arduino firmware installed or not (I likely will not care if I can re-upload it provided it's robust and not easily corrupted, but that for sure is good to know too, but that's a separate issue).

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • misaz
    misaz 7 months ago

    Shorting MD and SWDCLK does not seem right to me. It may work by accident though. MD is like BOOT0 on STM32s. Theare are two bootloaders on Arduino Nano R4. One is baked in the MCU and is triggered by MD pin at power up time. Second is Arduino bootloader is stored in flash memory and is triggered by two reset presses or whatever they use nowadays. It is not clear if "Unknown Device" come from Arduino bootloader (I guess) or Renesas baked bootloader which I would expect behave as standard USB DFU class. I think if you recover it by connecting MD pin to GND instead of SWDCLK, you were able to recover or flash new program directly over onboard USB using Renesas tooling without need of any soldering. But I do not have this board, so can't verify.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neerajrd82
    neerajrd82 7 months ago in reply to robogary

    Arduino Nano R4 is was not brain dead on arrival with no chance of recovery. preloaded program inside Arduino Nano R4 worked correctly but denied the access the USB to serial due to which COM port access was blocking & i m unable to use Renesas Flash programmer with this board. Only possible way to recover is SWD debugger connections with software configuration has been discussed already above.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neerajrd82
    neerajrd82 7 months ago in reply to robogary

    sorry! you interpretation of failure was incorrect. i have already said in given above review that preloaded program was working correctly but that program was not giving the access of USD to Serial , due to which i was not able to use Renesas flash programmer correctly. Again it was recover only by use of SWD debugger.    

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>