RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs Elegant and Robust Capacitive Touch Interfaces - Part 3 - Uploading new code
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: Workshopshed
  • Date Created: 23 Jul 2016 11:25 PM Date Created
  • Views 568 views
  • Likes 5 likes
  • Comments 1 comment
Related
Recommended

Elegant and Robust Capacitive Touch Interfaces - Part 3 - Uploading new code

Workshopshed
Workshopshed
23 Jul 2016

As mentioned at the end of part 2, I've installed Code Composer Studio so that I can upload new code to the development board. following the workshop guide the first step is to generate some code from design studio and import it into CCS. This works fine as long as you don't generate your code into the CCS workstation folder as it will be making a copy of it there.

image

You can then "Debug" the code to compile and upload it. This may take a few moments the first time as there are some libraries to compile.

I was prompted to upgrade my firmware. I did so and this went smoothly.

image

Eventually you get into the debugger, and you could step through your code at this point. However for the workshop instructions it's just a case of running the code to see the board in action.

image

It turned out that I did not need to generate the code, in fact for the proximity demo that did not work and the correct procedure was to import the project directly from the design centre folders. This is a fun demo as it has lights so you can see the interaction. I also tested this one with a glove which gave me a bit more confidence that my glove and overlay tests would work later in the roadtest.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The final demo project is the "phone" demo, this has a haptic feedback and demonstrates how it's possible to cram loads of sensors into one board. This is done with mutual capacitance of adjacent sensors. You can see how TI has built this board by looking on the back.

  imageimage

 

Next up, I'm going to look at how the technology works with different overlay materials and gloves. So I've reverted the board back to the out of the box code and will look at tuning the settings.

  • Sign in to reply

Top Comments

  • DAB
    DAB over 10 years ago +2
    Very good post. TI continues to impress me with the software and hardware integration they do before they ship the new devices. DAB
  • DAB
    DAB over 10 years ago

    Very good post.

     

    TI continues to impress me with the software and hardware integration they do before they ship the new devices.

     

    DAB