RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs Introduction of the B&K Precision DAS60 High Speed Multi-Function Recorder - unboxing
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: john.porter
  • Date Created: 5 Aug 2024 11:37 PM Date Created
  • Views 1039 views
  • Likes 11 likes
  • Comments 3 comments
Related
Recommended
  • RoadTest
  • sefram
  • recorder
  • data acquisition
  • bk precision
  • high speed
  • road test
  • DAS60

Introduction of the B&K Precision DAS60 High Speed Multi-Function Recorder - unboxing

john.porter
john.porter
5 Aug 2024
Introduction of the B&K Precision DAS60 High Speed Multi-Function Recorder - unboxing

image

B&K Precision DAS60 High Speed Multi-Function Recorder

The B&K Precision DAS60 is the top model in the High-Speed Multi-Function Recorder category and positioned for applications in research, development, maintenance, and power monitoring. I am thrilled to be selected as a road tester for this review and extend my thanks to Element 14 and B&K Precision for the opportunity!

At the most basic level, any Data Acquisition System (DAS) will measure samples of real-world signals, convert analog signals to digital format, then store or present the results to a user or a computer for analysis. A DAS can record multiple inputs for lengthy periods of time, which allows infrequent events to be captured, analyzed and compared to each other within a single instrument and the same time base. A practical example could be to monitor and record how an EV battery source is impacted by speed, driver use, temperature and other environmental factors at an instance in time. However, the B&K Precision DAS60 is not just any DAS. This model promises significant capability and speed:


• 6 isolated analog input channels with an input range from as low as +/- 5mv to +/- 500V rated for CAT III
• 16 logic inputs
• 2 dedicated platinum RTD temperature inputs (Pt100/1000)
• 4 outputs for alarms or external trigger
• 1MSa/s/channel sampling to memory, 500KSa/s/channel to file. 14-bit resolution
• Power analysis for single phase or three phase power sources, Fresnel diagram and harmonic distortion displays
• 10” TFT touchscreen LCD
• Custom filters and triggers
• Digital Numeric or Oscilloscope views
• Portable with battery life up to 9.5 hours
• Network connectivity


Unboxing the B&K Precision DAS60

The B&K Precision DAS60 ships in a rugged carrying case with custom fitted foam inserts securing the equipment inside:


• 1 B&K Precision DAS60
• 1 AC mains adapter 100 / 240 V
• 6 pair CAT III banana test leads with alligator clips
• 6 pair CAT II banana adapters for bare wire
• 1 DB25 pin male connector
• Pen/stylus
• Calibration certificate & test reports


The DAS60 promises exciting functionality. Getting up and running is intuitive and straightforward, I was able to get started easily. My first impressions are that this is a rugged, capable instrument – I couldn’t wait to get started and my review is well underway. For the interim I wanted to share my initial experience through an unboxing video.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

This concludes my brief introduction of the B&K Precision DAS60 High Speed Multi-Function Recorder. More to come along with my review. Please leave me a comment if you have any questions or requests!

{gallery}DAS 60 unboxing

image

DAS 60 panel

imageDAS60 Front

image

DAS60 In box

imageDAS60 Case

image

DAS60 Home Screen

image

DAS60 Alligator-Banana leads

image

DAS60 Banana - Bare Wire adapters

image

DAS60 DB25 Male adapter

image

DAS60 Terminal blocks

image

  • Sign in to reply
  • john.porter
    john.porter over 2 years ago in reply to kmikemoo

    It is portable but will not fit in my pocket, I confirmed this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kmikemoo
    kmikemoo over 2 years ago

    I wasn't able to gage the size of the unit until your video.  It's bigger than I imagined.  I like the case also.  Transit to and from the site is where a lot of stuff gets broke.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 2 years ago

    I was tempted to apply to test this device, so I am looking forward to your reports.