RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Review Blogs Keithley 2450: Battery characterization
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: neuromodulator
  • Date Created: 16 Jul 2020 2:45 PM Date Created
  • Views 2340 views
  • Likes 4 likes
  • Comments 5 comments
Related
Recommended

Keithley 2450: Battery characterization

neuromodulator
neuromodulator
16 Jul 2020

3.2 Battery Characterization

 

Battery selection for a specific application can depend on multiple factors: price, size, weight, safety and its electrical properties. Manufacturers are known for making dubious claims about their batteries lifetime and capacity, so the proper way to evaluate a battery is to characterize it.

 

Batteries are complex electrochemical devices that do not behave as constant voltage sources (Figure A). Their terminal voltage depends on the amount of charge in the battery, its temperature and the dynamics of the current being drawn. There are models of different levels of complexity that can simulate their behavior. A state of charge dependent voltage source model (Figure B) can simulate the voltage drop caused by the loss of battery charge. To simulate how the current causes a voltage drop at the terminals (Vt) a series resistor (Rs) needs to be added (Figure C). A current surge can drop Vt in non-series-resistor way, where Vt would slowly increase the voltage after the battery gets unloaded, to simulate that, an RC block needs to be added to the model (Figure D). Models can of course get much more complex, and can model self-discharge, temperature-dependence, or even the battery cell electrochemical dynamics.

 

Keithley provides a TSP script (Model generation script) to measure the Voc (open-circuit voltage) and equivalent series resistance (ESR) as the battery discharges. The generated data can then be used to create a battery model (Figure C) that can be used by the Keithley 2281S Battery simulator.

 

image

 

 

I decided to test the script with a 18650 Lithium battery and then plot the Voc, Vload and ESR (Rs) curves to see how they depend on the amount of charge of the battery.

 

image

 

 

The script requires to enter the "discharge current", which I set to 1 A, the cut-off voltage, which I set to 3 V, and the ESR measuring interval, which I set to 10 s. The script discharges the battery at constant current and measures the voltage (Vload), it periodically interrupts the discharge (sets the discharge current to 0 A) and measures the open circuit voltage (Voc). The ESR can then be derived as ESR = (Voc - Vload) / Idischarge. While the script discharges the battery it displays the elapsed time, the Voc, the Vload and the ESR.

 

image

 

 

After 2 hours the battery Vload hit the cut-off voltage, the discharge stopped and the data got saved into an USB drive. The script generated 2 files, one contains the raw data, and the other the battery model that can be used by the Keithley 2281S battery simulator.

 

The raw file contained:

 

TEST_PARAM.comment:,18650

SourceMeter Model:,2450
SourceMeter S/N:,00000000
SourceMeter Firmware:,1.7.1e

TEST_PARAM.terminals:,FRONT TERMINALS

TEST_PARAM.initial_voc:,4.1914849281
TEST_PARAM.vcutoff:,3

TEST_PARAM.discharge_type:,CONSTANT
TEST_PARAM.discharge_current:,1
TEST_PARAM.max_discharge_current:,1

TEST_PARAM.measure_interval:,10

TEST_PARAM.discharge_start_time:,07/03/20 14:51:05
TEST_PARAM.discharge_stop_time:,07/03/20 16:59:55

BATT_MODEL_RAW:,Index,Timestamp,Voc,Vload,ESR
BATT_MODEL_RAW:,1,0.04147066,4.1869735718,3.9285964966,0.2583770752
BATT_MODEL_RAW:,2,10.04163994,4.1751747131,3.9447231293,0.23045158386
BATT_MODEL_RAW:,3,20.04195438,4.1686229706,3.95063591,0.21798706055
BATT_MODEL_RAW:,4,30.04289712,4.1635017395,3.9475860596,0.21591567993
BATT_MODEL_RAW:,5,40.04404116,4.1592350006,3.9434394836,0.21579551697
BATT_MODEL_RAW:,6,50.04481626,4.1554431915,3.9393730164,0.21607017517
BATT_MODEL_RAW:,7,60.04562628,4.152048111,3.9423675537,0.20968055725
BATT_MODEL_RAW:,8,70.04634302,4.1489944458,3.9473381042,0.20165634155
BATT_MODEL_RAW:,9,80.04716334,4.1461925507,3.9474830627,0.19870948792
BATT_MODEL_RAW:,10,90.04737856,4.1436023712,3.9476509094,0.19595146179
BATT_MODEL_RAW:,11,100.04829772,4.1411247253,3.9458198547,0.19530487061
BATT_MODEL_RAW:,12,110.04906084,4.1387672424,3.9439659119,0.19480133057
BATT_MODEL_RAW:,13,120.05018826,4.1364307404,3.9417533875,0.19467735291
BATT_MODEL_RAW:,14,130.05060916,4.1343212128,3.9396514893,0.19466972351
BATT_MODEL_RAW:,15,140.05131596,4.1321258545,3.9372825623,0.19484329224
BATT_MODEL_RAW:,16,150.05158634,4.1300601959,3.936498642,0.19356155396
BATT_MODEL_RAW:,17,160.05184474,4.1280403137,3.9346523285,0.19338798523
BATT_MODEL_RAW:,18,170.05213434,4.126077652,3.9331703186,0.19290733337
BATT_MODEL_RAW:,19,180.05308966,4.1241550446,3.9298915863,0.19426345825
BATT_MODEL_RAW:,20,190.0534611,4.1222476959,3.926448822,0.1957988739
BATT_MODEL_RAW:,21,200.05388696,4.1203632355,3.9248046875,0.19555854797
BATT_MODEL_RAW:,22,210.05503024,4.1184978485,3.9234809875,0.19501686096
BATT_MODEL_RAW:,23,220.05631474,4.1166706085,3.9226894379,0.19398117065
BATT_MODEL_RAW:,24,230.05749754,4.1148509979,3.9226436615,0.19220733643
BATT_MODEL_RAW:,25,240.05781516,4.1130599976,3.9208621979,0.19219779968
BATT_MODEL_RAW:,26,250.05833834,4.1112728119,3.920091629,0.19118118286
BATT_MODEL_RAW:,27,260.0593152,4.1094818115,3.9175071716,0.19197463989
BATT_MODEL_RAW:,28,270.0603908,4.1077346802,3.9156265259,0.1921081543
BATT_MODEL_RAW:,29,280.06080194,4.1059894562,3.9137516022,0.192237854
BATT_MODEL_RAW:,30,290.06188338,4.1043128967,3.912569046,0.19174385071
BATT_MODEL_RAW:,31,300.0624175,4.1025085449,3.9104347229,0.19207382202
BATT_MODEL_RAW:,32,310.06318338,4.1007957458,3.9093151093,0.1914806366
BATT_MODEL_RAW:,33,320.06411186,4.0991306305,3.9074039459,0.19172668457
BATT_MODEL_RAW:,34,330.06466198,4.0974674225,3.9059638977,0.19150352478
BATT_MODEL_RAW:,35,340.06544256,4.095664978,3.9031410217,0.1925239563
BATT_MODEL_RAW:,36,350.06640894,4.0939750671,3.9018592834,0.19211578369
BATT_MODEL_RAW:,37,360.06768308,4.0922851563,3.9014205933,0.19086456299
BATT_MODEL_RAW:,38,370.0684368,4.090593338,3.9005413055,0.19005203247
BATT_MODEL_RAW:,39,380.06939068,4.0889205933,3.8992424011,0.18967819214
BATT_MODEL_RAW:,40,390.0699098,4.087266922,3.8982963562,0.1889705658
BATT_MODEL_RAW:,41,400.0707351,4.0855998993,3.8961029053,0.18949699402
BATT_MODEL_RAW:,42,410.07173234,4.0839252472,3.8947887421,0.18913650513
BATT_MODEL_RAW:,43,420.0728917,4.0823402405,3.8938293457,0.18851089478
BATT_MODEL_RAW:,44,430.0740412,4.0806236267,3.8922767639,0.18834686279
BATT_MODEL_RAW:,45,440.07472052,4.0790958405,3.891450882,0.1876449585
BATT_MODEL_RAW:,46,450.07591266,4.077419281,3.8901176453,0.18730163574
BATT_MODEL_RAW:,47,460.07613942,4.0756912231,3.8884849548,0.18720626831
BATT_MODEL_RAW:,48,470.07655048,4.0740585327,3.8873233795,0.1867351532
BATT_MODEL_RAW:,49,480.077216,4.072429657,3.8861198425,0.18630981445
BATT_MODEL_RAW:,50,490.07836948,4.0707969666,3.8853988647,0.18539810181
BATT_MODEL_RAW:,51,500.07951396,4.0691661835,3.8834381104,0.18572807312
BATT_MODEL_RAW:,52,510.08071844,4.0675601959,3.8822154999,0.18534469604
BATT_MODEL_RAW:,53,520.08164934,4.0660209656,3.8811225891,0.18489837646
BATT_MODEL_RAW:,54,530.0820863,4.0643215179,3.8794879913,0.18483352661
BATT_MODEL_RAW:,55,540.08262132,4.0627784729,3.8778133392,0.18496513367
BATT_MODEL_RAW:,56,550.0829232,4.0610961914,3.8764457703,0.18465042114
BATT_MODEL_RAW:,57,560.08408718,4.0595207214,3.8741149902,0.1854057312
BATT_MODEL_RAW:,58,570.08443458,4.0579013824,3.8733024597,0.18459892273
BATT_MODEL_RAW:,59,580.08536182,4.056312561,3.8713855743,0.18492698669
BATT_MODEL_RAW:,60,590.08609158,4.0547657013,3.8690624237,0.18570327759
BATT_MODEL_RAW:,61,600.08653976,4.0531101227,3.8673934937,0.18571662903
BATT_MODEL_RAW:,62,610.0871543,4.0515365601,3.865278244,0.18625831604
BATT_MODEL_RAW:,63,620.08754322,4.0499191284,3.8636035919,0.1863155365
BATT_MODEL_RAW:,64,630.08857226,4.0483283997,3.8625564575,0.18577194214
BATT_MODEL_RAW:,65,640.08880142,4.0467281342,3.8617916107,0.18493652344
BATT_MODEL_RAW:,66,650.08967788,4.0451526642,3.8603630066,0.18478965759
BATT_MODEL_RAW:,67,660.0898926,4.0435619354,3.8579826355,0.18557929993
BATT_MODEL_RAW:,68,670.09032444,4.0420742035,3.8564109802,0.18566322327
BATT_MODEL_RAW:,69,680.09136604,4.0404052734,3.8535423279,0.18686294556
BATT_MODEL_RAW:,70,690.09251666,4.0388336182,3.8519935608,0.18684005737
BATT_MODEL_RAW:,71,700.09357694,4.0372390747,3.8506469727,0.18659210205
BATT_MODEL_RAW:,72,710.09374676,4.0356769562,3.8489055634,0.18677139282
BATT_MODEL_RAW:,73,720.09436664,4.0340900421,3.847776413,0.18631362915
BATT_MODEL_RAW:,74,730.09489284,4.0325222015,3.8453083038,0.18721389771
BATT_MODEL_RAW:,75,740.09512284,4.0309562683,3.8430805206,0.18787574768
BATT_MODEL_RAW:,76,750.09547364,4.0293865204,3.8409404755,0.18844604492
BATT_MODEL_RAW:,77,760.0957287,4.0278129578,3.8394374847,0.18837547302
BATT_MODEL_RAW:,78,770.09605106,4.0262413025,3.8378829956,0.18835830688
BATT_MODEL_RAW:,79,780.09676726,4.0246906281,3.8364315033,0.18825912476
BATT_MODEL_RAW:,80,790.09745016,4.0231246948,3.834695816,0.18842887878
BATT_MODEL_RAW:,81,800.09769716,4.0215606689,3.8330345154,0.18852615356
BATT_MODEL_RAW:,82,810.09877796,4.0199985504,3.8322944641,0.1877040863
BATT_MODEL_RAW:,83,820.09914636,4.0184364319,3.830575943,0.18786048889
BATT_MODEL_RAW:,84,830.10033254,4.0168972015,3.8287315369,0.18816566467
BATT_MODEL_RAW:,85,840.10115234,4.0154285431,3.8272895813,0.18813896179
BATT_MODEL_RAW:,86,850.10185282,4.0137844086,3.8256187439,0.18816566467
BATT_MODEL_RAW:,87,860.10310216,4.0122375488,3.824131012,0.18810653687
BATT_MODEL_RAW:,88,870.10353326,4.0107707977,3.8224773407,0.18829345703
BATT_MODEL_RAW:,89,880.1042103,4.0092277527,3.8204059601,0.1888217926
BATT_MODEL_RAW:,90,890.1049132,4.0075931549,3.8183097839,0.18928337097
BATT_MODEL_RAW:,91,900.10536854,4.0060634613,3.8167266846,0.18933677673
BATT_MODEL_RAW:,92,910.10577336,4.0045070648,3.8143558502,0.1901512146
BATT_MODEL_RAW:,93,920.10594378,4.0029888153,3.8127250671,0.19026374817
BATT_MODEL_RAW:,94,930.10671694,4.0014419556,3.810968399,0.19047355652
BATT_MODEL_RAW:,95,940.10749688,3.9999008179,3.8080291748,0.19187164307
BATT_MODEL_RAW:,96,950.10857836,3.9983634949,3.807434082,0.19092941284
BATT_MODEL_RAW:,97,960.10967274,3.9968776703,3.8045711517,0.19230651855
BATT_MODEL_RAW:,98,970.109892,3.9952888489,3.8034439087,0.19184494019
BATT_MODEL_RAW:,99,980.1100553,3.9937648773,3.8020019531,0.19176292419
BATT_MODEL_RAW:,100,990.11088666,3.9922351837,3.8001651764,0.19207000732
BATT_MODEL_RAW:,101,1000.1117395,3.9907302856,3.7987918854,0.19193840027
BATT_MODEL_RAW:,102,1010.1124241,3.9891777039,3.7963638306,0.19281387329
BATT_MODEL_RAW:,103,1020.1135547,3.9877262115,3.7955436707,0.19218254089
BATT_MODEL_RAW:,104,1030.1141527,3.98620224,3.7940273285,0.1921749115
BATT_MODEL_RAW:,105,1040.1151561,3.9846115112,3.7928466797,0.19176483154
BATT_MODEL_RAW:,106,1050.11618,3.9830970764,3.7920207977,0.19107627869
BATT_MODEL_RAW:,107,1060.1167876,3.9815921783,3.7915115356,0.1900806427
BATT_MODEL_RAW:,108,1070.1170712,3.9800548553,3.7903270721,0.1897277832
BATT_MODEL_RAW:,109,1080.1175484,3.9785480499,3.7892799377,0.18926811218
BATT_MODEL_RAW:,110,1090.1185612,3.977142334,3.788766861,0.18837547302
BATT_MODEL_RAW:,111,1100.1190314,3.9755172729,3.7872276306,0.18828964233
BATT_MODEL_RAW:,112,1110.1193551,3.9740009308,3.7857551575,0.18824577332
BATT_MODEL_RAW:,113,1120.1199989,3.9725952148,3.7842998505,0.18829536438
BATT_MODEL_RAW:,114,1130.1205544,3.9710845947,3.7828826904,0.1882019043
BATT_MODEL_RAW:,115,1140.1208792,3.9694786072,3.7810077667,0.18847084045
BATT_MODEL_RAW:,116,1150.1211314,3.9679832458,3.779542923,0.18844032288
BATT_MODEL_RAW:,117,1160.1214676,3.9664745331,3.7780456543,0.18842887878
BATT_MODEL_RAW:,118,1170.1216419,3.9649734497,3.7767448425,0.18822860718
BATT_MODEL_RAW:,119,1180.1220134,3.963476181,3.7755413055,0.18793487549
BATT_MODEL_RAW:,120,1190.1231267,3.9619827271,3.7740383148,0.18794441223
BATT_MODEL_RAW:,121,1200.1237663,3.960483551,3.772310257,0.18817329407
BATT_MODEL_RAW:,122,1210.1247695,3.959066391,3.770740509,0.18832588196
BATT_MODEL_RAW:,123,1220.1250217,3.9575119019,3.7692432404,0.1882686615
BATT_MODEL_RAW:,124,1230.1260759,3.9560184479,3.7676353455,0.18838310242
BATT_MODEL_RAW:,125,1240.1265677,3.9545288086,3.7662220001,0.18830680847
BATT_MODEL_RAW:,126,1250.1267244,3.9530467987,3.7649974823,0.18804931641
BATT_MODEL_RAW:,127,1260.1270916,3.9515705109,3.7636451721,0.18792533875
BATT_MODEL_RAW:,128,1270.1272993,3.9501628876,3.7624759674,0.18768692017
BATT_MODEL_RAW:,129,1280.1278516,3.9485874176,3.7610664368,0.18752098083
BATT_MODEL_RAW:,130,1290.1287608,3.9471302032,3.7595767975,0.18755340576
BATT_MODEL_RAW:,131,1300.1290559,3.9457263947,3.7580509186,0.18767547607
BATT_MODEL_RAW:,132,1310.1295808,3.9442367554,3.7564506531,0.18778610229
BATT_MODEL_RAW:,133,1320.1300146,3.9427814484,3.754825592,0.18795585632
BATT_MODEL_RAW:,134,1330.1310061,3.9412136078,3.7533321381,0.18788146973
BATT_MODEL_RAW:,135,1340.1311909,3.9398365021,3.7520942688,0.18774223328
BATT_MODEL_RAW:,136,1350.1314688,3.9383583069,3.7507305145,0.18762779236
BATT_MODEL_RAW:,137,1360.1320154,3.9368152618,3.7491817474,0.1876335144
BATT_MODEL_RAW:,138,1370.1323078,3.9353561401,3.7475223541,0.18783378601
BATT_MODEL_RAW:,139,1380.1333796,3.9338798523,3.7460193634,0.18786048889
BATT_MODEL_RAW:,140,1390.134544,3.9324913025,3.7445220947,0.18796920776
BATT_MODEL_RAW:,141,1400.1350823,3.9309425354,3.742811203,0.1881313324
BATT_MODEL_RAW:,142,1410.1353242,3.9294834137,3.7411327362,0.18835067749
BATT_MODEL_RAW:,143,1420.1364242,3.9280185699,3.7390861511,0.18893241882
BATT_MODEL_RAW:,144,1430.1368941,3.926612854,3.7375202179,0.18909263611
BATT_MODEL_RAW:,145,1440.1374999,3.9250926971,3.7359104156,0.18918228149
BATT_MODEL_RAW:,146,1450.1385187,3.923658371,3.7350311279,0.18862724304
BATT_MODEL_RAW:,147,1460.1389116,3.9222011566,3.7339096069,0.18829154968
BATT_MODEL_RAW:,148,1470.1392986,3.9207458496,3.7322006226,0.18854522705
BATT_MODEL_RAW:,149,1480.1399008,3.9192848206,3.7303943634,0.18889045715
BATT_MODEL_RAW:,150,1490.140121,3.9178333282,3.7288284302,0.18900489807
BATT_MODEL_RAW:,151,1500.141015,3.91639328,3.7268924713,0.18950080872
BATT_MODEL_RAW:,152,1510.1420501,3.9149494171,3.7252426147,0.18970680237
BATT_MODEL_RAW:,153,1520.1424857,3.913520813,3.7238273621,0.18969345093
BATT_MODEL_RAW:,154,1530.1428878,3.9120788574,3.7223129272,0.18976593018
BATT_MODEL_RAW:,155,1540.1438171,3.9107017517,3.7207527161,0.18994903564
BATT_MODEL_RAW:,156,1550.144328,3.9091949463,3.7194442749,0.18975067139
BATT_MODEL_RAW:,157,1560.14454,3.9077682495,3.7179260254,0.18984222412
BATT_MODEL_RAW:,158,1570.1450214,3.9063777924,3.7167663574,0.18961143494
BATT_MODEL_RAW:,159,1580.1455874,3.9048843384,3.7153244019,0.18955993652
BATT_MODEL_RAW:,160,1590.1457759,3.903459549,3.713924408,0.18953514099
BATT_MODEL_RAW:,161,1600.1460267,3.9020442963,3.7127037048,0.18934059143
BATT_MODEL_RAW:,162,1610.1468302,3.9006137848,3.7115974426,0.18901634216
BATT_MODEL_RAW:,163,1620.1479299,3.8992595673,3.7103500366,0.18890953064
BATT_MODEL_RAW:,164,1630.1482598,3.8978424072,3.7091140747,0.18872833252
BATT_MODEL_RAW:,165,1640.1488333,3.8963336945,3.7073097229,0.18902397156
BATT_MODEL_RAW:,166,1650.1496371,3.894985199,3.7057723999,0.18921279907
BATT_MODEL_RAW:,167,1660.1508104,3.8935031891,3.7042236328,0.18927955627
BATT_MODEL_RAW:,168,1670.1512314,3.8920898438,3.70287323,0.18921661377
BATT_MODEL_RAW:,169,1680.1517068,3.8906669617,3.7014045715,0.18926239014
BATT_MODEL_RAW:,170,1690.1525194,3.889257431,3.6995849609,0.18967247009
BATT_MODEL_RAW:,171,1700.152946,3.8878517151,3.6978263855,0.19002532959
BATT_MODEL_RAW:,172,1710.1537267,3.8864307404,3.6959152222,0.19051551819
BATT_MODEL_RAW:,173,1720.1546401,3.8850917816,3.6940574646,0.19103431702
BATT_MODEL_RAW:,174,1730.1555115,3.8837089539,3.6920394897,0.19166946411
BATT_MODEL_RAW:,175,1740.1564768,3.8823013306,3.6903572083,0.19194412231
BATT_MODEL_RAW:,176,1750.1570428,3.8808994293,3.6886749268,0.19222450256
BATT_MODEL_RAW:,177,1760.1573468,3.87940979,3.6869010925,0.19250869751
BATT_MODEL_RAW:,178,1770.1577286,3.8780193329,3.6853637695,0.19265556335
BATT_MODEL_RAW:,179,1780.15886,3.876625061,3.6841316223,0.19249343872
BATT_MODEL_RAW:,180,1790.1591033,3.8752288818,3.6828079224,0.19242095947
BATT_MODEL_RAW:,181,1800.159741,3.8738327026,3.6818161011,0.19201660156
BATT_MODEL_RAW:,182,1810.1603091,3.8724517822,3.6805725098,0.19187927246
BATT_MODEL_RAW:,183,1820.1606877,3.8710651398,3.6794204712,0.19164466858
BATT_MODEL_RAW:,184,1830.1608512,3.8696746826,3.6779518127,0.19172286987
BATT_MODEL_RAW:,185,1840.1618023,3.8683452606,3.6765289307,0.19181632996
BATT_MODEL_RAW:,186,1850.1622332,3.8669090271,3.6752090454,0.19169998169
BATT_MODEL_RAW:,187,1860.1630705,3.865530014,3.6738624573,0.19166755676
BATT_MODEL_RAW:,188,1870.1633383,3.8641548157,3.6726493835,0.19150543213
BATT_MODEL_RAW:,189,1880.163978,3.8627815247,3.6715660095,0.19121551514
BATT_MODEL_RAW:,190,1890.1641428,3.8614749908,3.6703567505,0.19111824036
BATT_MODEL_RAW:,191,1900.1643453,3.8600921631,3.6688499451,0.19124221802
BATT_MODEL_RAW:,192,1910.1649408,3.858669281,3.6670379639,0.19163131714
BATT_MODEL_RAW:,193,1920.1653414,3.8573703766,3.6654853821,0.19188499451
BATT_MODEL_RAW:,194,1930.1664365,3.8559169769,3.6642227173,0.19169425964
BATT_MODEL_RAW:,195,1940.1673721,3.8545608521,3.6628379822,0.19172286987
BATT_MODEL_RAW:,196,1950.1684466,3.8532142639,3.6615600586,0.19165420532
BATT_MODEL_RAW:,197,1960.1694085,3.8518199921,3.6599807739,0.19183921814
BATT_MODEL_RAW:,198,1970.1702991,3.8505020142,3.6581420898,0.19235992432
BATT_MODEL_RAW:,199,1980.1706147,3.8491096497,3.6565437317,0.19256591797
BATT_MODEL_RAW:,200,1990.1717963,3.8477649689,3.6550979614,0.19266700745
BATT_MODEL_RAW:,201,2000.1724529,3.8465023041,3.6538047791,0.19269752502
BATT_MODEL_RAW:,202,2010.1727126,3.8450679779,3.6519050598,0.19316291809
BATT_MODEL_RAW:,203,2020.1730308,3.8437461853,3.6501731873,0.19357299805
BATT_MODEL_RAW:,204,2030.1737532,3.8423671722,3.6487464905,0.19362068176
BATT_MODEL_RAW:,205,2040.1743599,3.8410243988,3.6472892761,0.19373512268
BATT_MODEL_RAW:,206,2050.1754274,3.8397045135,3.6460990906,0.19360542297
BATT_MODEL_RAW:,207,2060.1765273,3.8383350372,3.6449623108,0.19337272644
BATT_MODEL_RAW:,208,2070.177267,3.8370075226,3.6439323425,0.19307518005
BATT_MODEL_RAW:,209,2080.1775112,3.8357505798,3.6429176331,0.19283294678
BATT_MODEL_RAW:,210,2090.1786653,3.8343429565,3.6415977478,0.19274520874
BATT_MODEL_RAW:,211,2100.1793953,3.833026886,3.6402549744,0.19277191162
BATT_MODEL_RAW:,212,2110.1795814,3.8316726685,3.6389808655,0.19269180298
BATT_MODEL_RAW:,213,2120.1806414,3.8303585052,3.6377182007,0.19264030457
BATT_MODEL_RAW:,214,2130.1808918,3.829044342,3.6364135742,0.19263076782
BATT_MODEL_RAW:,215,2140.1812198,3.8277854919,3.6352806091,0.19250488281
BATT_MODEL_RAW:,216,2150.1822597,3.826379776,3.6338500977,0.19252967834
BATT_MODEL_RAW:,217,2160.1830443,3.8250637054,3.6324691772,0.1925945282
BATT_MODEL_RAW:,218,2170.1840139,3.8238296509,3.63048172,0.19334793091
BATT_MODEL_RAW:,219,2180.1849618,3.8224258423,3.6291236877,0.19330215454
BATT_MODEL_RAW:,220,2190.1855226,3.8211078644,3.627658844,0.19344902039
BATT_MODEL_RAW:,221,2200.1862445,3.8197898865,3.6265525818,0.19323730469
BATT_MODEL_RAW:,222,2210.1871201,3.818572998,3.6254882813,0.1930847168
BATT_MODEL_RAW:,223,2220.187443,3.8172054291,3.6239738464,0.19323158264
BATT_MODEL_RAW:,224,2230.1877131,3.8159790039,3.6225471497,0.19343185425
BATT_MODEL_RAW:,225,2240.1886459,3.8145847321,3.6215705872,0.1930141449
BATT_MODEL_RAW:,226,2250.1894314,3.8133068085,3.6203193665,0.19298744202
BATT_MODEL_RAW:,227,2260.1900631,3.8119792938,3.6190795898,0.19289970398
BATT_MODEL_RAW:,228,2270.1904116,3.8107185364,3.617565155,0.19315338135
BATT_MODEL_RAW:,229,2280.1909642,3.8094062805,3.6160011292,0.19340515137
BATT_MODEL_RAW:,230,2290.1913139,3.8081302643,3.6147155762,0.19341468811
BATT_MODEL_RAW:,231,2300.192407,3.8068523407,3.6133041382,0.19354820251
BATT_MODEL_RAW:,232,2310.1934624,3.805562973,3.6120948792,0.19346809387
BATT_MODEL_RAW:,233,2320.1944183,3.8042888641,3.6109542847,0.19333457947
BATT_MODEL_RAW:,234,2330.1946055,3.8030490875,3.6099472046,0.19310188293
BATT_MODEL_RAW:,235,2340.195518,3.8017196655,3.608379364,0.19334030151
BATT_MODEL_RAW:,236,2350.1963123,3.8005313873,3.6069717407,0.19355964661
BATT_MODEL_RAW:,237,2360.1969718,3.7991752625,3.6053886414,0.19378662109
BATT_MODEL_RAW:,238,2370.1974348,3.797908783,3.6037559509,0.19415283203
BATT_MODEL_RAW:,239,2380.1975907,3.7966480255,3.6023216248,0.19432640076
BATT_MODEL_RAW:,240,2390.1977553,3.7953853607,3.6006736755,0.19471168518
BATT_MODEL_RAW:,241,2400.1983065,3.7941417694,3.5993118286,0.1948299408
BATT_MODEL_RAW:,242,2410.1993375,3.7929363251,3.5981445313,0.19479179382
BATT_MODEL_RAW:,243,2420.2003928,3.7916069031,3.5969390869,0.19466781616
BATT_MODEL_RAW:,244,2430.201436,3.790353775,3.595703125,0.19465065002
BATT_MODEL_RAW:,245,2440.2016925,3.7891044617,3.5944252014,0.19467926025
BATT_MODEL_RAW:,246,2450.2025763,3.7878570557,3.5930786133,0.19477844238
BATT_MODEL_RAW:,247,2460.2030338,3.7866973877,3.5919532776,0.19474411011
BATT_MODEL_RAW:,248,2470.2035422,3.7853775024,3.5906791687,0.19469833374
BATT_MODEL_RAW:,249,2480.2038442,3.7841396332,3.5892486572,0.19489097595
BATT_MODEL_RAW:,250,2490.2042964,3.7828998566,3.5881881714,0.19471168518
BATT_MODEL_RAW:,251,2500.2050429,3.7817497253,3.5874557495,0.19429397583
BATT_MODEL_RAW:,252,2510.2055379,3.7804489136,3.5866088867,0.19384002686
BATT_MODEL_RAW:,253,2520.2060592,3.7792129517,3.5857658386,0.19344711304
BATT_MODEL_RAW:,254,2530.2067009,3.7779960632,3.5844688416,0.19352722168
BATT_MODEL_RAW:,255,2540.2069688,3.7767715454,3.5831375122,0.1936340332
BATT_MODEL_RAW:,256,2550.2078636,3.7755336761,3.5819396973,0.19359397888
BATT_MODEL_RAW:,257,2560.2083798,3.7744026184,3.5808563232,0.19354629517
BATT_MODEL_RAW:,258,2570.2089833,3.7731132507,3.5794525146,0.19366073608
BATT_MODEL_RAW:,259,2580.2098239,3.7719974518,3.5782852173,0.1937122345
BATT_MODEL_RAW:,260,2590.2103883,3.7707767487,3.5771598816,0.19361686707
BATT_MODEL_RAW:,261,2600.2111209,3.769493103,3.5761108398,0.19338226318
BATT_MODEL_RAW:,262,2610.2115384,3.7682876587,3.5751609802,0.19312667847
BATT_MODEL_RAW:,263,2620.2119146,3.7671794891,3.5741004944,0.19307899475
BATT_MODEL_RAW:,264,2630.2130281,3.7659835815,3.5727539063,0.19322967529
BATT_MODEL_RAW:,265,2640.2137852,3.7647151947,3.571434021,0.19328117371
BATT_MODEL_RAW:,266,2650.2145186,3.7635269165,3.5702133179,0.19331359863
BATT_MODEL_RAW:,267,2660.2154316,3.7623500824,3.5690002441,0.19334983826
BATT_MODEL_RAW:,268,2670.2156243,3.7611465454,3.5678062439,0.19334030151
BATT_MODEL_RAW:,269,2680.2161005,3.7600822449,3.5666313171,0.19345092773
BATT_MODEL_RAW:,270,2690.2168678,3.7588157654,3.5651473999,0.19366836548
BATT_MODEL_RAW:,271,2700.2179907,3.757724762,3.5640983582,0.19362640381
BATT_MODEL_RAW:,272,2710.2187643,3.756526947,3.5627861023,0.19374084473
BATT_MODEL_RAW:,273,2720.2193168,3.7552986145,3.5617713928,0.19352722168
BATT_MODEL_RAW:,274,2730.2203498,3.7541427612,3.5606536865,0.19348907471
BATT_MODEL_RAW:,275,2740.2206273,3.7530059814,3.5593414307,0.19366455078
BATT_MODEL_RAW:,276,2750.221038,3.7518959045,3.5582962036,0.19359970093
BATT_MODEL_RAW:,277,2760.221494,3.7507019043,3.5570487976,0.19365310669
BATT_MODEL_RAW:,278,2770.2224626,3.7495384216,3.556022644,0.19351577759
BATT_MODEL_RAW:,279,2780.2233429,3.7484016418,3.5550079346,0.19339370728
BATT_MODEL_RAW:,280,2790.2240206,3.74725914,3.5539283752,0.19333076477
BATT_MODEL_RAW:,281,2800.2244176,3.7461280823,3.5527038574,0.19342422485
BATT_MODEL_RAW:,282,2810.2253191,3.7450733185,3.5515060425,0.193567276
BATT_MODEL_RAW:,283,2820.2259454,3.7438621521,3.5500221252,0.19384002686
BATT_MODEL_RAW:,284,2830.2265754,3.7427406311,3.5489959717,0.19374465942
BATT_MODEL_RAW:,285,2840.2275292,3.7416191101,3.5479507446,0.19366836548
BATT_MODEL_RAW:,286,2850.2282051,3.7405033112,3.5468673706,0.19363594055
BATT_MODEL_RAW:,287,2860.2286195,3.7393894196,3.5455665588,0.19382286072
BATT_MODEL_RAW:,288,2870.2296059,3.7382850647,3.5443191528,0.19396591187
BATT_MODEL_RAW:,289,2880.2307076,3.7372055054,3.5434074402,0.19379806519
BATT_MODEL_RAW:,290,2890.2309549,3.7360591888,3.542388916,0.19367027283
BATT_MODEL_RAW:,291,2900.2314527,3.7349758148,3.5413818359,0.19359397888
BATT_MODEL_RAW:,292,2910.2324707,3.7338943481,3.5403633118,0.19353103638
BATT_MODEL_RAW:,293,2920.2332943,3.7327842712,3.5390930176,0.19369125366
BATT_MODEL_RAW:,294,2930.233567,3.7316951752,3.5381317139,0.1935634613
BATT_MODEL_RAW:,295,2940.2340513,3.7306194305,3.5372200012,0.19339942932
BATT_MODEL_RAW:,296,2950.2351909,3.7295398712,3.5362892151,0.19325065613
BATT_MODEL_RAW:,297,2960.2355434,3.7284412384,3.5351829529,0.19325828552
BATT_MODEL_RAW:,298,2970.2366828,3.7273693085,3.5342903137,0.19307899475
BATT_MODEL_RAW:,299,2980.2378515,3.7262992859,3.5332984924,0.19300079346
BATT_MODEL_RAW:,300,2990.2380486,3.7252540588,3.5322303772,0.19302368164
BATT_MODEL_RAW:,301,3000.2384616,3.7241821289,3.5312423706,0.1929397583
BATT_MODEL_RAW:,302,3010.2393535,3.7231254578,3.5304489136,0.19267654419
BATT_MODEL_RAW:,303,3020.2402629,3.7220649719,3.5295982361,0.19246673584
BATT_MODEL_RAW:,304,3030.2404248,3.7210044861,3.5286903381,0.19231414795
BATT_MODEL_RAW:,305,3040.2411871,3.7199630737,3.5278549194,0.1921081543
BATT_MODEL_RAW:,306,3050.2422106,3.718914032,3.5268630981,0.19205093384
BATT_MODEL_RAW:,307,3060.2428997,3.7179489136,3.5260276794,0.19192123413
BATT_MODEL_RAW:,308,3070.2438465,3.716835022,3.524974823,0.19186019897
BATT_MODEL_RAW:,309,3080.2445068,3.7158088684,3.5240478516,0.19176101685
BATT_MODEL_RAW:,310,3090.2448357,3.7147750854,3.522983551,0.19179153442
BATT_MODEL_RAW:,311,3100.2454437,3.7137527466,3.5219802856,0.19177246094
BATT_MODEL_RAW:,312,3110.2460561,3.712726593,3.5211334229,0.19159317017
BATT_MODEL_RAW:,313,3120.2463175,3.7117118835,3.5202598572,0.19145202637
BATT_MODEL_RAW:,314,3130.2465718,3.7106895447,3.5193595886,0.19132995605
BATT_MODEL_RAW:,315,3140.2469993,3.7096862793,3.5186080933,0.19107818604
BATT_MODEL_RAW:,316,3150.2472466,3.7086601257,3.5175361633,0.1911239624
BATT_MODEL_RAW:,317,3160.2483737,3.7077484131,3.5164146423,0.19133377075
BATT_MODEL_RAW:,318,3170.2486989,3.7066574097,3.5154685974,0.19118881226
BATT_MODEL_RAW:,319,3180.2492204,3.7057533264,3.5145797729,0.19117355347
BATT_MODEL_RAW:,320,3190.2496347,3.7047424316,3.5137062073,0.19103622437
BATT_MODEL_RAW:,321,3200.2505373,3.7036857605,3.5127029419,0.1909828186
BATT_MODEL_RAW:,322,3210.2508951,3.7026977539,3.5118217468,0.19087600708
BATT_MODEL_RAW:,323,3220.2518768,3.701713562,3.5110092163,0.1907043457
BATT_MODEL_RAW:,324,3230.2527011,3.7007217407,3.5101699829,0.19055175781
BATT_MODEL_RAW:,325,3240.2529436,3.6998176575,3.5092201233,0.19059753418
BATT_MODEL_RAW:,326,3250.2541429,3.6987800598,3.5081672668,0.19061279297
BATT_MODEL_RAW:,327,3260.2547547,3.6978912354,3.5072517395,0.19063949585
BATT_MODEL_RAW:,328,3270.2556079,3.6968421936,3.5061340332,0.1907081604
BATT_MODEL_RAW:,329,3280.2565053,3.6959533691,3.5053443909,0.19060897827
BATT_MODEL_RAW:,330,3290.2569454,3.6950187683,3.5042228699,0.19079589844
BATT_MODEL_RAW:,331,3300.2574065,3.6939811707,3.5031471252,0.19083404541
BATT_MODEL_RAW:,332,3310.258046,3.6930427551,3.5021247864,0.19091796875
BATT_MODEL_RAW:,333,3320.2585678,3.6920700073,3.5010566711,0.19101333618
BATT_MODEL_RAW:,334,3330.2593486,3.6911506653,3.4998703003,0.19128036499
BATT_MODEL_RAW:,335,3340.2597528,3.6902008057,3.4987831116,0.19141769409
BATT_MODEL_RAW:,336,3350.2605721,3.6893463135,3.4978294373,0.19151687622
BATT_MODEL_RAW:,337,3360.2615384,3.6883430481,3.4968185425,0.19152450562
BATT_MODEL_RAW:,338,3370.2624104,3.687412262,3.4957885742,0.19162368774
BATT_MODEL_RAW:,339,3380.2631273,3.6864776611,3.4948272705,0.19165039063
BATT_MODEL_RAW:,340,3390.2638755,3.6855773926,3.4939193726,0.19165802002
BATT_MODEL_RAW:,341,3400.2649824,3.6846618652,3.4928741455,0.19178771973
BATT_MODEL_RAW:,342,3410.2660352,3.6837348938,3.4919319153,0.19180297852
BATT_MODEL_RAW:,343,3420.2663073,3.6828994751,3.4909858704,0.19191360474
BATT_MODEL_RAW:,344,3430.2671939,3.6819152832,3.4898109436,0.1921043396
BATT_MODEL_RAW:,345,3440.2681706,3.681098938,3.4888114929,0.19228744507
BATT_MODEL_RAW:,346,3450.2686604,3.6801872253,3.487739563,0.19244766235
BATT_MODEL_RAW:,347,3460.2695938,3.6792182922,3.4866600037,0.19255828857
BATT_MODEL_RAW:,348,3470.2699009,3.6784057617,3.4856872559,0.19271850586
BATT_MODEL_RAW:,349,3480.2708169,3.6774291992,3.4845237732,0.19290542603
BATT_MODEL_RAW:,350,3490.271705,3.6765441895,3.4836082458,0.1929359436
BATT_MODEL_RAW:,351,3500.2719038,3.6757545471,3.4825210571,0.19323348999
BATT_MODEL_RAW:,352,3510.2726908,3.6747970581,3.481388092,0.19340896606
BATT_MODEL_RAW:,353,3520.2736179,3.6739273071,3.4803886414,0.19353866577
BATT_MODEL_RAW:,354,3530.2744364,3.673160553,3.4794883728,0.19367218018
BATT_MODEL_RAW:,355,3540.2746976,3.672252655,3.4785614014,0.19369125366
BATT_MODEL_RAW:,356,3550.2752055,3.6713180542,3.4776000977,0.19371795654
BATT_MODEL_RAW:,357,3560.2757913,3.6704673767,3.4765357971,0.19393157959
BATT_MODEL_RAW:,358,3570.276127,3.6696166992,3.4753952026,0.19422149658
BATT_MODEL_RAW:,359,3580.2772051,3.6687583923,3.4744720459,0.19428634644
BATT_MODEL_RAW:,360,3590.2783316,3.6679229736,3.4738922119,0.19403076172
BATT_MODEL_RAW:,361,3600.2788311,3.6670455933,3.4730834961,0.19396209717
BATT_MODEL_RAW:,362,3610.2794417,3.6661987305,3.4720611572,0.19413757324
BATT_MODEL_RAW:,363,3620.2803403,3.6653938293,3.4710769653,0.19431686401
BATT_MODEL_RAW:,364,3630.2812399,3.6645507813,3.470085144,0.19446563721
BATT_MODEL_RAW:,365,3640.2817493,3.6637878418,3.4693260193,0.19446182251
BATT_MODEL_RAW:,366,3650.2827801,3.6628799438,3.4684066772,0.1944732666
BATT_MODEL_RAW:,367,3660.2831202,3.6620559692,3.4677772522,0.19427871704
BATT_MODEL_RAW:,368,3670.2835358,3.6612968445,3.4671554565,0.19414138794
BATT_MODEL_RAW:,369,3680.2836652,3.6604118347,3.4663162231,0.19409561157
BATT_MODEL_RAW:,370,3690.2838109,3.659614563,3.4655723572,0.19404220581
BATT_MODEL_RAW:,371,3700.284245,3.6587905884,3.4648513794,0.19393920898
BATT_MODEL_RAW:,372,3710.2849285,3.6579742432,3.4643211365,0.19365310669
BATT_MODEL_RAW:,373,3720.2857137,3.6571960449,3.4636993408,0.1934967041
BATT_MODEL_RAW:,374,3730.2867205,3.6564559937,3.4630470276,0.19340896606
BATT_MODEL_RAW:,375,3740.2877529,3.6555938721,3.462272644,0.19332122803
BATT_MODEL_RAW:,376,3750.2886082,3.6547927856,3.4613227844,0.19347000122
BATT_MODEL_RAW:,377,3760.2895793,3.6539993286,3.4605140686,0.19348526001
BATT_MODEL_RAW:,378,3770.290069,3.6532897949,3.4598083496,0.19348144531
BATT_MODEL_RAW:,379,3780.2911992,3.6524200439,3.4590530396,0.19336700439
BATT_MODEL_RAW:,380,3790.2920243,3.6516342163,3.4583282471,0.19330596924
BATT_MODEL_RAW:,381,3800.2925774,3.6509590149,3.4576034546,0.1933555603
BATT_MODEL_RAW:,382,3810.2932636,3.6501083374,3.4569969177,0.19311141968
BATT_MODEL_RAW:,383,3820.2940702,3.6493339539,3.456413269,0.19292068481
BATT_MODEL_RAW:,384,3830.2946129,3.6485671997,3.4560432434,0.1925239563
BATT_MODEL_RAW:,385,3840.2952435,3.647808075,3.4557991028,0.19200897217
BATT_MODEL_RAW:,386,3850.2960229,3.6470375061,3.45545578,0.19158172607
BATT_MODEL_RAW:,387,3860.2969595,3.6463012695,3.4549560547,0.19134521484
BATT_MODEL_RAW:,388,3870.2974377,3.645614624,3.4542388916,0.19137573242
BATT_MODEL_RAW:,389,3880.2979057,3.6448707581,3.4531898499,0.1916809082
BATT_MODEL_RAW:,390,3890.2985226,3.6440429688,3.4520835876,0.1919593811
BATT_MODEL_RAW:,391,3900.2991378,3.6433067322,3.4513931274,0.19191360474
BATT_MODEL_RAW:,392,3910.2997156,3.6425628662,3.4508743286,0.1916885376
BATT_MODEL_RAW:,393,3920.3006315,3.6418914795,3.4503707886,0.19152069092
BATT_MODEL_RAW:,394,3930.3013288,3.6410980225,3.4496879578,0.1914100647
BATT_MODEL_RAW:,395,3940.3015279,3.6403808594,3.4491043091,0.19127655029
BATT_MODEL_RAW:,396,3950.3017786,3.6397247314,3.4483718872,0.19135284424
BATT_MODEL_RAW:,397,3960.3020032,3.6389198303,3.4477119446,0.19120788574
BATT_MODEL_RAW:,398,3970.3025804,3.6381988525,3.4470787048,0.19112014771
BATT_MODEL_RAW:,399,3980.3032721,3.6374893188,3.4465675354,0.19092178345
BATT_MODEL_RAW:,400,3990.3035082,3.6367645264,3.4459266663,0.19083786011
BATT_MODEL_RAW:,401,4000.3039961,3.6361465454,3.4451980591,0.19094848633
BATT_MODEL_RAW:,402,4010.304243,3.6353569031,3.444393158,0.19096374512
BATT_MODEL_RAW:,403,4020.3044197,3.6346702576,3.4436836243,0.1909866333
BATT_MODEL_RAW:,404,4030.30484,3.6340332031,3.442905426,0.1911277771
BATT_MODEL_RAW:,405,4040.3060153,3.6332740784,3.4328422546,0.20043182373
BATT_MODEL_RAW:,406,4050.306549,3.6325874329,3.4349098206,0.1976776123
BATT_MODEL_RAW:,407,4060.3076581,3.6319007874,3.4351425171,0.19675827026
BATT_MODEL_RAW:,408,4070.3079769,3.6313018799,3.4353904724,0.19591140747
BATT_MODEL_RAW:,409,4080.3082943,3.6305427551,3.4360046387,0.19453811646
BATT_MODEL_RAW:,410,4090.30933,3.6298713684,3.4359931946,0.19387817383
BATT_MODEL_RAW:,411,4100.3099591,3.6291923523,3.43516922,0.19402313232
BATT_MODEL_RAW:,412,4110.3109876,3.6285743713,3.435092926,0.19348144531
BATT_MODEL_RAW:,413,4120.3112645,3.6278495789,3.4346199036,0.19322967529
BATT_MODEL_RAW:,414,4130.3116564,3.6272621155,3.4340782166,0.19318389893
BATT_MODEL_RAW:,415,4140.3124607,3.6265182495,3.4335289001,0.19298934937
BATT_MODEL_RAW:,416,4150.3128079,3.6258544922,3.4330177307,0.19283676147
BATT_MODEL_RAW:,417,4160.3138703,3.6252212524,3.4326629639,0.19255828857
BATT_MODEL_RAW:,418,4170.3148748,3.624622345,3.4321784973,0.19244384766
BATT_MODEL_RAW:,419,4180.3151136,3.6239013672,3.4318504333,0.19205093384
BATT_MODEL_RAW:,420,4190.3156833,3.6232528687,3.4316711426,0.19158172607
BATT_MODEL_RAW:,421,4200.3168724,3.6225967407,3.4310760498,0.19152069092
BATT_MODEL_RAW:,422,4210.3172671,3.6219520569,3.4304237366,0.19152832031
BATT_MODEL_RAW:,423,4220.3180377,3.6213607788,3.4298477173,0.19151306152
BATT_MODEL_RAW:,424,4230.3187767,3.6206817627,3.4291419983,0.1915397644
BATT_MODEL_RAW:,425,4240.3195742,3.6200447083,3.4282264709,0.1918182373
BATT_MODEL_RAW:,426,4250.3205228,3.6194038391,3.4277229309,0.1916809082
BATT_MODEL_RAW:,427,4260.320782,3.6187591553,3.4271812439,0.19157791138
BATT_MODEL_RAW:,428,4270.3210309,3.618221283,3.4265556335,0.19166564941
BATT_MODEL_RAW:,429,4280.3216851,3.6175270081,3.4256019592,0.19192504883
BATT_MODEL_RAW:,430,4290.322005,3.6168899536,3.4247665405,0.19212341309
BATT_MODEL_RAW:,431,4300.3228822,3.616268158,3.4243850708,0.19188308716
BATT_MODEL_RAW:,432,4310.3230709,3.6156425476,3.424030304,0.19161224365
BATT_MODEL_RAW:,433,4320.3236277,3.6150360107,3.4234733582,0.19156265259
BATT_MODEL_RAW:,434,4330.324128,3.6144065857,3.4228401184,0.19156646729
BATT_MODEL_RAW:,435,4340.3250503,3.6138076782,3.4222221375,0.19158554077
BATT_MODEL_RAW:,436,4350.3256862,3.6131858826,3.4216003418,0.19158554077
BATT_MODEL_RAW:,437,4360.3259834,3.6126708984,3.4211349487,0.19153594971
BATT_MODEL_RAW:,438,4370.3268641,3.6119842529,3.4203414917,0.19164276123
BATT_MODEL_RAW:,439,4380.3271106,3.6113777161,3.419719696,0.19165802002
BATT_MODEL_RAW:,440,4390.3275646,3.6108779907,3.4193954468,0.19148254395
BATT_MODEL_RAW:,441,4400.3278167,3.6101837158,3.4187393188,0.19144439697
BATT_MODEL_RAW:,442,4410.3280298,3.6095962524,3.4183425903,0.19125366211
BATT_MODEL_RAW:,443,4420.3291916,3.6090774536,3.4178619385,0.19121551514
BATT_MODEL_RAW:,444,4430.3295194,3.6084976196,3.417049408,0.19144821167
BATT_MODEL_RAW:,445,4440.3298115,3.6078147888,3.4163665771,0.19144821167
BATT_MODEL_RAW:,446,4450.3300075,3.6072463989,3.415561676,0.1916847229
BATT_MODEL_RAW:,447,4460.3305703,3.6066932678,3.414855957,0.19183731079
BATT_MODEL_RAW:,448,4470.3314322,3.6061553955,3.4144706726,0.1916847229
BATT_MODEL_RAW:,449,4480.3326268,3.6054916382,3.4137382507,0.19175338745
BATT_MODEL_RAW:,450,4490.3336232,3.6049118042,3.4132804871,0.19163131714
BATT_MODEL_RAW:,451,4500.3347471,3.6043243408,3.4127998352,0.19152450562
BATT_MODEL_RAW:,452,4510.3358831,3.6037483215,3.4124488831,0.19129943848
BATT_MODEL_RAW:,453,4520.336818,3.6032371521,3.4123916626,0.1908454895
BATT_MODEL_RAW:,454,4530.3372652,3.6026000977,3.4122009277,0.19039916992
BATT_MODEL_RAW:,455,4540.3384872,3.6020545959,3.4118156433,0.19023895264
BATT_MODEL_RAW:,456,4550.3387597,3.6015510559,3.4114608765,0.19009017944
BATT_MODEL_RAW:,457,4560.3394534,3.6009063721,3.4109649658,0.18994140625
BATT_MODEL_RAW:,458,4570.3404476,3.6003379822,3.4105606079,0.18977737427
BATT_MODEL_RAW:,459,4580.3407965,3.5998573303,3.4102478027,0.18960952759
BATT_MODEL_RAW:,460,4590.3411555,3.5992202759,3.4095726013,0.18964767456
BATT_MODEL_RAW:,461,4600.3420071,3.5986595154,3.4091835022,0.18947601318
BATT_MODEL_RAW:,462,4610.342217,3.5981025696,3.4084472656,0.18965530396
BATT_MODEL_RAW:,463,4620.3428244,3.5975379944,3.407787323,0.18975067139
BATT_MODEL_RAW:,464,4630.3439776,3.5969772339,3.4067802429,0.19019699097
BATT_MODEL_RAW:,465,4640.3444751,3.596446991,3.4055938721,0.1908531189
BATT_MODEL_RAW:,466,4650.3454159,3.5958747864,3.4044494629,0.19142532349
BATT_MODEL_RAW:,467,4660.3459147,3.59532547,3.4043045044,0.19102096558
BATT_MODEL_RAW:,468,4670.346854,3.5947685242,3.4036865234,0.19108200073
BATT_MODEL_RAW:,469,4680.3476577,3.5942153931,3.4026603699,0.19155502319
BATT_MODEL_RAW:,470,4690.3483124,3.5936813354,3.4015426636,0.19213867188
BATT_MODEL_RAW:,471,4700.3486118,3.5932006836,3.4013214111,0.19187927246
BATT_MODEL_RAW:,472,4710.3491792,3.5925636292,3.4005126953,0.19205093384
BATT_MODEL_RAW:,473,4720.3495788,3.5920219421,3.4002037048,0.1918182373
BATT_MODEL_RAW:,474,4730.3499595,3.5914840698,3.3997535706,0.19173049927
BATT_MODEL_RAW:,475,4740.3503992,3.5909423828,3.3987846375,0.19215774536
BATT_MODEL_RAW:,476,4750.351375,3.5903930664,3.3984565735,0.19193649292
BATT_MODEL_RAW:,477,4760.351686,3.5898513794,3.3981933594,0.19165802002
BATT_MODEL_RAW:,478,4770.3523168,3.5893096924,3.3981323242,0.19117736816
BATT_MODEL_RAW:,479,4780.3532405,3.5887718201,3.3966369629,0.19213485718
BATT_MODEL_RAW:,480,4790.35387,3.5882301331,3.3962783813,0.19195175171
BATT_MODEL_RAW:,481,4800.3543432,3.5876922607,3.3955001831,0.19219207764
BATT_MODEL_RAW:,482,4810.3553711,3.5871582031,3.3949127197,0.1922454834
BATT_MODEL_RAW:,483,4820.3556691,3.5866127014,3.3947639465,0.19184875488
BATT_MODEL_RAW:,484,4830.3562724,3.5861587524,3.3941116333,0.19204711914
BATT_MODEL_RAW:,485,4840.3570253,3.5855484009,3.3939704895,0.19157791138
BATT_MODEL_RAW:,486,4850.3572526,3.5850830078,3.393321991,0.19176101685
BATT_MODEL_RAW:,487,4860.3581682,3.5845031738,3.3924713135,0.19203186035
BATT_MODEL_RAW:,488,4870.3585744,3.5839576721,3.3920021057,0.19195556641
BATT_MODEL_RAW:,489,4880.3595397,3.5834388733,3.3918266296,0.19161224365
BATT_MODEL_RAW:,490,4890.3603815,3.582901001,3.3913497925,0.1915512085
BATT_MODEL_RAW:,491,4900.3608975,3.5824432373,3.3914222717,0.19102096558
BATT_MODEL_RAW:,492,4910.3619865,3.5818481445,3.3908500671,0.19099807739
BATT_MODEL_RAW:,493,4920.3628808,3.5813140869,3.3902778625,0.19103622437
BATT_MODEL_RAW:,494,4930.3633325,3.5807952881,3.3898582458,0.19093704224
BATT_MODEL_RAW:,495,4940.3644729,3.580329895,3.3893203735,0.19100952148
BATT_MODEL_RAW:,496,4950.3652743,3.5797309875,3.3886566162,0.19107437134
BATT_MODEL_RAW:,497,4960.3661908,3.5792236328,3.388343811,0.19087982178
BATT_MODEL_RAW:,498,4970.3666682,3.5787582397,3.3878288269,0.19092941284
BATT_MODEL_RAW:,499,4980.3671698,3.5781555176,3.3873023987,0.1908531189
BATT_MODEL_RAW:,500,4990.3681843,3.5776252747,3.3868522644,0.19077301025
BATT_MODEL_RAW:,501,5000.3685374,3.5771141052,3.3865661621,0.19054794312
BATT_MODEL_RAW:,502,5010.3689851,3.5765914917,3.3858528137,0.19073867798
BATT_MODEL_RAW:,503,5020.3699379,3.5760612488,3.3851165771,0.19094467163
BATT_MODEL_RAW:,504,5030.3707677,3.5755462646,3.3844528198,0.19109344482
BATT_MODEL_RAW:,505,5040.371573,3.575012207,3.3837203979,0.19129180908
BATT_MODEL_RAW:,506,5050.3717749,3.5745048523,3.3811759949,0.19332885742
BATT_MODEL_RAW:,507,5060.3725699,3.5739974976,3.3807067871,0.19329071045
BATT_MODEL_RAW:,508,5070.3734059,3.5734596252,3.3810462952,0.19241333008
BATT_MODEL_RAW:,509,5080.3737351,3.5729522705,3.3796653748,0.19328689575
BATT_MODEL_RAW:,510,5090.3744849,3.5724258423,3.3795013428,0.19292449951
BATT_MODEL_RAW:,511,5100.3752711,3.5719070435,3.3792114258,0.19269561768
BATT_MODEL_RAW:,512,5110.3761699,3.5713844299,3.3788223267,0.19256210327
BATT_MODEL_RAW:,513,5120.3768413,3.5708694458,3.3785858154,0.19228363037
BATT_MODEL_RAW:,514,5130.3778812,3.5703468323,3.3784866333,0.19186019897
BATT_MODEL_RAW:,515,5140.3782802,3.5698394775,3.3785705566,0.1912689209
BATT_MODEL_RAW:,516,5150.3791639,3.5693206787,3.3781394958,0.19118118286
BATT_MODEL_RAW:,517,5160.3800456,3.5687980652,3.3776702881,0.1911277771
BATT_MODEL_RAW:,518,5170.3801875,3.5682792664,3.3774757385,0.19080352783
BATT_MODEL_RAW:,519,5180.3813916,3.5677833557,3.3775138855,0.19026947021
BATT_MODEL_RAW:,520,5190.3823016,3.5673370361,3.3774032593,0.18993377686
BATT_MODEL_RAW:,521,5200.383011,3.566734314,3.3770256042,0.18970870972
BATT_MODEL_RAW:,522,5210.3842069,3.5663070679,3.3765983582,0.18970870972
BATT_MODEL_RAW:,523,5220.3844974,3.5657196045,3.376083374,0.18963623047
BATT_MODEL_RAW:,524,5230.3854313,3.5651817322,3.3757019043,0.18947982788
BATT_MODEL_RAW:,525,5240.3861539,3.5647468567,3.3753814697,0.18936538696
BATT_MODEL_RAW:,526,5250.3864691,3.5641670227,3.3750419617,0.18912506104
BATT_MODEL_RAW:,527,5260.3869659,3.5636558533,3.3746986389,0.18895721436
BATT_MODEL_RAW:,528,5270.3875531,3.5631332397,3.374256134,0.18887710571
BATT_MODEL_RAW:,529,5280.387903,3.5626144409,3.374168396,0.18844604492
BATT_MODEL_RAW:,530,5290.3888011,3.5621604919,3.3738098145,0.18835067749
BATT_MODEL_RAW:,531,5300.389169,3.5615844727,3.3730697632,0.18851470947
BATT_MODEL_RAW:,532,5310.3894798,3.5610771179,3.372467041,0.1886100769
BATT_MODEL_RAW:,533,5320.3898467,3.5606575012,3.3721809387,0.1884765625
BATT_MODEL_RAW:,534,5330.3904771,3.5600547791,3.3718261719,0.18822860718
BATT_MODEL_RAW:,535,5340.3908388,3.5595245361,3.3712730408,0.18825149536
BATT_MODEL_RAW:,536,5350.3910321,3.5590858459,3.3709068298,0.18817901611
BATT_MODEL_RAW:,537,5360.3912367,3.5585670471,3.3705215454,0.18804550171
BATT_MODEL_RAW:,538,5370.3916882,3.5580635071,3.3701934814,0.18787002563
BATT_MODEL_RAW:,539,5380.3925742,3.5574760437,3.3695869446,0.18788909912
BATT_MODEL_RAW:,540,5390.3928318,3.5569648743,3.3688316345,0.18813323975
BATT_MODEL_RAW:,541,5400.3934203,3.5564460754,3.3684616089,0.18798446655
BATT_MODEL_RAW:,542,5410.3941184,3.5559272766,3.3682365417,0.18769073486
BATT_MODEL_RAW:,543,5420.3950691,3.5553970337,3.367603302,0.18779373169
BATT_MODEL_RAW:,544,5430.3953264,3.5548706055,3.3673324585,0.18753814697
BATT_MODEL_RAW:,545,5440.3954846,3.5543708801,3.3668937683,0.18747711182
BATT_MODEL_RAW:,546,5450.3962305,3.5538711548,3.3656959534,0.18817520142
BATT_MODEL_RAW:,547,5460.3973649,3.5533332825,3.3647956848,0.18853759766
BATT_MODEL_RAW:,548,5470.3978446,3.5528259277,3.364780426,0.18804550171
BATT_MODEL_RAW:,549,5480.3988857,3.5522918701,3.3647232056,0.18756866455
BATT_MODEL_RAW:,550,5490.3995906,3.5517692566,3.3647460938,0.18702316284
BATT_MODEL_RAW:,551,5500.40037,3.5512504578,3.364112854,0.18713760376
BATT_MODEL_RAW:,552,5510.4005483,3.5507202148,3.3638000488,0.18692016602
BATT_MODEL_RAW:,553,5520.4013935,3.5502052307,3.3632125854,0.18699264526
BATT_MODEL_RAW:,554,5530.4015353,3.5497016907,3.3626174927,0.187084198
BATT_MODEL_RAW:,555,5540.4025653,3.5492324829,3.36195755,0.18727493286
BATT_MODEL_RAW:,556,5550.4037492,3.548625946,3.3615112305,0.18711471558
BATT_MODEL_RAW:,557,5560.4049702,3.5481796265,3.3610992432,0.1870803833
BATT_MODEL_RAW:,558,5570.4059304,3.5475883484,3.3607673645,0.18682098389
BATT_MODEL_RAW:,559,5580.4066367,3.5470466614,3.3603363037,0.18671035767
BATT_MODEL_RAW:,560,5590.4069955,3.5465316772,3.359752655,0.18677902222
BATT_MODEL_RAW:,561,5600.4078729,3.5459899902,3.3591346741,0.18685531616
BATT_MODEL_RAW:,562,5610.4081549,3.5454521179,3.3583946228,0.18705749512
BATT_MODEL_RAW:,563,5620.4086179,3.5449371338,3.3578224182,0.18711471558
BATT_MODEL_RAW:,564,5630.4096431,3.5444068909,3.3573379517,0.18706893921
BATT_MODEL_RAW:,565,5640.4100318,3.5438766479,3.3568725586,0.18700408936
BATT_MODEL_RAW:,566,5650.4105463,3.5433425903,3.3561897278,0.18715286255
BATT_MODEL_RAW:,567,5660.4115604,3.5429458618,3.3552742004,0.18767166138
BATT_MODEL_RAW:,568,5670.4118315,3.5423164368,3.3546714783,0.1876449585
BATT_MODEL_RAW:,569,5680.4121842,3.5417327881,3.3543434143,0.18738937378
BATT_MODEL_RAW:,570,5690.4127979,3.5412025452,3.3537025452,0.1875
BATT_MODEL_RAW:,571,5700.4130364,3.5406723022,3.3530082703,0.18766403198
BATT_MODEL_RAW:,572,5710.4132163,3.5401191711,3.3522377014,0.18788146973
BATT_MODEL_RAW:,573,5720.4141536,3.5395812988,3.3520011902,0.18758010864
BATT_MODEL_RAW:,574,5730.4143482,3.539100647,3.3514938354,0.18760681152
BATT_MODEL_RAW:,575,5740.4154554,3.5384750366,3.3507003784,0.1877746582
BATT_MODEL_RAW:,576,5750.4160131,3.5379447937,3.3502922058,0.18765258789
BATT_MODEL_RAW:,577,5760.4169623,3.5374412537,3.3500442505,0.18739700317
BATT_MODEL_RAW:,578,5770.4180763,3.5369415283,3.349445343,0.1874961853
BATT_MODEL_RAW:,579,5780.4185592,3.5362968445,3.3490028381,0.18729400635
BATT_MODEL_RAW:,580,5790.4190869,3.535736084,3.3483085632,0.18742752075
BATT_MODEL_RAW:,581,5800.4193488,3.5351867676,3.3478469849,0.18733978271
BATT_MODEL_RAW:,582,5810.4197636,3.5347137451,3.3473701477,0.18734359741
BATT_MODEL_RAW:,583,5820.4207908,3.5340461731,3.3466720581,0.18737411499
BATT_MODEL_RAW:,584,5830.4210559,3.53358078,3.3459892273,0.18759155273
BATT_MODEL_RAW:,585,5840.4221521,3.5329437256,3.3457679749,0.18717575073
BATT_MODEL_RAW:,586,5850.4228056,3.5323638916,3.3457298279,0.18663406372
BATT_MODEL_RAW:,587,5860.4230577,3.5318069458,3.3449897766,0.18681716919
BATT_MODEL_RAW:,588,5870.4234936,3.5312385559,3.3445205688,0.18671798706
BATT_MODEL_RAW:,589,5880.4237379,3.5306434631,3.3435821533,0.18706130981
BATT_MODEL_RAW:,590,5890.4242991,3.5300788879,3.3426399231,0.18743896484
BATT_MODEL_RAW:,591,5900.4252607,3.5294837952,3.342086792,0.18739700317
BATT_MODEL_RAW:,592,5910.4263167,3.5289611816,3.3413238525,0.1876373291
BATT_MODEL_RAW:,593,5920.4264605,3.5283164978,3.3407325745,0.18758392334
BATT_MODEL_RAW:,594,5930.4270946,3.5278167725,3.3402290344,0.18758773804
BATT_MODEL_RAW:,595,5940.4279413,3.527141571,3.3397483826,0.18739318848
BATT_MODEL_RAW:,596,5950.428292,3.5265579224,3.3391189575,0.18743896484
BATT_MODEL_RAW:,597,5960.4287355,3.5260162354,3.3383865356,0.18762969971
BATT_MODEL_RAW:,598,5970.4297347,3.5253410339,3.3375320435,0.18780899048
BATT_MODEL_RAW:,599,5980.4302038,3.5247764587,3.3369827271,0.18779373169
BATT_MODEL_RAW:,600,5990.4303759,3.5241241455,3.3363800049,0.18774414063
BATT_MODEL_RAW:,601,6000.4313329,3.5235862732,3.3364143372,0.18717193604
BATT_MODEL_RAW:,602,6010.4320477,3.5229187012,3.3360328674,0.18688583374
BATT_MODEL_RAW:,603,6020.4329585,3.5223350525,3.3353157043,0.18701934814
BATT_MODEL_RAW:,604,6030.4331833,3.5216331482,3.3346061707,0.18702697754
BATT_MODEL_RAW:,605,6040.4342101,3.5210037231,3.3333129883,0.18769073486
BATT_MODEL_RAW:,606,6050.4346998,3.5203666687,3.3322982788,0.18806838989
BATT_MODEL_RAW:,607,6060.4357505,3.5197257996,3.3314857483,0.18824005127
BATT_MODEL_RAW:,608,6070.4361077,3.5190887451,3.3302536011,0.18883514404
BATT_MODEL_RAW:,609,6080.4372722,3.5184288025,3.3292999268,0.18912887573
BATT_MODEL_RAW:,610,6090.437496,3.5178451538,3.3285255432,0.1893196106
BATT_MODEL_RAW:,611,6100.4382895,3.5171127319,3.3272895813,0.18982315063
BATT_MODEL_RAW:,612,6110.4384409,3.5164337158,3.3266448975,0.18978881836
BATT_MODEL_RAW:,613,6120.4386939,3.5157623291,3.325378418,0.19038391113
BATT_MODEL_RAW:,614,6130.4388455,3.5151519775,3.3245162964,0.19063568115
BATT_MODEL_RAW:,615,6140.4390324,3.5144577026,3.3241615295,0.1902961731
BATT_MODEL_RAW:,616,6150.4399449,3.5137138367,3.3232727051,0.19044113159
BATT_MODEL_RAW:,617,6160.4408773,3.5130081177,3.3229141235,0.19009399414
BATT_MODEL_RAW:,618,6170.4417085,3.512298584,3.3223342896,0.18996429443
BATT_MODEL_RAW:,619,6180.4422978,3.5116157532,3.3215065002,0.19010925293
BATT_MODEL_RAW:,620,6190.4432141,3.5108909607,3.320728302,0.19016265869
BATT_MODEL_RAW:,621,6200.4442863,3.5101509094,3.3196907043,0.19046020508
BATT_MODEL_RAW:,622,6210.4447966,3.5094223022,3.3193206787,0.19010162354
BATT_MODEL_RAW:,623,6220.4452613,3.5087471008,3.3179359436,0.19081115723
BATT_MODEL_RAW:,624,6230.4457464,3.5079231262,3.3159790039,0.19194412231
BATT_MODEL_RAW:,625,6240.446065,3.5071640015,3.3145484924,0.19261550903
BATT_MODEL_RAW:,626,6250.4471447,3.5064277649,3.3135871887,0.19284057617
BATT_MODEL_RAW:,627,6260.4475844,3.5057220459,3.3118629456,0.19385910034
BATT_MODEL_RAW:,628,6270.4479254,3.5048599243,3.3110656738,0.19379425049
BATT_MODEL_RAW:,629,6280.4488499,3.5040855408,3.3111000061,0.19298553467
BATT_MODEL_RAW:,630,6290.4497994,3.5033683777,3.3105964661,0.19277191162
BATT_MODEL_RAW:,631,6300.4501297,3.502494812,3.3085021973,0.19399261475
BATT_MODEL_RAW:,632,6310.4510714,3.5017318726,3.3086357117,0.19309616089
BATT_MODEL_RAW:,633,6320.4512741,3.5008621216,3.3077201843,0.19314193726
BATT_MODEL_RAW:,634,6330.4523382,3.500038147,3.3063774109,0.19366073608
BATT_MODEL_RAW:,635,6340.4530753,3.4992790222,3.30701828,0.19226074219
BATT_MODEL_RAW:,636,6350.4539234,3.4983711243,3.3064994812,0.19187164307
BATT_MODEL_RAW:,637,6360.4549595,3.4975204468,3.3056945801,0.1918258667
BATT_MODEL_RAW:,638,6370.455726,3.4966850281,3.3042831421,0.19240188599
BATT_MODEL_RAW:,639,6380.4559251,3.4958267212,3.3032989502,0.192527771
BATT_MODEL_RAW:,640,6390.4567627,3.4949607849,3.3024330139,0.192527771
BATT_MODEL_RAW:,641,6400.4575915,3.4940986633,3.3012390137,0.19285964966
BATT_MODEL_RAW:,642,6410.4582572,3.4932327271,3.3009529114,0.19227981567
BATT_MODEL_RAW:,643,6420.4589363,3.4923362732,3.3005371094,0.19179916382
BATT_MODEL_RAW:,644,6430.4594701,3.4915313721,3.2996177673,0.19191360474
BATT_MODEL_RAW:,645,6440.4596092,3.4905815125,3.2990913391,0.19149017334
BATT_MODEL_RAW:,646,6450.4604346,3.4897041321,3.2979660034,0.19173812866
BATT_MODEL_RAW:,647,6460.4607633,3.4888153076,3.2972831726,0.19153213501
BATT_MODEL_RAW:,648,6470.4611515,3.4879417419,3.2953834534,0.19255828857
BATT_MODEL_RAW:,649,6480.4617738,3.4870605469,3.293712616,0.19334793091
BATT_MODEL_RAW:,650,6490.462259,3.4861869812,3.2934684753,0.19271850586
BATT_MODEL_RAW:,651,6500.4629246,3.4853172302,3.2928237915,0.19249343872
BATT_MODEL_RAW:,652,6510.4633135,3.4844551086,3.2917022705,0.19275283813
BATT_MODEL_RAW:,653,6520.463974,3.4835853577,3.2911643982,0.19242095947
BATT_MODEL_RAW:,654,6530.4645489,3.4828224182,3.2905845642,0.192237854
BATT_MODEL_RAW:,655,6540.4654394,3.4819107056,3.290058136,0.19185256958
BATT_MODEL_RAW:,656,6550.4660994,3.4811401367,3.2897796631,0.19136047363
BATT_MODEL_RAW:,657,6560.466909,3.4802627563,3.2896003723,0.19066238403
BATT_MODEL_RAW:,658,6570.4672738,3.4794311523,3.2892456055,0.19018554688
BATT_MODEL_RAW:,659,6580.4680741,3.4786872864,3.2893028259,0.18938446045
BATT_MODEL_RAW:,660,6590.4687752,3.4778251648,3.2881202698,0.18970489502
BATT_MODEL_RAW:,661,6600.4689509,3.4770355225,3.2869224548,0.19011306763
BATT_MODEL_RAW:,662,6610.4691758,3.4762496948,3.2871742249,0.18907546997
BATT_MODEL_RAW:,663,6620.4693217,3.4754600525,3.2860145569,0.18944549561
BATT_MODEL_RAW:,664,6630.4701299,3.4747695923,3.2857894897,0.18898010254
BATT_MODEL_RAW:,665,6640.4712686,3.4739112854,3.2848472595,0.18906402588
BATT_MODEL_RAW:,666,6650.4716465,3.4731407166,3.2839775085,0.18916320801
BATT_MODEL_RAW:,667,6660.4725929,3.472366333,3.2834472656,0.18891906738
BATT_MODEL_RAW:,668,6670.4733932,3.471660614,3.2823600769,0.18930053711
BATT_MODEL_RAW:,669,6680.4743507,3.4708099365,3.2814903259,0.1893196106
BATT_MODEL_RAW:,670,6690.4746671,3.4700469971,3.2810287476,0.18901824951
BATT_MODEL_RAW:,671,6700.4751867,3.4692726135,3.2805900574,0.18868255615
BATT_MODEL_RAW:,672,6710.4761384,3.4685554504,3.2799339294,0.188621521
BATT_MODEL_RAW:,673,6720.4766208,3.4677772522,3.2790527344,0.18872451782
BATT_MODEL_RAW:,674,6730.4775554,3.4669036865,3.278263092,0.18864059448
BATT_MODEL_RAW:,675,6740.4782669,3.4661712646,3.2774162292,0.1887550354
BATT_MODEL_RAW:,676,6750.4786117,3.4652786255,3.2768783569,0.18840026855
BATT_MODEL_RAW:,677,6760.4788592,3.4645423889,3.2760162354,0.18852615356
BATT_MODEL_RAW:,678,6770.4793857,3.4636154175,3.2749481201,0.18866729736
BATT_MODEL_RAW:,679,6780.4800543,3.4627799988,3.2736625671,0.18911743164
BATT_MODEL_RAW:,680,6790.4811196,3.4620018005,3.2724952698,0.18950653076
BATT_MODEL_RAW:,681,6800.481592,3.4610519409,3.2710151672,0.19003677368
BATT_MODEL_RAW:,682,6810.481876,3.4601669312,3.2703094482,0.18985748291
BATT_MODEL_RAW:,683,6820.4828832,3.4592628479,3.2693939209,0.189868927
BATT_MODEL_RAW:,684,6830.4839092,3.4583778381,3.2677116394,0.19066619873
BATT_MODEL_RAW:,685,6840.4848913,3.4574394226,3.2666091919,0.19083023071
BATT_MODEL_RAW:,686,6850.4853412,3.4565010071,3.2658157349,0.19068527222
BATT_MODEL_RAW:,687,6860.486415,3.4555664063,3.2653999329,0.19016647339
BATT_MODEL_RAW:,688,6870.4875586,3.454624176,3.2647171021,0.18990707397
BATT_MODEL_RAW:,689,6880.4883348,3.4537086487,3.2635650635,0.19014358521
BATT_MODEL_RAW:,690,6890.4885872,3.4527168274,3.2628555298,0.18986129761
BATT_MODEL_RAW:,691,6900.4894706,3.4516716003,3.2621498108,0.18952178955
BATT_MODEL_RAW:,692,6910.4900318,3.4506530762,3.2611160278,0.18953704834
BATT_MODEL_RAW:,693,6920.4902848,3.4496459961,3.2602424622,0.18940353394
BATT_MODEL_RAW:,694,6930.4907929,3.4486198425,3.2597923279,0.18882751465
BATT_MODEL_RAW:,695,6940.4918846,3.4475784302,3.2588043213,0.18877410889
BATT_MODEL_RAW:,696,6950.492181,3.446521759,3.2576179504,0.18890380859
BATT_MODEL_RAW:,697,6960.4927105,3.4454574585,3.2569503784,0.18850708008
BATT_MODEL_RAW:,698,6970.4933823,3.4444503784,3.256362915,0.18808746338
BATT_MODEL_RAW:,699,6980.4941378,3.4433097839,3.2550048828,0.18830490112
BATT_MODEL_RAW:,700,6990.4945901,3.4422111511,3.2535591125,0.18865203857
BATT_MODEL_RAW:,701,7000.4949885,3.4411277771,3.2529258728,0.1882019043
BATT_MODEL_RAW:,702,7010.4960468,3.4399833679,3.252456665,0.18752670288
BATT_MODEL_RAW:,703,7020.4966079,3.4388580322,3.2510528564,0.18780517578
BATT_MODEL_RAW:,704,7030.4970782,3.4377288818,3.2505226135,0.18720626831
BATT_MODEL_RAW:,705,7040.4980243,3.4365882874,3.2492713928,0.18731689453
BATT_MODEL_RAW:,706,7050.4985116,3.4354171753,3.2480773926,0.18733978271
BATT_MODEL_RAW:,707,7060.4988093,3.4342651367,3.2462348938,0.18803024292
BATT_MODEL_RAW:,708,7070.4990776,3.4330787659,3.2449913025,0.18808746338
BATT_MODEL_RAW:,709,7080.5000097,3.4319534302,3.2438087463,0.18814468384
BATT_MODEL_RAW:,710,7090.5011523,3.4306907654,3.2426452637,0.18804550171
BATT_MODEL_RAW:,711,7100.5016306,3.4294700623,3.2411231995,0.18834686279
BATT_MODEL_RAW:,712,7110.5027395,3.4282264709,3.2397880554,0.18843841553
BATT_MODEL_RAW:,713,7120.5036729,3.4269866943,3.2388725281,0.18811416626
BATT_MODEL_RAW:,714,7130.5039091,3.4257316589,3.2378463745,0.18788528442
BATT_MODEL_RAW:,715,7140.5041887,3.4244613647,3.2362670898,0.1881942749
BATT_MODEL_RAW:,716,7150.5046,3.4231758118,3.2353553772,0.18782043457
BATT_MODEL_RAW:,717,7160.5049492,3.4219169617,3.2342300415,0.18768692017
BATT_MODEL_RAW:,718,7170.5051739,3.4205780029,3.2326622009,0.187915802
BATT_MODEL_RAW:,719,7180.5057113,3.4192504883,3.2312202454,0.18803024292
BATT_MODEL_RAW:,720,7190.5066248,3.4179229736,3.2299537659,0.18796920776
BATT_MODEL_RAW:,721,7200.507504,3.4165611267,3.2286911011,0.18787002563
BATT_MODEL_RAW:,722,7210.5081853,3.4152526855,3.2276725769,0.18758010864
BATT_MODEL_RAW:,723,7220.5093332,3.413860321,3.2265357971,0.18732452393
BATT_MODEL_RAW:,724,7230.5102767,3.4124031067,3.2253952026,0.18700790405
BATT_MODEL_RAW:,725,7240.5107426,3.4109573364,3.2237701416,0.18718719482
BATT_MODEL_RAW:,726,7250.5113117,3.4095840454,3.2223205566,0.18726348877
BATT_MODEL_RAW:,727,7260.5119086,3.4080467224,3.2206497192,0.18739700317
BATT_MODEL_RAW:,728,7270.5128059,3.4065589905,3.2191123962,0.18744659424
BATT_MODEL_RAW:,729,7280.5132808,3.4050598145,3.2174377441,0.18762207031
BATT_MODEL_RAW:,730,7290.5142153,3.403503418,3.2157402039,0.18776321411
BATT_MODEL_RAW:,731,7300.5149241,3.4019355774,3.2140579224,0.18787765503
BATT_MODEL_RAW:,732,7310.5159176,3.4003410339,3.2127380371,0.18760299683
BATT_MODEL_RAW:,733,7320.5162453,3.3987579346,3.2110214233,0.18773651123
BATT_MODEL_RAW:,734,7330.5172238,3.3970603943,3.2093353271,0.18772506714
BATT_MODEL_RAW:,735,7340.517424,3.3953514099,3.2080841064,0.18726730347
BATT_MODEL_RAW:,736,7350.5177572,3.3935966492,3.2064552307,0.18714141846
BATT_MODEL_RAW:,737,7360.5189183,3.3917884827,3.2047996521,0.18698883057
BATT_MODEL_RAW:,738,7370.5199273,3.3900222778,3.2026939392,0.18732833862
BATT_MODEL_RAW:,739,7380.5201093,3.3880310059,3.2005653381,0.18746566772
BATT_MODEL_RAW:,740,7390.5209667,3.3860397339,3.198890686,0.18714904785
BATT_MODEL_RAW:,741,7400.5217972,3.3839683533,3.1966171265,0.18735122681
BATT_MODEL_RAW:,742,7410.5226953,3.3818092346,3.1943740845,0.18743515015
BATT_MODEL_RAW:,743,7420.5230502,3.3795433044,3.1920204163,0.18752288818
BATT_MODEL_RAW:,744,7430.5234532,3.377243042,3.1897506714,0.18749237061
BATT_MODEL_RAW:,745,7440.5239176,3.3746299744,3.1872901917,0.18733978271
BATT_MODEL_RAW:,746,7450.5250145,3.3719673157,3.1845932007,0.18737411499
BATT_MODEL_RAW:,747,7460.5256786,3.3691253662,3.1818504333,0.18727493286
BATT_MODEL_RAW:,748,7470.5262382,3.3660888672,3.1789398193,0.18714904785
BATT_MODEL_RAW:,749,7480.5263848,3.3628540039,3.1758117676,0.18704223633
BATT_MODEL_RAW:,750,7490.5270744,3.3593826294,3.172542572,0.18684005737
BATT_MODEL_RAW:,751,7500.5274617,3.3556747437,3.168964386,0.18671035767
BATT_MODEL_RAW:,752,7510.5283428,3.3516807556,3.1651725769,0.18650817871
BATT_MODEL_RAW:,753,7520.5286212,3.347442627,3.1611099243,0.18633270264
BATT_MODEL_RAW:,754,7530.5292174,3.3429069519,3.1567611694,0.18614578247
BATT_MODEL_RAW:,755,7540.5303806,3.3381500244,3.1519126892,0.18623733521
BATT_MODEL_RAW:,756,7550.5305475,3.3329544067,3.1469802856,0.18597412109
BATT_MODEL_RAW:,757,7560.5310287,3.3275146484,3.1416168213,0.18589782715
BATT_MODEL_RAW:,758,7570.531172,3.3217544556,3.1357040405,0.18605041504
BATT_MODEL_RAW:,759,7580.5313574,3.3156814575,3.1293029785,0.186378479
BATT_MODEL_RAW:,760,7590.5318214,3.3093032837,3.1225395203,0.18676376343
BATT_MODEL_RAW:,761,7600.532926,3.3026695251,3.1158218384,0.18684768677
BATT_MODEL_RAW:,762,7610.533952,3.2955551147,3.1085548401,0.18700027466
BATT_MODEL_RAW:,763,7620.5349241,3.2882041931,3.1014595032,0.18674468994
BATT_MODEL_RAW:,764,7630.5356491,3.2804870605,3.0941123962,0.18637466431
BATT_MODEL_RAW:,765,7640.5363102,3.2724456787,3.0860290527,0.18641662598
BATT_MODEL_RAW:,766,7650.5367257,3.2640686035,3.0777359009,0.18633270264
BATT_MODEL_RAW:,767,7660.5378271,3.2554244995,3.0689544678,0.18647003174
BATT_MODEL_RAW:,768,7670.5383546,3.2462425232,3.0595283508,0.18671417236
BATT_MODEL_RAW:,769,7680.5393808,3.2367858887,3.0498886108,0.18689727783
BATT_MODEL_RAW:,770,7690.5402193,3.2269935608,3.0403633118,0.18663024902
BATT_MODEL_RAW:,771,7700.5410812,3.2166366577,3.0303268433,0.18630981445
BATT_MODEL_RAW:,772,7710.5420372,3.2059288025,3.0196228027,0.18630599976
BATT_MODEL_RAW:,773,7720.5430585,3.1948776245,3.0089645386,0.18591308594
BATT_MODEL_RAW:,774,7730.5438031,3.1831436157,2.9977035522,0.18544006348
BATT_MODEL_RAW.capacity:,2.1473732786

BATT_MODEL:,Index,Timestamp,Voc,Vload,ESR
BATT_MODEL:,1,7730.5023325,3.1831436157,2.9977035522,0.18544006348
BATT_MODEL:,2,7650.495255,3.2640686035,3.0777359009,0.18633270264
BATT_MODEL:,3,7580.4898867,3.3156814575,3.1293029785,0.186378479
BATT_MODEL:,4,7500.4859911,3.3556747437,3.168964386,0.18671035767
BATT_MODEL:,5,7420.4815796,3.3795433044,3.1920204163,0.18752288818
BATT_MODEL:,6,7340.4759533,3.3953514099,3.2080841064,0.18726730347
BATT_MODEL:,7,7270.4713352,3.4065589905,3.2191123962,0.18744659424
BATT_MODEL:,8,7190.4651542,3.4179229736,3.2299537659,0.18796920776
BATT_MODEL:,9,7110.4612688,3.4282264709,3.2397880554,0.18843841553
BATT_MODEL:,10,7030.4556075,3.4377288818,3.2505226135,0.18720626831
BATT_MODEL:,11,6960.4512398,3.4454574585,3.2569503784,0.18850708008
BATT_MODEL:,12,6880.4468641,3.4537086487,3.2635650635,0.19014358521
BATT_MODEL:,13,6800.4401214,3.4610519409,3.2710151672,0.19003677368
BATT_MODEL:,14,6730.4360847,3.4669036865,3.278263092,0.18864059448
BATT_MODEL:,15,6650.4301758,3.4731407166,3.2839775085,0.18916320801
BATT_MODEL:,16,6570.4258032,3.4794311523,3.2892456055,0.19018554688
BATT_MODEL:,17,6490.4207883,3.4861869812,3.2934684753,0.19271850586
BATT_MODEL:,18,6420.4174656,3.4923362732,3.3005371094,0.19179916382
BATT_MODEL:,19,6340.4116047,3.4992790222,3.30701828,0.19226074219
BATT_MODEL:,20,6260.4061137,3.5057220459,3.3118629456,0.19385910034
BATT_MODEL:,21,6180.4008271,3.5116157532,3.3215065002,0.19010925293
BATT_MODEL:,22,6110.3969702,3.5164337158,3.3266448975,0.18978881836
BATT_MODEL:,23,6030.3917126,3.5216331482,3.3346061707,0.18702697754
BATT_MODEL:,24,5950.3868213,3.5265579224,3.3391189575,0.18743896484
BATT_MODEL:,25,5870.3820229,3.5312385559,3.3445205688,0.18671798706
BATT_MODEL:,26,5800.3778782,3.5351867676,3.3478469849,0.18733978271
BATT_MODEL:,27,5720.3726829,3.5395812988,3.3520011902,0.18758010864
BATT_MODEL:,28,5640.3685612,3.5438766479,3.3568725586,0.18700408936
BATT_MODEL:,29,5570.3644598,3.5475883484,3.3607673645,0.18682098389
BATT_MODEL:,30,5490.3581199,3.5517692566,3.3647460938,0.18702316284
BATT_MODEL:,31,5410.3526477,3.5559272766,3.3682365417,0.18769073486
BATT_MODEL:,32,5330.3490065,3.5600547791,3.3718261719,0.18822860718
BATT_MODEL:,33,5260.3454953,3.5636558533,3.3746986389,0.18895721436
BATT_MODEL:,34,5180.3399209,3.5677833557,3.3775138855,0.19026947021
BATT_MODEL:,35,5100.3338004,3.5719070435,3.3792114258,0.19269561768
BATT_MODEL:,36,5020.3284673,3.5760612488,3.3851165771,0.19094467163
BATT_MODEL:,37,4950.3238036,3.5797309875,3.3886566162,0.19107437134
BATT_MODEL:,38,4870.3171038,3.5839576721,3.3920021057,0.19195556641
BATT_MODEL:,39,4790.3123993,3.5882301331,3.3962783813,0.19195175171
BATT_MODEL:,40,4720.3081082,3.5920219421,3.4002037048,0.1918182373
BATT_MODEL:,41,4640.3030044,3.596446991,3.4055938721,0.1908531189
BATT_MODEL:,42,4560.2979827,3.6009063721,3.4109649658,0.18994140625
BATT_MODEL:,43,4480.2911561,3.6054916382,3.4137382507,0.19175338745
BATT_MODEL:,44,4410.2865592,3.6095962524,3.4183425903,0.19125366211
BATT_MODEL:,45,4330.2826574,3.6144065857,3.4228401184,0.19156646729
BATT_MODEL:,46,4250.2790521,3.6194038391,3.4277229309,0.1916809082
BATT_MODEL:,47,4170.2734041,3.624622345,3.4321784973,0.19244384766
BATT_MODEL:,48,4100.2684884,3.6291923523,3.43516922,0.19402313232
BATT_MODEL:,49,4020.262949,3.6346702576,3.4436836243,0.1909866333
BATT_MODEL:,50,3940.2600573,3.6403808594,3.4491043091,0.19127655029
BATT_MODEL:,51,3870.255967,3.645614624,3.4542388916,0.19137573242
BATT_MODEL:,52,3790.2505537,3.6516342163,3.4583282471,0.19330596924
BATT_MODEL:,53,3710.2434579,3.6579742432,3.4643211365,0.19365310669
BATT_MODEL:,54,3630.2397692,3.6645507813,3.470085144,0.19446563721
BATT_MODEL:,55,3560.2343206,3.6704673767,3.4765357971,0.19393157959
BATT_MODEL:,56,3480.2293462,3.6774291992,3.4845237732,0.19290542603
BATT_MODEL:,57,3400.2235117,3.6846618652,3.4928741455,0.19178771973
BATT_MODEL:,58,3320.2170971,3.6920700073,3.5010566711,0.19101333618
BATT_MODEL:,59,3250.2126723,3.6987800598,3.5081672668,0.19061279297
BATT_MODEL:,60,3170.2072283,3.7066574097,3.5154685974,0.19118881226
BATT_MODEL:,61,3090.203365,3.7147750854,3.522983551,0.19179153442
BATT_MODEL:,62,3010.1978829,3.7231254578,3.5304489136,0.19267654419
BATT_MODEL:,63,2940.1925807,3.7306194305,3.5372200012,0.19339942932
BATT_MODEL:,64,2860.1871489,3.7393894196,3.5455665588,0.19382286072
BATT_MODEL:,65,2780.1818723,3.7484016418,3.5550079346,0.19339370728
BATT_MODEL:,66,2710.1772936,3.756526947,3.5627861023,0.19374084473
BATT_MODEL:,67,2630.1715575,3.7659835815,3.5727539063,0.19322967529
BATT_MODEL:,68,2550.1663929,3.7755336761,3.5819396973,0.19359397888
BATT_MODEL:,69,2470.1620716,3.7853775024,3.5906791687,0.19469833374
BATT_MODEL:,70,2400.1568358,3.7941417694,3.5993118286,0.1948299408
BATT_MODEL:,71,2320.1529477,3.8042888641,3.6109542847,0.19333457947
BATT_MODEL:,72,2240.1471752,3.8145847321,3.6215705872,0.1930141449
BATT_MODEL:,73,2160.1415736,3.8250637054,3.6324691772,0.1925945282
BATT_MODEL:,74,2090.1371947,3.8343429565,3.6415977478,0.19274520874
BATT_MODEL:,75,2010.1312419,3.8450679779,3.6519050598,0.19316291809
BATT_MODEL:,76,1930.1249658,3.8559169769,3.6642227173,0.19169425964
BATT_MODEL:,77,1860.1215998,3.865530014,3.6738624573,0.19166755676
BATT_MODEL:,78,1780.1173893,3.876625061,3.6841316223,0.19249343872
BATT_MODEL:,79,1700.1114753,3.8878517151,3.6978263855,0.19002532959
BATT_MODEL:,80,1620.1064592,3.8992595673,3.7103500366,0.18890953064
BATT_MODEL:,81,1550.1028573,3.9091949463,3.7194442749,0.18975067139
BATT_MODEL:,82,1470.097828,3.9207458496,3.7322006226,0.18854522705
BATT_MODEL:,83,1390.0930733,3.9324913025,3.7445220947,0.18796920776
BATT_MODEL:,84,1310.0881101,3.9442367554,3.7564506531,0.18778610229
BATT_MODEL:,85,1240.085097,3.9545288086,3.7662220001,0.18830680847
BATT_MODEL:,86,1160.079997,3.9664745331,3.7780456543,0.18842887878
BATT_MODEL:,87,1080.0760778,3.9785480499,3.7892799377,0.18926811218
BATT_MODEL:,88,1000.0702689,3.9907302856,3.7987918854,0.19193840027
BATT_MODEL:,89,930.06524628,4.0014419556,3.810968399,0.19047355652
BATT_MODEL:,90,850.06038216,4.0137844086,3.8256187439,0.18816566467
BATT_MODEL:,91,770.0545804,4.0262413025,3.8378829956,0.18835830688
BATT_MODEL:,92,700.05210628,4.0372390747,3.8506469727,0.18659210205
BATT_MODEL:,93,620.04607256,4.0499191284,3.8636035919,0.1863155365
BATT_MODEL:,94,540.04115066,4.0627784729,3.8778133392,0.18496513367
BATT_MODEL:,95,460.03466876,4.0756912231,3.8884849548,0.18720626831
BATT_MODEL:,96,390.02843914,4.087266922,3.8982963562,0.1889705658
BATT_MODEL:,97,310.02171272,4.1007957458,3.9093151093,0.1914806366
BATT_MODEL:,98,230.01602688,4.1148509979,3.9226436615,0.19220733643
BATT_MODEL:,99,150.01011568,4.1300601959,3.936498642,0.19356155396
BATT_MODEL:,100,80.00569268,4.1461925507,3.9474830627,0.19870948792
BATT_MODEL:,101,0,4.1869735718,3.9285964966,0.2583770752
BATT_MODEL.capacity:,2.1474

 

 

I wrote a short Python program (Battery.py) to process and plot the data:

 

image

 

 

The plot shows that the battery ESR stayed relatively constant at around 200 mΩ while the battery voltage dropped in a very predictable way as the battery lost charge. Besides being able to simulate a battery, the generated data can be used to compare batteries of different brands to evaluate which is better or also to evaluate how much a battery has degraded from its usage. Higher capacity and lower ESR make the battery better, but the ESR may not always be relevant. At high currents the ESR can cause a major waste of energy, but at very low currents it may have almost no negative effect, and other characteristics such as the self-discharge rate may become more relevant when deciding what type of battery to use.

  • Sign in to reply

Top Comments

  • neuromodulator
    neuromodulator over 6 years ago in reply to jw0752 +2
    Thanks you John. I would think you should be able to do something like this if you are using a programmable electronic load.
  • jw0752
    jw0752 over 6 years ago +1
    Hi, I really enjoyed your post. I too have been testing 18650s of different brands and mAh ratings to see what is going on with them. I have been timing a discharge from full to 2.8 volts at a 1 A discharge…
  • jw0752
    jw0752 over 6 years ago in reply to neuromodulator +1
    Much of my test gear has been built by me and lacks the sophistication of commercial units. To do my battery tests I have an electronic load that I built but it isn't programmable and I use another piece…
  • jw0752
    jw0752 over 6 years ago in reply to neuromodulator

    Yes I can do that.

    Thanks for your guidance.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neuromodulator
    neuromodulator over 6 years ago in reply to jw0752

    I see, but would it be that hard to disconnect the load to measure Voc and the ESR automatically while it discharges?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 6 years ago in reply to neuromodulator

    Much of my test gear has been built by me and lacks the sophistication of commercial units. To do my battery tests I have an electronic load that I built but it isn't programmable and I use another piece of equipment that monitors a voltage, times it as it approaches a target voltage and then stores the elapsed time until I request it.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neuromodulator
    neuromodulator over 6 years ago in reply to jw0752

    Thanks you John. I would think you should be able to do something like this if you are using a programmable electronic load.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 6 years ago

    Hi,

    I really enjoyed your post. I too have been testing 18650s of different brands and mAh ratings to see what is going on with them. I have been timing a discharge from full to 2.8 volts at a 1 A discharge rate. This data will give me the batteries mAh at the 1 amp discharge rate. It would be nice to have the additional data your Keithly supplies but for me I will have to be satisfied with what I have. Thanks for your post.

     

    John