RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Review Blogs LED Road Test - Vehicle Situational Awareness System Indoor Demo - Blog 12 Dec 20
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: dougw
  • Date Created: 20 Dec 2015 8:29 AM Date Created
  • Views 801 views
  • Likes 2 likes
  • Comments 2 comments
Related
Recommended
  • vehicle_situational_awareness_system
  • lighting
  • ledroadtestplus
  • würth
  • texas_instruments
  • vsas
  • led_road_test

LED Road Test - Vehicle Situational Awareness System Indoor Demo - Blog 12 Dec 20

dougw
dougw
20 Dec 2015

This blog will mainly consist of a video demonstration of the V-SAS in an indoor setting. The previous blog (#11) covered the system objectives and features. There will be a third blog in this mini-series to demonstrate operation of the system in a vehicle.

 

Ultrasonic Distance Sensing

Ultrasonic sensors need to be very sensitive to detect distant reflections off small objects, but this makes them very prone to detection of spurious noise and pressure variations. To prevent these spurious detections from confusing the readings some signal processing is normally required. A simple low-pass filter on the distance readings can minimize the possibility of showing a full-scale reading, but it also means that any spurious signal will influence good data and make it less accurate. A better solution is to take several readings and choose the median reading as the most accurate reading. This solution will tend to ignore full scale spurious readings at either end of the scale. I found this works reasonably well, but it does require a fairly complicated algorithm to find the median reading. In my limited testing, the sensor seems to detect a lot more spurious “short” reflections than long reflections, so it may be more effective to choose a reading above the median reading. Currently, I am using the largest of 3 readings as the most accurate choice, and this is performing better than choosing the median reading. If I go to 5 readings, the median is likely to be better than the largest, but it also slows down response of the system. So far, I think I would rather use my brain to help ignore spurious readings than allow the system to take more time to present better data. In applications where the machine must be correct without human help, a different approach would be used.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The LED Road Test page is here:

http://www.element14.com/community/roadTests/1481


The Lighting Group page is here:

Lighting


Here are links to my other blog entries for this road test:

LED Road Test - Proposal - Blog 0 Jan 1, 2016

Light Emitting Diodes Road Test - Blog 1 Nov 1

LED Road Test - 3D Printed Housings - blog 2 Nov 10

LED Road Test - Dodecahedron Light Fixture  Blog 3 Nov12

LED Road Test - Wearable Interactive Lights - Blog 4 - Nov 13

LED Road Test - Interactive Trophy - Blog 5 Nov 16

LED Road Test - Making Household Objects Interactive - Blog 6 Nov 22

LED Road Test - Power LEDs - Up & Running - Blog 7 Nov 24

LED Road Test - Star Wars - The Force Awakens - Blog 8 Nov 28

LED Road Test - Selfie Phenomenon - Blog 9 Nov 29

LED Road Test - MSP EXP430FR4133 Launchpad IDE - Blog 10 Dec 6

LED Road Test - Vehicle Situational Awareness System Blog 11 Dec 14

LED Road Test - Vehicle Situational Awareness System Indoor Demo - Blog 12 Dec 20

LED Road Test - Maple Leaf Christmas Decoration - Blog 13 Dec 24

LED Road Test - Vehicle Situational Awareness System - Detecting the Borg in the Driveway - Blog 14 Dec 26

LED Road Test - Reflow Soldering Power LEDs - Blog 15 Jan 10

LED Road Test - Induction Heating Reflow Soldering - Blog 16 Jan12

LED Road Test - Summary - Blog 17 Jan 15

 

Associated Video Links

LED Road Test Unboxing

MSP-EXP430FR4133 Demo

BLE LED Power On Test

BLE LED 3D Printed Housings 2

Dodecahedron Light Fixture

Creating a Light Fixture using 123D Design

Wearable Interactive Arc Reactor

Interactive Trophy

Interactive Illuminated Household Objects

Power LEDs Thermal Discussion

LED Ring Light

Star Wars - Let The Force Be With The Light

CCS Cloud Basics

UltrasonicDistanceMeter-Boot

VSAS Indoor Demo

Maple Leaf BLE LED Decoration

Maple Leaf CAD design

Vehicle Situational Awareness System in Operation

Vehicle Situational Awareness System Operating at Night

Reflow Soldering SMT LEDs

Induction Heating Reflow Soldering


  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 10 years ago +1
    dougw , seems we're working on similar subjects. You're ultrasonically sensing distances. I'm busy with ultrasonic liquid hight measurements and identification. You suggested that I should include distance…
  • DAB
    DAB over 10 years ago +1
    Nice update Douglas. I am very interested in your air based distance measurement tests. DAB
  • DAB
    DAB over 10 years ago

    Nice update Douglas.

     

    I am very interested in your air based distance measurement tests.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago

    dougw, seems we're working on similar subjects. You're ultrasonically sensing distances. I'm busy with ultrasonic liquid hight measurements and identification.

     

    You suggested that I should include distance measurements while doing the TI UltraSonic Sensor roadtest. Unfortunately, the piezo transducer that I have is 1 MHz - ideal for liquids but out of range for measurements in gas (e.g.: air).

    Glad to see that you picked up distance measurement in your roadtest.