RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs Microchip CAN Analyzer Road Test - part 4: Advanced Functions
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: Jan Cumps
  • Date Created: 29 Oct 2017 8:23 PM Date Created
  • Views 1230 views
  • Likes 3 likes
  • Comments 4 comments
Related
Recommended
  • RoadTest
  • microchip
  • bus
  • automotive
  • hercules
  • can

Microchip CAN Analyzer Road Test - part 4: Advanced Functions

Jan Cumps
Jan Cumps
29 Oct 2017

This was supposed to be my 4th blog. Discussing advanced topics such as triggers, filters, multiple messages.

But this is when the Microchip CAN Analyzer didn't perform to its advertised specs.

 

Good Basic functionality

The device performed perfectly when doing basic analysis. It performed well on logic level and on physical bus level. Receiving, Sending and logging work just fine.
Some additional features such as terminating the line via software, changing frequency and set the device to listen-only mode are a big asset. So far so good.

It's perfectly usable in that context. Not a single failure. Not a single let-down.

 

Advertised Functionality not Implemented

The disappointment comes when moving to the advanced functions. They are not implemented.

It feels like an abandoned device. Functionality that's key to make it useful as a real can bus development and test utility (group message) are announced as "to be implemented as a future functionality" in 2010.

That's a pity but acceptable. No commitments were made, so I can't complain.

Functionality that's mentioned on the product page and user manual (triggers, filters in the GUI) are not implemented. I have no words for that.

Microchip has had 7 years to work on that or remove the features from the product page and User Manual. Customers have been asking them since 2010. They gave up in 2012.

 

This is a Road Test, so I hope that Microchip will chime in and correct me. I will check - hope I stand corrected ...

 

 

Road Test Blog
part 1: First trials
part 2: Inject CAN Messages
part 3: Analyzer as Test Tool
part 4: Advanced Functions
Related Blog
part 1: tryout
part 2: Communication between 2 Devices
part 3a: Design a Bus Driver PCB
part 3b: Design a Bus Driver PCB - Schematics and Custom Components
part 3c: Design a Bus Driver PCB - Layout
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 8 years ago in reply to mcb1 +1
    I have the same versions as you for all components, mcb1 . These funtions are listed on the product page or on the summary of features in the manual.
  • kas.lewis
    kas.lewis over 8 years ago in reply to Jan Cumps +1
    This disappointing to hear, someone may want the product because of these features. Low cost and has the needed functionality... then you buy it and oops, doesn't work as advertised... Kas
  • mcb1
    mcb1 over 8 years ago in reply to Jan Cumps +1
    Jan Cumps Just for fun I loaded ver2 to see if there were changes. Interestingly the source files are all in where the program is installed. I've only had a quick look, but they do include a guide to load…
  • mcb1
    mcb1 over 8 years ago in reply to Jan Cumps

    Jan Cumps

    Just for fun I loaded ver2 to see if there were changes.

     

    Interestingly the source files are all in where the program is installed.

    I've only had a quick look, but they do include a guide to load them and the PC Application is there as well.

     

    Maybe the ability to add the feature is somewhere, they have forms for the Group transmit function.

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kas.lewis
    kas.lewis over 8 years ago in reply to Jan Cumps

    This disappointing to hear, someone may want the product because of these features. Low cost and has the needed functionality... then you buy it and oops, doesn't work as advertised...

     

    Kas

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to mcb1

    I have the same versions as you for all components, mcb1 . These funtions are listed on the product page or on the summary of features in the manual.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 8 years ago

    There is actually two future features.

    Group send and Filter Trigger.

     

    Software is from 2014

    image

     

    Jan Cumps

    You may also be interested in these patches for Linux.

    https://github.com/rkollataj/mcba_usb

     

    Mark