RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs Microchip PoE to USB-C®︎ Power and Data Adapter RoadTest: What is PoE?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: colporteur
  • Date Created: 15 Jun 2021 1:50 AM Date Created
  • Views 2681 views
  • Likes 4 likes
  • Comments 4 comments
Related
Recommended

Microchip PoE to USB-C®︎ Power and Data Adapter RoadTest: What is PoE?

colporteur
colporteur
15 Jun 2021

image

 

I received noticed from UPS that there is a package on route to me. I will assume it is the equipment for this RoadTest. I have no other items I am waiting to receive. I didn't click the link to confirm. I'm hoping it not just a UPS related phishing attempt. Oh well, let's post some theory for this RoadTest in the mean time.

 

What is Power over Ethernet (PoE) as it relates to this device. With the Microchip PoE, a USB-C powered device can get power over the same cable that carries network data. In Scenario A drawing, the Network switch is designed to provide power and data over the network cable. In the top drawing, the Microchip PoE device is interfacing the power and data to the Pi Zero. In the lower pictorial from Scenario A, you have a Pi with a PoE HAT that interfaces power and data to the Pi4B+.

 

Some additional details in the scenario. The devices are attached back to the Network Switch on 100 meters of CAT 6. The Network Switch is connected to a device that provides Internet access. In this case a Internet Gateway. The Pi Zero or Pi4B+ can gain access the Internet over the cable and be powered from that same cable.

 

In Scenario B, the PoE support network switch is replaced with a regular switch. A regular switch doesn't supply PoE power on it outputs. To support this design a PoE injector or PoE power supply is added to the circuit. The injector provides the power out to the end devices. The PoE injector takes data connection on one side and feeds power and data out the other connection. The PoE injector is plugged into a wall outlet to get it power.

 

To complete this RoadTest Scenario B will be used with a TP-Link Gigabit PoE injector TL-POE150S deployed. Not all PoE power providing devices are the same. I have another PoE power supply that I have used in the past The Road to Raspberry Pi4B/ PoE Hat RoadTest Review (power supply) . I discovered the device limits the data throughput on the network to 100Mb's, down from 1G. Since this RoadTest includes a data components, The TP-Link injector is the being used to ensure the highest data throughput.

 

Hey wait a minute, a Pi Zero doesn't have an Ethernet connection! Besides it's power is via a USB mini and not USB-C connector. The different power connectors can easily be accommodated with adapators. The data requires something more. That is where On-The-Go (OTG) technology comes into play.

 

The PiZero power connector supports a data output. The same can be said for the Pi4B+. The power connector (USB mini for PiZero and USB-C for the Pi4B+) has data capabilitie using OTG. The initial blog post for this RoadTest Microchip PoE to USB-CRegistered Power and Data Adapter RoadTest Review Introduction provides some insight.

 

I am hoping (again not sure), the Pi OTG will provide a network data connection. That would enable a wired network to a PiZero. It also would provide a wired network connection to the Pi4B+ without using the Ethernet adaptor.

 

In addition to achieving data connection, the end device needs to be loaded down so it draws maximum power from it's supply. The network cable has considerable length, this provides resistance that can impact power. Creating a heavy load on the end device ensures all the components in the chain work effectively if the end device is to function correctly. The TP-Link injector has been used in the past as a power source with good success. Will the Mircochip PoE supply added to the chain, can it supply the needed power?

  • Sign in to reply
  • colporteur
    colporteur over 5 years ago in reply to DAB

    Great suggestion. I will include two different cables in the power test.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 5 years ago in reply to colporteur

    Hi Sean,

     

    If you have a shorter cable, you can use it and the long one to see how much they affect performance and power loss over distance.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 5 years ago in reply to DAB

    I'm trying to keep the variables that change to a minimum. My plan is to use a 328ft piece of CAT6 I built for the PoE Hat review. I know it worked and should work for this test.

     

    The stickler is going to be data and Pi OTG. Question: If you configure OGT on the Pi and assign the interface an IP, can this be supported through the Microchip PoE. If it does, the the PiZero has a wired network interface. The is a very big if!

     

    I don't have any cable longer that the 328ft piece sorry.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 5 years ago

    I look forward to your test report.

     

    I would also be interested in how far away you can run the cable and still get good power and communication with a distributed RPi.

     

    DAB