RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs Multipurpose Modular Light Bar Project: [03] Shopping for Parts
  • Blogs
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: ipv1
  • Date Created: 25 Nov 2015 5:25 PM Date Created
  • Views 838 views
  • Likes 2 likes
  • Comments 2 comments
Related
Recommended
  • modular_led_light
  • ip_modular_light
  • ledroadtestplus
  • ip_iot

Multipurpose Modular Light Bar Project: [03] Shopping for Parts

ipv1
ipv1
25 Nov 2015

Intro

 

Its been the holiday week all last week with Diwali and stuff and family gatherings and such hence the delayed post. My focus has been on the shopping list since it usually takes LOOOOONG to get the needed parts and I have been successful in placing the request for samples from Wurth. The e13 shopping list is a different story altogether. Lets see if I can log this right.

 

A bit of background and progress report

 

My design uses the TPS92512 to drive a bunch of LEDs and the intensity is controlled via a CC3200. The objective is to have an RGB light that can replace commercial lighting. To bring down voltages to usable levels, I need an SMPS. No I will not be designing on because its a Design Challenge on its own BUT I will be doing something about that since I have long needed my own SMPS design. Hence I need an SMPS which does not fit into my budget from e14- therefore...Bought-out.

 

The Extra Bits

 

Additionally, I will be designing a PCB for the TPS92512 and the LEDs as well. I will getting it manufactured from seeedstudio’s Fusion service during the holidays. Still working on that part. The passives such as coils and Caps as well as the LEDs I can get from WE. I was able to get the sample request out to Wurth and I got a call from FedEX the third day of the email. That’s mind bogglingly fast! Kudos to the guys at Wurth Electronics for getting them shipped so fast. Brilliant!

 

Shopping from E14

 

I need a long list of parts such as the TPS92512 and some other LEDs which were not available from WE(Agricultural Grow lights types LEDs) and since I do not have a reflow soldering oven, I though I would make one so I need the parts for that as well. Next I thought I would get a BTLE solution just in case I wanna go from CC3200 to something else BUT the TI solution is just TOO expensive. I have some issues with placing an order request with element14 which should get resolved pretty soon as well.

 

What next?

 

I need to test out the PWM functionality with the TPS92512 as well as layout the PCB. This I need to fit into my freakishly busy schedule in the next week and I will prolly have a video in the next post for the unboxing of the parts I get from Wurth. Along with that I will be doing a description video of Wurth Electronics Kits which I have received in the past as a part of previous design challenges. So essentially my next post will be dedicated to Wurth Electronics. image

 

So thats it for now. Keeping building image

Cheers,

IP

  • Sign in to reply

Top Comments

  • ipv1
    ipv1 over 10 years ago in reply to gpolder +1
    Hi Gerrit, Yep! I am planning a four channel TPS board with individual control for each channel. I am going ahead with a variety of LEDs which I will show in the next blog vid which includes Whites, reds…
  • ipv1
    ipv1 over 10 years ago in reply to gpolder

    Hi Gerrit,

    Yep! I am planning a four channel TPS board with individual control for each channel. I am going ahead with a variety of LEDs which I will show in the next blog vid which includes Whites, reds, greens, blues and some different wavelength for the colors for use in a DIY Hydroponics system.

    I am planning a bar shaped panel and a small disc shape for the high wattage LEDs  which means I have two types of enclosures. The bar type will have a diffuser and will only be used for passive lighting while the disc ones will be fitted in a metallic enclosure with heatsinks and will be used for focused lighting.

     

    Will pass on the PCB layout at the end if you wanna use it but its basically the same as that of the EVM modules(times 4 and an MSP430 for control)

     

    IP

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gpolder
    gpolder over 10 years ago

    Hi Inderpreet,

     

    am I right, are you planning to use a separate TPS92512, next to the EVM we got?

    regarding the PCB, will that be for these WL-SWTC SMD White Top View Ceramic LED - Product Catalog LEDs ?

    I'm looking for a PCB too, just only the leds, to connect to the EVM. If possible it should be ring shaped.

     

    Gerrit.

    • Cancel
    • Vote Up 0 Vote Down