RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Review Blogs Omron HVC-P2 Roadtest - Getting Started
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: ralphjy
  • Date Created: 31 Aug 2018 1:24 AM Date Created
  • Views 1374 views
  • Likes 6 likes
  • Comments 4 comments
Related
Recommended
  • omron roadtest
  • image recognition

Omron HVC-P2 Roadtest - Getting Started

ralphjy
ralphjy
31 Aug 2018

I received my Omron Vision Sensor yesterday via UPS.  The box was so light that is seemed empty; but there was the kit wrapped in bubble wrap in a static bag.

image

The kit consists of a Camera board (25mm x 25mm) that is the size of an RPi camera and an image processor board (45mm x 45mm) connected with a 9cm flex cable..  I am going to have to print an enclosure to support and protect the boards so that I don't damage them in use.  The communication and power to the processor board is via a micro usb cable.

 

Front and back of processor board:

image

There appears to be a spot for a large IC that is not stuffed.  It would be interesting to know what capability could be added to this unit.

 

Front and back of camera board:

image

 

 

I did a quick test using the Evaluation Software on my Windows 10 PC.  The USB Driver for the board installed automatically on first connection.

 

Evaluation Software GUI:

image

 

The GUI is reasonably intuitive to use.  For my quick test I was only about 1m away from the camera.  With all the default settings I am getting poor repeatability with the image classifications.  There are quite a few settings in the classifier and I'm sure that it will take me a while to get up the learning curve.  Good news is that it appears that everything is basically functional.

 

Execution settings (default):

image

 

Stabilization settings (default):

image

 

My next step will be building a case for the unit.  Then I'll proceed to learning to operate it and testing it using the Evaluation GUI in the Windows environment.  And for my roadtest I'll deploy it with a RPi0W using python to evaluate its capability as a security sensor.

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 8 years ago +2
    Hi Ralph, This looks like an interesting road test. I will enjoy following you. The unit says your anger level is 44. Good thing the drivers loaded up right away or that might have been higher. John
  • ralphjy
    ralphjy over 8 years ago in reply to jw0752 +2
    Hi John, I couldn't get the GUI to resize so that it would show the whole output window without the scrollbars, but if you scrolled to the right it said my "sadness" level was 56. But I did think I looked…
  • fmilburn
    fmilburn over 8 years ago +2
    This should be interesting Happy
  • dixonselvan
    dixonselvan over 8 years ago

    This looks like an interesting road test, excited to see whats more in store!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 8 years ago

    This should be interesting image  Happy

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 8 years ago in reply to jw0752

    Hi John,

     

    I couldn't get the GUI to resize so that it would show the whole output window without the scrollbars, but if you scrolled to the right it said my "sadness" level was 56.  But I did think I looked more angry than sad....

     

    Ralph

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 8 years ago

    Hi Ralph,

    This looks like an interesting road test. I will enjoy following you. The unit says your anger level is 44. Good thing the drivers loaded up right away or that might have been higher.

    John