RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs Part 2: Load Regulation
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: waleedelmughrabi
  • Date Created: 22 Dec 2020 6:42 PM Date Created
  • Views 925 views
  • Likes 4 likes
  • Comments 2 comments
Related
Recommended
  • desktop power supply
  • r&s
  • r&s®ngp800
  • power supplies

Part 2: Load Regulation

waleedelmughrabi
waleedelmughrabi
22 Dec 2020

Part 2 of R&S NGP814 Power Supply - Review

 

It is important for any power supply to be able to maintain the output level independant of the load variation.

The NGP814 load regulation test is shown below.

 

image

image

Channel 1 @32V, 6.25A:

 

A- Using the built in multimeter in the DL3021

= [(31.9943V - 31.8313V) / (31.8313V) ] x 100% = 0.5120746%

image

 

B- Using DMM6500

= [ (32.00127V - 32.00333V) / (32.00333V) ] x 100% = - 0.00643683%

The negative value indicates a leading power factor (Capacitive load).

Figure below shows the behaviour at the moment of switching on the load.

image

@no load: Vripple P-P = 0.8 mV

@Full load: Vripple P-P = 0.82 mV (Corrected)

 

 

Channel 3 @64V, 3.125A:

 

A- Using the built in multimeter in the DL3021

= [(63.9909V - 63.9102V) / (63.9102V) ] x 100% = 0.126271%

 

image

 

B- Using DMM6500

= [ (64.00465V - 64.00836V) / (64.00836V) ] x 100% = - 0.00579612%

Same as channel 1 the negative value indicate a leading power factor.

Channel 3 also shows a dip in voltage at the moment of switching.

image

@no load: Vripple P-P = 1.6 mV

@Full load: Vripple P-P = 1.8 mV (Corrected)

 

 

It can be noticed that the built-in multimeter of the electronic load and the external multimeter have quiet a noticeable difference in the measured values.

Assuming that the dedicated DMM6500 is the more accurate of the two it shows a load regulation of about -0.006% which is an impressive value achieved by the NGP814.

 

One thing to notice about transient behaviour is the yellow circle in both graphs, that is the reading at the moment of switching on the load where the power supply jumps from No-Load to Full-Load.

This voltage dip is still tolerable, 2.5mV for the 32V range about 5mV for the 64V range, which shows that this voltage dip is proportional to the voltage of the test. The red circle still needs more investigation as it took about 12 seconds for the voltage to reach the accurate steady state.

  • Sign in to reply

Top Comments

  • DAB
    DAB over 5 years ago +2
    Nice test presentation. DAB
  • Gough Lui
    Gough Lui over 5 years ago +2
    Such tests are highly load dependent and the transient level is also dependent on your measuring equipment's sampling rate and potentially even the inductance of the cables. Traditionally, more accurate…
  • Gough Lui
    Gough Lui over 5 years ago

    Such tests are highly load dependent and the transient level is also dependent on your measuring equipment's sampling rate and potentially even the inductance of the cables. Traditionally, more accurate values may be derived using a DC electronic load capable of fast transients while observing the result on an oscilloscope, noting that the DC electronic load may have an overshoot at turn-on which may cause additional "sag" in the output, so if the DC electronic load has a current monitor output, that should also be checked.

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 5 years ago

    Nice test presentation.

     

    DAB