RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Review Blogs POST 3 What is in the box... Red Pitaya STEMlab 125-14 PRO Gen 2 Starter Kit
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: colporteur
  • Date Created: 17 Sep 2026 4:14 PM Date Created
  • Views 64 views
  • Likes 9 likes
  • Comments 14 comments
Related
Recommended
  • RoadTest
  • test equipment
  • red pitaya

POST 3 What is in the box... Red Pitaya STEMlab 125-14 PRO Gen 2 Starter Kit

colporteur
colporteur
17 Sep 2026

I've discovered that the documentation is significantly behind the product supplied for this RoadTest. I would have liked to provide the resource I discovered that my fellow RoadTester could use and not have to visit the dead end rabbit warrens that I have traveled.

image

It appears this is the unit used for the documentation. Notice next to the RJ45 connector the narrow silver case of a USB-A socket.

image

We are provided this unit. Note the USB is not present.

image

In addition, the kit comes with a QSPI eMCC module. It mates with the E3 connector on the board. This module promises to eliminate the need for the SD card, if it only worked!

I've discovered the firmware for this module has changed (as promised in documentation). I have been unsuccessful in trying to load the OS to this module in the current firmware version because of the watchdog timer. It reboots the OS when it fails to get a proper response. It has to be disabled to load the OS (through a USB port that doesn't exist) into the module. A github dev version I found appears to fix the issue.

The documentation is for the board I don't have so even if I solve the watchdog timer issue my board doesn't have the USB-A port to move the OS.

After backing out of the last warren run that ended in a dead end, I've sent an email to Red Pitaya support for assistance.

My intent was to get a stable Pitaya platform to pursue SDR objectives. A self contained bootable Pitaya I felt was a reasonable starting point. That would give me a chance to explore the setup and then investigate SDR. That setup part is proving to be a bit of a challenge.

Getting the OS working was a struggle. I'm going to park the module boot option until I get a response from support.

  • Sign in to reply
  • colporteur
    colporteur 26 days ago in reply to beacon_dave

    You have more gray matter in this area than myself BD. Through all my efforts the watchdog timer starts after approx 7 seconds. Even if I was to get it to stop, I'm not sure I can load the eMCC module. The latest response from an email I sent to tech support has encourage me to look at other objectives.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave 26 days ago in reply to obones

    I guess this is what they are referring to ?
    "...Modify the E3 module firmware source code to disable the watchdog timer check..."

    imagehttps://github.com/RedPitaya/RedPitaya-Examples/blob/main/E3_source_code/QSPI_eMMC_code.ino

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur 27 days ago in reply to obones

    I just received a reply from tech support regarding this. I'm going to post the questions I submitted via email and their response in another post. I'm not holding out but want to confirm some things first and capture some content. That and my questions were lengthy and I don't want to run this thread longer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • obones
    obones 30 days ago in reply to beacon_dave

    Ah boy, this documentation is a maze in and of itself.
    So, yes, connecting to the SSH console works (user/password are in yet another page deep down in the developer's guide)

    Then, sure, I can do that:

    root@rp-f0f9ca:~# e3_i2c_controller -r -v
    HW ID = 0x01
    Data = 0x02 - PWR_ON

    but that does not help much, and the documentation for the E3 module is not giving more information either about a watchdog so I guess it's not there yet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • obones
    obones 30 days ago in reply to colporteur

    Yeah, I get that feeling, and came to the conclusion that the eMMC module is out of my league for the time being.

    I installed HPSDR, and I'm seeing communication with the SDR Transceiver app but for the life of me, I can't figure out how to change the center frequency in HPSDR.

    So, I went back to SDRAngel that I'm more used to, but the SoapySDR input does not show up despite having installed PothosSDR, and that led to this question: https://github.com/f4exb/sdrangel/discussions/2938#discussioncomment-18502772

    More at the next episode.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>