RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Review Blogs PYNQ-Z2 Dev Kit - CIFAR-10 Webcam continued....
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: ralphjy
  • Date Created: 14 Aug 2019 5:03 AM Date Created
  • Views 2367 views
  • Likes 8 likes
  • Comments 7 comments
Related
Recommended
  • RoadTest
  • pynqworkshpch
  • pynq-z2
  • cifar10
  • machine learning

PYNQ-Z2 Dev Kit - CIFAR-10 Webcam continued....

ralphjy
ralphjy
14 Aug 2019

In the previous blog PYNQ-Z2 Dev Kit - CIFAR-10 Convolutional Neural Network , I verified the 3 hardware classifiers against the reference "deer" test image.  Now I'm going to see how the classifiers perform with captured webcam images.  I expect the performance will be degraded because the webcam will produce lower quality images due to issues like image brightness and focus.  CIFAR-10 has a small training set (5000 images per class), so I'm going to use a solid background to help keep the image simple.  Intuitively, I would expect that with higher quantization level the classification accuracy would improve.

 

I decided that since CIFAR-10 has transportation classes (automobile, truck, ship, airplane) that I would try to classify a few Matchbox vehicles that had escaped being recycled.

 

Here is my test setup.  I was a bit disappointed in the auto-focus and auto-exposure of the webcam, but I haven't figured out whether I can manually control this particular camera with OpenCV.

image

 

 

First try is the firetruck.  I expected this one to be easy, but only the W2A2 classifier got it right.

image

 

Second try is the convertible.  All the classifiers thought this was an airplane.  I'm assuming that the odd colors may have been confusing.

image

 

Third try is a car that I thought should be easy but interestingly the classifiers with higher quantization very clearly classified it as an airplane and the binary classifier thought it was a ship.

image

 

 

As a head check I grabbed one of the CIFAR-10 test images and it correctly classified with increasing accuracy as the quantization increased.

image

 

At this point I'm confused as to the primary cause of the poor classification of the webcam images.  Is it the image quality or the actual image.  I suspect it is both.

 

I noticed that the example notebook includes a sample webcam capture of an elk figurine which should classify as a "deer".

image

 

I would consider this a much harder image to classify because of the background.  It's interesting that in two of the classifiers that "airplane" and "deer" are closely ranked.  I'm getting the impression that CIFAR-10 trained networks are a good educational tool, but would not work well in the real world.  I'm going to move on to look at other neural network examples.

  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 7 years ago in reply to genebren +2
    Just wondering if the solid background and the loose framing isn't helping matters here ? Perhaps try adding some whitespace around the sports car training image and see if it too starts to fly...
  • ralphjy
    ralphjy over 7 years ago in reply to beacon_dave +2
    Okay, I did as you suggested and now it indeed does fly. Something tells me you've done this before . It does suggest that this network would not have worked as I would have tried to use it.
  • dubbie
    dubbie over 7 years ago +2
    It is one of the strange (?) things about using Artificial Neural Networks (ANN), particularly when using image systems or other data that is viewed by humans, is that they use all the data. When a human…
  • genebren
    genebren over 7 years ago

    Ralph,

     

    Interesting results.  The models really seem to be heavily weighted to call everything airplanes (even a plastic elk).  Image quality, likeness of image to learning images and many other minor details seem to influence the item classification.

     

    Great work on digging in and comparing these classifiers.

     

    Gene

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 7 years ago

    I agree with the comment about not being too good in the real world. Artificial Neural Networks can work well when the data set is limited or clearly distinguishable but once the data gets a bit iffy and vague they are not so good. They can be fun things to play with thou.

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<