RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs PYNQ-Z2 Dev Kit - Logictools
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: ralphjy
  • Date Created: 19 Jul 2019 10:48 PM Date Created
  • Views 1479 views
  • Likes 4 likes
  • Comments 2 comments
Related
Recommended
  • RoadTest
  • pynqworkshpch
  • pynq-z2

PYNQ-Z2 Dev Kit - Logictools

ralphjy
ralphjy
19 Jul 2019

I thought that I'd try out another of the basic overlays before moving on to a neural network application.

 

The PYNQ development software provides a set of logic tools using the logictools overlay.  You can create a digital circuit by specifying its function and IOs with a simple, declarative API in Python.

 

The logictools overlay has 3 function generators plus a trace analyzer to capture generated patterns.

  • Boolean Generator - up to 26 independent Boolean functions of up to 5 inputs each can be specified simultaneously
  • Pattern Generator - uses Wavedrom description language to specify arbitrary digital signals
  • FSM Generator - specify a finite state machine with up to 8 inputs, 19 outputs (not simultaneously).  e.g. FSM with up to 127 states, up to 6 inputs, and up to 14 outputs
  • Trace Analyzer - captures signals and displays waveforms using the Wavedrom application

 

image

 

I'll go through an example of creating a waveform with Wavedrom and generating the pattern on a set of pins on the Arduino Uno compatible IO connectors.

 

The Wavedrom application uses a straightforward JSON format to specify a waveform.  Syntax is explained here: https://wavedrom.com/tutorial.html

 

For pattern generation the 3 primary keys are 'name' (signal name), 'pin' (hardware pin designator), and 'wave' (pin state at each clock).

 

Here is the 3 bit counter pattern that I'll be demonstrating:

image

 

And the resulting pattern (the loopback waveform is not captured until the pattern and trace analyzer execute):

image

 

Short video showing the loopback operation and capture of the output waveform in the analyzer and an external scope:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

A picture of the physical setup:

image

 

 

 

Next for my roadtest I'm going to try some image processing  with neural networks.

  • Sign in to reply

Top Comments

  • DAB
    DAB over 7 years ago +1
    Nice post, I had not considered using the FPGA as a signal generator. DAB
  • genebren
    genebren over 7 years ago

    Nice post and demonstration of the tool set.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 7 years ago

    Nice post, I had not considered using the FPGA as a signal generator.

     

    DAB