RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Review Blogs Roadtest Review Blog Functionality tests S2Go Sensors
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: anuag_ashim
  • Date Created: 29 Sep 2018 11:11 PM Date Created
  • Views 1345 views
  • Likes 3 likes
  • Comments 2 comments
Related
Recommended
  • infineon
  • xmc11_boot_kit
  • s2go infineon
  • iot board
  • xmc1100 boot kit

Roadtest Review Blog Functionality tests S2Go Sensors

anuag_ashim
anuag_ashim
29 Sep 2018

This is part 2 from the blog MyIoT: Infineon Shield2Go Boards for IoT - Review

 

Here I will explain in detail about the tests I performed with the Infineon Shield2Go boards and the sensors. After setting up the Arduino IDE for the XMC_BOOTKIT and XMC2GO micro-controller and installing the libraries needed to work with the S2Go sensors I made a simple setup to test the S2Go sensors.

 

  • Blinking LED Test on XMC1100 Boot Kit
  • Blinking the LEDs on the XMC2Go board
  • Testing the S2GO DPS310-Pressure-Sensor with XMC1100 BootKit
  • Testing the TLV493D-A1B6-3DMagnetic S2Go with XMC1100
  • Testing the TLI4970-D050T4 Current Sensor with XMC1100
  • Wemos functionality Test

 

Blinking LED Test on XMC1100 Boot Kit

 

This was a simple test. The XMC1100 6 LEDs. I toggled the LEDs with different delays in between the toggling.

 

image

 

image

image

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Blinking the LEDs on the XMC2Go board

 

The mini XMC2Go board has only 2 user leds as seen in the last theory blog.

 

image

image

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Testing the S2GO DPS310-Pressure-Sensor with XMC1100 BootKit

It was a very straightforward test. After loading the zip files from GITHub in Arduino IDE the sample examples were easy to run. The DPS310 pressure sensor communicates to the XMC bootkit with I2C bus through SDA and SCL lines. I pulled the SDA and SCL lines with 10K resistors to the 3V3 power. As seen in my first blog the connections to the I2C lines are at pin 4 and pin 5 on the S2GO PRESSURE DPS310 Shield board.

 

image

 

My easy to go test setup

 

image

 

image

 

Testing the pressure sensor in Arduino IDE

 

The pressure is measured in pascal and not in millibar (as europeans are used to)

 

image

 

image

 

After disconnecting the sensor failure messages were also displayed as shown below

 

image

Testing the TLV493D-A1B6-3DMagnetic S2Go with XMC1100

 

The TLV493D-A1B6-3DMagnetic S2Go can measure in XYZ Cartesian format for linear motion detection and in Spherical format. The output of the of the sensor is also read by 2 wire I2C interface which can be upto 1 MBit/sec and 12 bit data resolution for each measurement direction (Bx, By and Bz linear field measurement up to +-130mT). The head of the S2Go board can be broken off and used in a another project easily.

 

image

 

image

TLV493D-A1B6-3DMagnetic S2Go interfaced to the XMC1100 bootKit

 

In this setup I measured by moving the 3D sensor by hand and recording the plot.

image

Cartesian Coordinates

 

image

Measuring Angular Motion of the 3D sensor

 

image

Used the fast plotting code for the spherical coordinates

 

Note: This sensor has temperature drift and should be compensated for. Detailed way to calibrate the sensor is mentioned on the Infineon website.

 

image

Resolution of the sensor at different temperatures

 

 

Testing the TLI4970-D050T4 Current Sensor with XMC1100

 

TLI4970-D050T4 is a coreless magnetic current sensor. It is a digital current sensor with full measurement range of +/- 50Amps. It can be used to measure AC and DC currents. The ambient operating temperature of max 85°C (limited) due to the power dissipation in the current rail. This sensor uses the 3-pin serial peripheral interface (SPI) and 16-bit SPI protocol to output the value.

 

image

The transfer function is used in the code to measure the current vs the output sent via SPI.

 

My test setup to run the sample code and get the sensor working

image

image

 

image

 

In this blog I did the tests to get all the S2Go infineon sensors tested for the functionality and running. I plan to integrate these sensors in a small project in the future. The  S2Go infineon sensor shields are easy to setup and working with Arduino. I also investigated the simulation aspects of the XMC1100 Bootkit board.

 

Wemos functionality Test

 

The wemos tests are done in the blog MyIoT: Infineon Shield2Go Boards for IoT with Wemos functionality

  • Sign in to reply
  • anuag_ashim
    anuag_ashim over 8 years ago in reply to thamizharasan

    Hi Desikan,

     

    Yes I still need to find some time to do the wemos tests. i have just run the test code for now. but application i still need to make final. hopefully i will do in the coming week.

     

    How is your road-test going?

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • thamizharasan
    thamizharasan over 8 years ago

    Hi Anurag,

     

    Nice detailed Roadtest review, but missing is the Wemos test results.

    There are so many use cases to test Wemos functionality, from which you can pick one.

     

    Thanks again.