Products
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
RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs TDK 24  LS10024
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: e14 Contributor
  • Date Created: 20 May 2010 1:22 PM Date Created
  • Views 908 views
  • Likes 0 likes
  • Comments 1 comment
Related
Recommended

TDK 24  LS10024

e14 Contributor
e14 Contributor
20 May 2010

I chose the LS100 24V 4.5A model to test, afterwards I intend to use it to power some stepper motor drivers.

 

First impressions are that the unit is of good quality and was made in Vietnam where I guess labour is

cheap. There are very similar items on eBay in fact they look identical but are not made by TDK, I think

I might get one to compare the quality.

 

I liked the easily removable hexagonally punched cover which slides off once the screw
is removed. There is a threaded hole for a second screw but this was missing.

 

I adjusted the VDJ pot to 24.01 V no load. (the pot is quite sensitive to get exact) I don’t have any

resistive loads to properly test the current but I did have two old 12V car headlamps that were wired

in series which drew a measured current of 4.33A. Initial surge current was just over 6 Amps from

cold, voltage drop was 0.03V

 

Testing the Over Voltage Protection (OVP) by adjusting the VDJ pot the unit shutdown it's
output at 27.9V which was just over the specified voltage range of 27.6 - 32.4V, minimum adjustment

was 19.29V, input mains disconnection is required for at least 2 minutes for the OVP to reset.

 

This model has a seven terminal block of the barrier type, three for mains input L-N-E,
and two sets of screws for the output, on higher current models 25A+ it is recommended to use
both sets of terminals to spread the load

 

The internal fuse is vertically soldered to the board, I would have preferred to see an easily
replaceable fuse, however being a compact unit with the other upper side comonents also
vertically mounted there is little space, there are surface mount components on the underside
of the pcb


On reassembly after taking a look at the quality of the soldering which was good, I noticed the
bracket and neoprene boot holding the Q2 power Mosfet against the chassis. I have never seen this
arrangement before. I assume this would not get that hot to cause concern as the unit is rated at
86% efficient. The boot insulates the TO-220-68TO-220-68 casing from the chassis but I would have preferred
to see the more usual through bolt with insulating washer.

 

With thanks to Alistair and Garden State

Attachments:
image
image
image
image
  • Sign in to reply
  • firatkocak
    firatkocak over 16 years ago

    Hi,

     

    A very good review. I have not received mine yet. After receving it, i am thinking of using it to power all the products placed in our shop window and see how it will be efficient to power all of them.

     

    Firat,