RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Review Blogs TI and Würth Elektronik LED RoadTest+ - Blue Print - 7/10
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: tonyboubady
  • Date Created: 8 Jan 2016 5:51 PM Date Created
  • Views 501 views
  • Likes 1 like
  • Comments 4 comments
Related
Recommended
  • RoadTest
  • ledroadtestplus
  • würth
  • we
  • elektronik
  • texas_instruments
  • ti

TI and Würth Elektronik LED RoadTest+ - Blue Print - 7/10

tonyboubady
tonyboubady
8 Jan 2016

NEW UPDATE:  Please check end of the blog post...

 

I am working hard to finish this project lately...Here is the update of my previous schematics and the final PCB design of the board.

 

image

 

Instead of 2N2222A BJT transistor I am using TIP122 now, the TIP122 can handle high current which is upto 5A and at the peak 8A, this is more enough for me to drive current for my LEDs. The resistors will be 10 ohm 1W or more than 1W. The yellow LED series has beed changed as it's forward voltage is 3V maximum, so 5 LEDs in series and each LEDs will get 2.4V.

 

The final version of PCB design, I am not going to use any fabrication house for my boards. I am going to etch it by myself (Just the money, nothing against PCB fab houses image)... So, it will be home brewing with limited resources like, 4 x 8 inch copper clad board and it's one sided etc... The board size will be 4x4 inch...

 

image

 

Eagle cadsoft helped me a lot with LED alignment using ULP, really nice PCB application to have. It's my hands-on with Eagle cadsoft... The circuit has 2 layers but the bottom layer going to be resistors and wires on backside of the copper clad board. I haven't used component footprints, because in this way it will be easy for etching.

 

image

 

The image below is the actual etching circuit area...

 

image

 

My original idea was to include ambient sensor in the same LED board but the sensor react to the LED light itself, so it is better to give a space foe sensor to work properly...

 

image

 

There is still loads of work to do... I feel that I am too late... but I will try my best to finish this.

 

UPDATE: I just realised that I have missed to connect the LEDs in series on PCB design, I will update it...


UPDATED DESIGN:


image

  • Sign in to reply

Top Comments

  • DAB
    DAB over 10 years ago +1
    Good update. Time management is one of the key issues with doing a successful project. There are always little things that do not go according to plan. DAB
  • tomaja
    tomaja over 10 years ago +1
    Hi, You have a nice looking board there How do you connect these diodes? I don't see from these PCB images how LED D2 is connected to the rest of your circuit for example...
  • tonyboubady
    tonyboubady over 10 years ago in reply to tomaja

    Thanks,

    There was a mistake, I left out to connect the LEDs in series, there will be traces in between the LEDs which is in series...I will update this design before etching...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tonyboubady
    tonyboubady over 10 years ago in reply to DAB

    Thanks, and yes that's the one thing I should practice on to keep timing...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tomaja
    tomaja over 10 years ago

    Hi,

    You have a nice looking board there image

    How do you connect these diodes? I don't see from these PCB images how LED D2 is connected to the rest of your circuit for example...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 10 years ago

    Good update.

     

    Time management is one of the key issues with doing a successful project.

    There are always little things that do not go according to plan.

     

    DAB