RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs TI and Würth Elektronik LED RoadTest+ - The Schema - 5/10
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: tonyboubady
  • Date Created: 30 Dec 2015 4:24 PM Date Created
  • Views 925 views
  • Likes 1 like
  • Comments 6 comments
Related
Recommended
  • RoadTest
  • ledroadtestplus
  • würth
  • we
  • elektronik
  • texas_instruments
  • ti

TI and Würth Elektronik LED RoadTest+ - The Schema - 5/10

tonyboubady
tonyboubady
30 Dec 2015

It took a while for me to post my blog... just had to face some issues and The Christmas celebrations. I have managed to do my schematics of my Smart Headlight circuit.

 

 

image

 

The 3.3 voltage, GND and ADC channel 8 goes through the ST1 screw terminal of the circuit, the GPIO pins P2.5, P8.2 and P8.3 goes through the ST2 screw terminal. The second part of the whole circuit schematics is shown below...

 

image

 

The ST1 screw terminal connected to LDR with 100K resistor, along with voltage divider point, the LDR will act as light sensor and send analog data to MSPFR4133 to the ADC channel 8, the MCU then process the data and send the output in GPIO pins P2.5, P8.2 and P8.3 which connected to ST2 screw terminal. The 3 outputs from MCU are connected to BJT NPN 2N2222A transistors to drive high voltage and control LEDs, as the MCU can able to send not more than 3.3V on GPIO pins. We need to supply secondary voltage which is able to drive high power LEDs, so we can close the 12V secondary voltage circuit by passing Base voltage to each transistor with GPIO outputs. On each Collector side of the transistors the LEDs are connected both in series and parallel, 4 LEDs in series with 1K resistor and the LED series connected in parallel.

 

Würth Elektronik's high bright LED can drive 3.2V average and 3.6V maximum forward voltage in the typical current rate of 350mA, we can pass maximum limit of 1A current. So in my circuit there is 4 LEDs in series which is 12/4 = 3V for each LED, each series will get 12V of power, so I will get real bright output from WE LEDs... 32 LEDs connected for white light, 24 LEDs connected for yellow light and 20 LEDs for blue light.

 

I am working on my PCB design for my circuit, I am going to etch it myself and I will post the process...

 

Würth Elektronik's components are really helping me a lot in my situation, they have sent all the parts I have asked in prompt manner, even they put me in guilty position by asking me "What else you need" I am speechless...This is my personal message to Würth Elektronik - You guys are GREAT and ROCKS image

  • Sign in to reply

Top Comments

  • DAB
    DAB over 10 years ago +1
    Nice start. DAB
  • jc2048
    jc2048 over 10 years ago +1
    Don't do the pcb yet, this isn't going to work. The LEDs won't light up (and the transistors couldn't switch them properly if they did). You need to read up on Ohm's law and look carefully at how diodes…
  • gpolder
    gpolder over 10 years ago in reply to tonyboubady +1
    Hi Antony, why not use the TPS9251 LED driver provided with this roadtest? It will keep the current trough the LEDs constant and you don't have any issues with wasted power heating up resistors. It also…
  • DAB
    DAB over 10 years ago

    Nice start.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<