RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs TMC2300-IOT-REF - Remote controlled Stepper Motor - A closer look
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: Workshopshed
  • Date Created: 10 Feb 2021 8:43 PM Date Created
  • Views 1587 views
  • Likes 3 likes
  • Comments 6 comments
Related
Recommended

TMC2300-IOT-REF - Remote controlled Stepper Motor - A closer look

Workshopshed
Workshopshed
10 Feb 2021

Following my problem trying to get the motor to run, I thought I'd check the board with a microscope to see if there were any issues. It all looks good an there are no obvious shorts, melted components or burns.

 

Power

image

USB

image

TMC2300

image

 

ESP32

 

image

  • Sign in to reply

Top Comments

  • Gough Lui
    Gough Lui over 5 years ago in reply to Jan Cumps +3
    I would too personally, or a mishap damaging a component, but the reason I bought it up was because that resistor is R23 which pulls down the EN line on the TMC2300x which trinamic_lisa suggested was worth…
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to Gough Lui +3
    Gough Lui wrote: I.. Nice to see KiCad getting some love . True <3
  • Jan Cumps
    Jan Cumps over 5 years ago +2
    Andy, I read that your power circuit gets hot, no matter what's connected as source or load. If it gets hot even when there's no motor attached, that's a real sign that things are wrong. These are all…
  • Jan Cumps
    Jan Cumps over 5 years ago

    Andy, I read that your power circuit gets hot, no matter what's connected as source or load.

    If it gets hot even when there's no motor attached, that's a real sign that things are wrong.

    These are all low power components without "prior state" memory. No component on the board can cause overheating without the motor.

    Troubleshooting should focus on finding what components are defect.

     

    The only easy test is to remove D6 and D8. If the board still gets hot, you know it's on the easy part.

    But if not, you'll have to troubleshoot the ICs downstream the diodes.

     

    The bad part is that it's most likely downstream, and those are more difficult components to troubleshoot.

    The good part is that you have the UART kit, and the downstream components can be stolen from that ...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<