RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs TMC2300-IOT-REF - Remote controlled Stepper Motor - Getting your motor running
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: Workshopshed
  • Date Created: 7 Feb 2021 8:31 AM Date Created
  • Views 6344 views
  • Likes 11 likes
  • Comments 35 comments
Related
Recommended

TMC2300-IOT-REF - Remote controlled Stepper Motor - Getting your motor running

Workshopshed
Workshopshed
7 Feb 2021

As mentioned in the last post TMC2300-IOT-REF - Remote controlled Stepper Motor - Getting to blink there was an issue with the connector on the motor. I found a grove connector was about the right size if I trimmed it slightly so I soldered that on.

 

Get your motor running

The next thing to try is to have the motor running. For this there are a few steps needed. Firstly to provide some power then to send the right serial commands to the controller chip and the finally to enable motor output.

 

The supply to the motor is connected to +VBAT, this in turn is connected to the charger circuit. The AN058 tech note suggests you can use a power supply to power the motor.

 

image

Serial communication is covered in section 4 of the tmc3200 data sheet and Jan Cumps also did a detailed look at the serial comms for a previous road test, Trinamic Stepper Motor Controller TMC2300 - UART Interface  Jan also references a library which looks like it could be useful https://github.com/trinamic/TMC-API

 

The key part of the serial communications is that the commands to send to the motor are wrapped in a special data structure for error checking and addressing. The address is configured via AD0 and AD1 pins, in this reference design these are both tied to ground so it would be address zero. The algorithm for the CRC is also included in the notes but the is a practical example for the code in the blynk example. https://github.com/trinamic/TMC2300-IOT-REF/blob/master/Blynk/Stepper_Mode

image

The enable pin can also be found in the schematic on pin 32 and this is confirmed by the code example.

 

I copied in the TMC_2300.ino, CRC.ino and include files from the Blynk example. I was initially puzzled why the libraries were named with the INO suffix, but that allows the Arduino IDE to compile the files with the right headers so TMC_2300.ino can find Serial1 without needing to reference the Arduino header files. You just need to ensure you open the right ino to for your project. In my case "MotorRun.ino"

image

Checking the Blynk document we can see that the speed value is between 500 and 9000, and the current is between 9 and 31. So I plugged those values straight into the code.

#include "include/Functions.h"
#include "include/TMC2300.h"
#include "include/CRC.h"


#define LED_STATUS 18
#define MOTOR_EN 32


void setup() {
  pinMode(LED_STATUS, OUTPUT);
  pinMode(MOTOR_EN, OUTPUT);


// Debug console
  Serial.begin(115200);


// TMC2300 IC UART connection
  Serial1.begin(115200);


// Initialize CRC calculation for TMC2300 UART datagrams
  tmc_fillCRC8Table(0x07, true, 0);


// Set the speed to 7000
  tmc2300_writeInt(TMC2300_VACTUAL, 7000);


// Set the current limit to 31 (default)
  uint32_t value = 1 << TMC2300_IHOLDDELAY_SHIFT | ((31 << TMC2300_IRUN_SHIFT) & TMC2300_IRUN_MASK) | 8 << TMC2300_IHOLD_SHIFT;
                 
  tmc2300_writeInt(TMC2300_IHOLD_IRUN, value);


// Enable the motor
  digitalWrite(MOTOR_EN, HIGH);   


  Serial.print("Initialisation Complete");
}


void loop() {
    // Toggle the status LED while the motor is active
    digitalWrite(18, HIGH);
    delay(250);
    digitalWrite(18, LOW);
    delay(250);
    digitalWrite(18, HIGH);
    delay(250);
    digitalWrite(18, LOW);


  // Re-write the CHOPCONF register periodically
  tmc2300_writeInt(TMC2300_CHOPCONF, 0x14008001); 
}

 

The LED is still flashing nicely but no response from the motor. Possible causes include the motor wiring, power supply, Trinamic's code, my code.

 

I cross checked the wiring and confirmed that there was one coil of the motor connected to pins 1 and 2 and the other to pins 3 and 4. However, looking at the datasheet in more detail vs the pinouts on the board, I spotted that the A coil was reversed, I'd still expect some kind of motion from the motor with that configuration but I swapped the connectors just to check. And still no motor movement.

imageimage

To check if power was an issue, I plugged in the board directly to a charger. Again, flashing lights but no motion. Looking at the schematic the diag pin is connected to a white led and would illuminate when there was a driver error or stall. This was not the case.

 

So my next thought was to use the serial interface to query the state of the chip and see if I could diagnose what was going on.

 

Serial Reading

Looking at the datasheet there were 3 registers that seemed of interest. GSTAT, GCONF and IOIN. So I updated the code to read these using the read int function and a simple display function

 

void printByte(uint8_t var) {
  for (uint8_t test = 0x80; test; test >>= 1) {
    Serial.write(var  & test ? '1' : '0');
  }
  Serial.println();
}


void loop() {
    delay(1000);
  
    result = tmc2300_readInt(TMC2300_GCONF);
    Serial.print("GCONF:");
    printByte(result);    


    result = tmc2300_readInt(TMC2300_GSTAT);
    Serial.print("GSTAT:");
    printByte(result);  


    result = tmc2300_readInt(TMC2300_IOIN);
    Serial.print("IOIN:");
    printByte(result);  
}

 

These all returned zero which made me suspect that it wasn't communicating with the TMC2300 correctly, but I double checked by adding IHOLD_IRUN and CHOPCONF which also came back as zero.

Next up I set the speed for the serial communication lower to 57600, that also made no difference.

One thing I didn't try was to see if there was an issue with the CRC. Looking at the code in TMC2300.INO there is a line that returns zero if the CRC does not tally. So that might be something to try.

 

Back to basics

Scouring the data sheet for the reference board, I spotted that the step and direction pins were connected to the ESP32. So I tried a simple sketch that pulsed the step pin and the motor did turn. However the motor got quite warm, quite quickly so I reflashed to a simple blink sketch.

So this does demonstrate that at least the motor is wired up correctly.

CAUTION: Do not simply pulse the step pin, that can overload the board.

At this point I decided to take a break as the board had got quite warm too.

 

Damaged?!

After leaving it an hour, I decided to try it again. If I power it up either from the battery or from USB the LED blinks so the ESP32 is obviously getting power. But the board is no longer detected as a serial port by the computer. The area ringed below gets very hot. One of the other roadtesters mentioned an under voltage condition which got me thinking that I may have just discharged the battery. So I checked that and the battery voltage seems a little high, am getting 3.9v on the connector on the edge of the board. The overheating happens regardless of if the battery is attachd or the USB or both. Also the the board is not recognise by the PC.

 

It is possible that this is caused by software e.g. the TMC2300 is still trying to draw a massive current on startup. Or it could be that the previous experiments damaged the battery charge/power regulation stage?

image

Backup Plan

I've devised a backup plan. It might not look so similar but the combination of an off the shelf ESP32 module and the TMC2300 from a previous test should allow me to prove out the communication between the ESP32 and TMC2300. And the results from this should be reproduceable on the IOT reference design.

image

  • Sign in to reply

Top Comments

  • Gough Lui
    Gough Lui over 5 years ago +4
    Unfortunately, I don't have one of these boards, but if there is some schematic, that would usually be quite helpful. I haven't got the time to go and dig up documentation at this moment, but some basic…
  • Workshopshed
    Workshopshed over 5 years ago +4
    Gough Lui , trinamic_lisa thanks for to help. The 3.3v line is reading 3.3v when powered from battery. I think I have a USB isolator which should allow me to measure the current draw from the port. Gough…
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to Gough Lui +4
    In lieu of a thermal camera, there is always the nose and finger. You can often smell what got hot after the facts (carbon or silicon burn smell). Or put some spit on your pinky and touch each component…
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to Gough Lui

    In lieu of a thermal camera, there is always the nose and finger.

     

    You can often smell what got hot after the facts (carbon or silicon burn smell).

    Or put some spit on your pinky and touch each component for a few seconds. If you hear a scream, that's the one.

     

    If you do not like pain, pour a layer of cleaning alcohol over it. The part that dries first is the hot one.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 5 years ago in reply to Jan Cumps

    I missed seeing that STEPPER and VIO/nSTANDBY are connected and knowing the nSTANDBY line is connected with an internal pulldown will indeed mean 3.3V or nothing ... so perhaps this means that it is pulling down STEPPER to zero to save quiescent draw when the TMC2300 is shut down hence moving the state into a "do not use" may not be a problem at all. Phew. I thought I was going mad for a second .... haha ... thanks Workshopshed & Jan Cumps.

     

    Getting hot regardless of USB or battery ... hmm. I'd expect some warmth on USB as a linear charger IC will dissipate the difference in voltage as heat, but getting hot on battery (supposedly) not doing anything ... well, perhaps if you can find someone with a thermal imaging camera or even by sweeping an IR laser thermometer, I suppose you can more definitively narrow down which chip. The area you circled is home to the battery charger IC and the linear 3.3V regulator. While 3.3V measured good, if it is still getting hot and no action on the USB, then perhaps the CH340 is not happy but that may not be the only thing unhappy on that board (could be almost anything ... connected to 3.3V).

     

    All the best for your board, but at this point, it seems a bit of a mystery why it ended up behaving like this. Perhaps infant mortality or ESD gremlins are to blame?

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to Gough Lui

    Gough Lui  wrote:

     

    ...

     

    EDIT - actually, the MOSFET is a little ambiguous - it seems the source potential is whatever the STEPPER input is ... so the MOSFET may not actually switch to zero but open the circuit ... it's a but curious.

     

    - Gough

    Excuse me for skipping the core part of your reply. I removed it because I have no questions or remarks.

     

    The MOSFET, I think, only switches the digital source. Either 3V3, or something lower than that. VCio on a TMC2300 is the source for the digital output circuit.

    So there is no magical voltage at the FET's source. It can only be the 3V3 or (almost) nothing.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 5 years ago in reply to Gough Lui

    Thanks Gough, it's getting hot regardless of if it is powered from USB or from battery. I think you are right that the mosfet opens the circuit, the standby pin has an internal pulldown.

    image

    I'll look at making some current measurements. No obvious issues from the microscope pics but I've posted those as a separate blog.

    TMC2300-IOT-REF - Remote controlled Stepper Motor - A closer look

     

    Checking the CAD vs the photo, we can see that the missing resistor is R4 as you suspected.

    imageimage

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 5 years ago in reply to Workshopshed

    Thanks for that Workshopshed - I've been very busy myself so haven't had much of time to "breathe", but since I'm off work now, I'll take some time to delve into it a bit.

     

    From what I can see, the USB power input is being sent to both the TI TP4054 charger IC and the AP2112K linear regulator. If the 3.3V line is reading 3.3V when plugged into battery (and isn't getting warm), that's a good sign indicating that at least the AP2112K linear regulator is happy and hopefully everything connected to it isn't overloading the rail. You could check the current draw from the battery with a DMM if it is getting warm to get an idea how big the drain is, and see if it is different with a motor attached and without a motor attached (assuming that is allowed).

     

    What happens when you power from USB? Does the 3.3V line fall below 3.3V? Do things get hot? Does the USB voltage fall to below expected levels (i.e. <4.75V)? You could try measuring the USB Vbus from the anode side of D6 as it's probably easier than trying to probe the back of a USB 3.0 connector where the pins are absolutely tiny.

     

    The main difference between powering from battery and USB is that power is on the input side of the TP4054 and if it has failed in some way, then it could be consuming enough current to collapse the USB input due to overcurrent protection. The TMC2300x is powered directly from battery from my glance of the schematics, while the ESP32 relies on 3.3V, so my guess is that they shouldn't be culprits - but as suggested by trinamic_lisa, while you have the microscope out you might want to examine the EN line which should have R23 pulldown resistor - perhaps if that is knocked off then the line could be floating/undefined.

     

    From my understanding, R4 and R5 should be a one-or-the-other jumper as you've surmised. I suspect it is pre-populated in the R5 position so that STEPPER is receiving Vcc_IO which is being driven out of the ESP32 page of the schematic. IO5 is driving an N-ch MOSFET which allows the input to be toggled between 3.3V (when IO5 is outputting a logic high) and zero (when IO5 is outputting a logic low). It seems from the datasheet, STEPPER and MODE form two bits to select mode. MODE line is tied to GND by the design, so only a combination of 00 or 10 mode selection can be made - between a "do not use" and "UART stepper". Why it is configured so you could select a "do not use" mode is probably something which is intended for factory debug or testing ... but it is curious. My suspicion is that you should set IO5 to be high when you want to use the UART stepper mode, but don't hold me to this - I haven't got one of these boards myself and no firsthand experience with it, so I'm only going off what I can get from the literature.

     

    But before we rule anything out, have you checked for a stray solder blob or wire scrap? I've had that be the cause of mysterious malfunctions before ... just thought I'd throw it out there before we get too deep into troubleshooting ...

     

    EDIT - actually, the MOSFET is a little ambiguous - it seems the source potential is whatever the STEPPER input is ... so the MOSFET may not actually switch to zero but open the circuit ... it's a but curious.

     

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>