RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs VectorBlox SDK setup
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: dimiterk
  • Date Created: 19 Dec 2023 3:32 PM Date Created
  • Views 3472 views
  • Likes 6 likes
  • Comments 3 comments
Related
Recommended
  • VectorBlox

VectorBlox SDK setup

dimiterk
dimiterk
19 Dec 2023

VectorBlox SDK Setup

in this part we'll install the VectorBlox SDK and test the example networks on board. The VectorBlox AI accelerator makes use of an SDK that leverages the openVino framework to convert AI networks from floating point format designed in multiple frameworks such as Keras , Tensorflow1 or TF2 , Pytorch, ONNX into a quantized version that can run on the FPGA fabric accelerator.  As of 13/10/2023 Vectorblox SDK only supports Ubuntu 16/18/20.04. WSL can also be used for AI network development.

For this project WSL2 and Ubuntu 20.04 WSL image from the Windows store were used. Some additional SW packages have to be installed as shown below.
Using the VectorBlox IP on the Polarfire Video SOC is a multi-step process.

First an FPGA design has to be programmed into the Polarfire SOC fabric. Next a compatible Yocto image needs to be programmed on the on-board eMMC or sd card. Next the SDK has to be loaded on board the Yocto image and a new project folder has to be uploaded using the framework of choice. Then the AI network has to be compiled and converted into a .vnnx file on the host.  Finally, if all the AI network ops (instructions) are compatible and the conversion of the floating point network is successful the last steps are integration with the video pipeline by adding the per-processing and post processing steps. Before all that the SDK has to be installed on a host PCB for development.

1. VectoBlox FPGA design

As of Oct 18 2023  Libero 2023.1 with a valid VectorBlox license must be used to compile the reference design. Complication takes 40 minutes on a Ryzen-7. Libero compilation for Polarfire is single threaded.

image

Clone the repo : git clone https://github.com/Microchip-Vectorblox/VectorBlox-SoC-Video-Kit-Demo

Then launch Libero and source the .tcl file. This will create the VectorBlox Accelerator Libero project from the MPFS_VIDEO_KIT_VECTORBLOX_DESIGN.tcl file.

image

Note that compiling this design requires Libero 2023.1. Once the project is compiled and programmed on board, the next step is to install the SDK on board the Polarfire Video SOC

The board was already pre-programmed with the latest Yocto image as shown in the previous article.

image

The board is connected to one of the Ethernet jacks so since it is configured in DHCP mode it will automatically lease an IP. Once the FPGA design is programmed, next step is to connect and Ethernet cable to any of the two Gigabit network ports.

image

Now we can move on to download the SDK on board.

2. Install VectorBlox SDK on Polarfire Video SOC

.At this point we can download and unzip the sample networks from https://vector-blox-model-zoo.s3.us-west-2.amazonaws.com/Releases/ModelZoo/samples_V1000_1.4.4.zip to the root directory.

    wget --no-check-certificate https://vector-blox-model-zoo.s3.us-west-2.amazonaws.com/Releases/ModelZoo/samples_V1000_1.4.4.zip
    
    unzip samples_V1000_1.4.4.zip

    

image

Download and unzip the VectorBlox SDK from https://github.com/Microchip-Vectorblox/VectorBlox-SDK/archive/refs/tags/release-v1.4.4.1.zip and navigate to this example

image

wget --no-check-certificate https://github.com/Microchip-Vectorblox/VectorBlox-SDK/archive/refs/tags/release-v1.4.4.1.zip

unzip release-v1.4.4.1.zip
cd release-v1.4.4.1.zip/example/soc-video-c


image
Two HDMI cables were connected to the PolarFire SoC Video Kit (Rx/Tx). The RX cable was plugged into a laptop which is used as the video source.

To test that the HDMI is working correctly , the user can run

make hdmi

to toggle the frame buffers (for ~1 sec) to verify their HDMI setup.

The demo does not support the camera as a video feed so only the framebuffer data from the HDMI RX is used.


3. Install VectorBlox SDK on Host

To develop and port AI networks like Imagenet, Mibolinet or similar the SDK must be installed on a host PC.

Install GIT LFS

curl -s https://packagecloud.io/install/repositories/github/git-lfs/script.deb.sh | sudo bash
sudo apt update && sudo apt install git-lfs
git lfs install

If having an issue with clock synchronization update as below: sudo hwclock --hctosys

Installing the VectorBlox SDK requires some additonal steps which are not clearly laid out on the github repo.

git clone https://github.com/Microchip-Vectorblox/VectorBlox-SDK
cd VectorBlox-SDK/
chmod +x install_dependencies.sh
chmod +x install_venv.sh
chmod +x setup_vars.sh

Install dependencies first.

./install_dependencies.sh


Next setup variables. This will download a number of frameworks and take a couple of minutes.

./install_venv.sh


The script setup_vars.sh will create a virtual environment so it can be run only once. Any other time simple activate the environment as below.

Next start the virtual env and export SDK location

cd vbx_env
source bin/activate
export VBX_SDK=/home/user/VectorBlox-SDK

At this point, one can compile the examples , copy them on the Polarfire Video SOC board and run them.

The top level SDK folder contains the following folders:

/example -

/tutorials

/drivers

/fw

/app_notes

The /fw folder contains the binaries that are used to program the SPI flash.

The /tutorials folder contains example networks for Pytorch , Keras, TF1/TF2, Darknet and onnx.

The /example folder contains 4 sub-folders:

/python

/sim-c

/soc-c

/soc-video-c

The python and sim-c folder contains scripts to simulate the developed networks.

The /soc-c is used to run networks on images.

The /soc-video-c uses additional pre and post processing steps for individual networks.

The framework does not have any python support to run network on board so all code at the moment needs to be developed in C.

4. AI Network on Polarfire Video SOC

Test the installation by switching under onnx directory and compiling MNIST

cd ../tutorials/onnx
chmod +x mnist.sh
./mnist.sh


This will copy pass the number 7 image from the folder and print the expected results.

image

Testing Mobilenets

Next download and unzip the sample networks to the `/home/root` directory

wget https://as2.ftcdn.net/v2/jpg/00/97/58/97/1000_F_97589769_t45CqXyzjz0KXwoBZT9PRaWGHRk5hQqQ.jpg

mv 1000_F_97589769_t45CqXyzjz0KXwoBZT9PRaWGHRk5hQqQ.jpg cat.jpg
 
./run-model ../../fw/firmware.bin ~/samples_V1000_1.4.4/mobilenet-v2.vnnx cat.jpg CLASSIFY

5. VectorBlox-SoC-Video-Kit-Demo

The VectorBlox SDK comes loaded with a demo composed of multiple AI networks. To start the app follow the instructions on the repo by issuing 

make overlay

make to

./run-video-model

   

The networks can be replaced on the fly by pressing enter.

{gallery}Face recognition

image

image

image

image

image

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

So now we have completed the setup of the Polarfire SOC Video Kit by updating the Yocto image and programming the FPGA fabric with the Vectorblox AI accelerator, installed the Vectorblox SDK on the FPGA SOC and Host computer, tested the demo networks and verified network connectivity and HDMI pipeline. Last step will be to implement a custom network on the VectorBlox SDK. Before we delve into that we'll take a look at the FPGA design examples that comes with the kit.

References

[1] https://docs.openvino.ai/2021.4/openvino_docs_MO_DG_prepare_model_convert_model_Converting_Model.html

[2] https://github.com/Microchip-Vectorblox/VectorBlox-SoC-Video-Kit-Demo

[3] https://github.com/Microchip-Vectorblox/VectorBlox-SDK/tree/master/example/soc-video-c

  • Sign in to reply
  • rscasny
    rscasny over 2 years ago

    A great blog on Vector Blox! Thanks for writing it.

    Randall

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dimiterk
    dimiterk over 2 years ago in reply to DAB

    Will build a custom network and try to port YOLOV8 and stereo network next. The above post was flagged as spam due to the videos probably so rscasny  had to step in. I received around ~8 emails from the system yesterday.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 2 years ago

    Nice update.

    You are moving right along with some interesting capability.