RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum which SOIC-8 clip ?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 2752 subscribers
  • Views 4287 views
  • Users 0 members are here
Related

which SOIC-8 clip ?

ttt7
ttt7 over 6 years ago

I'd like to buy a SOIC-8 clip

https://si.farnell.com/c/test-measurement/test-connectors-ic-clips/ic-test-clips?no-of-contacts=8contacts

 

Is there a notable difference between 3M 923650-08 and 3M 923655-08  ?

Are 3M 923650-08923650-08 sold nowadays still the ones sold in 2010, some of the customers described problems using them

https://www.element14.com/community/message/12898/l/test-clips-which-dont-fit-soic-8#12898

 

I'm excluding 923739-08, since it's only stocked in the USA.

image

923739-08923739-08 vs 923650-08923650-08, do higher numbers mean a newer model ?

 

Thank you

  • Sign in to reply
  • Cancel
  • dougw
    dougw over 6 years ago

    I have used the 3M 2409346 and the Pomona.

    The 3M worked a bit better, but the Pomona could get into tighter spaces.

    Both do the job.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 6 years ago

    Edward,

     

    I have a couple of the Pomona 5250 that I bought used off of Ebay (along with several other SOIC and DIP clips).  I don't know if some clipped off some of the plastic tabs that go between the spring loaded contacts that connect to the SOIC part or if they broke off, but I think that the clips would work much better (alignment) with them in place. Even with the missing tabs, they work very well and make great contact to the chips.

     

    If space is not an issue, but you can use higher pin count clips (like 14 and 16) to connect to an SOIC-8, so if you think you might need to clip on to larger parts in the future, you might get a larger clip now.

     

    Good luck,

    Gene

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to ttt7

    I didn't know these were still sold : )

    If it is for one-off, personally I use individual probes (the kind that have a spring plunger since I rarely need to connect to so many pins simultaneously). If it is for production, maybe a test jig is better (using the pogo type probes) onto test points.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • ttt7
    ttt7 over 6 years ago

    ( I can't edit nor delete my post above ? I didn't want to submit it yet, maybe some keyboard shortcut did so )

     

    I'd buy either 3M 923650-08923650-08 or Pomona 5250, but it seems one can find critiques of both.

    Any experience with these ?