RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum which SOIC-8 clip ?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 2752 subscribers
  • Views 4288 views
  • Users 0 members are here
Related

which SOIC-8 clip ?

ttt7
ttt7 over 6 years ago

I'd like to buy a SOIC-8 clip

https://si.farnell.com/c/test-measurement/test-connectors-ic-clips/ic-test-clips?no-of-contacts=8contacts

 

Is there a notable difference between 3M 923650-08 and 3M 923655-08  ?

Are 3M 923650-08923650-08 sold nowadays still the ones sold in 2010, some of the customers described problems using them

https://www.element14.com/community/message/12898/l/test-clips-which-dont-fit-soic-8#12898

 

I'm excluding 923739-08, since it's only stocked in the USA.

image

923739-08923739-08 vs 923650-08923650-08, do higher numbers mean a newer model ?

 

Thank you

  • Sign in to reply
  • Cancel
Parents
  • ttt7
    ttt7 over 6 years ago

    ( I can't edit nor delete my post above ? I didn't want to submit it yet, maybe some keyboard shortcut did so )

     

    I'd buy either 3M 923650-08923650-08 or Pomona 5250, but it seems one can find critiques of both.

    Any experience with these ?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to ttt7

    I didn't know these were still sold : )

    If it is for one-off, personally I use individual probes (the kind that have a spring plunger since I rarely need to connect to so many pins simultaneously). If it is for production, maybe a test jig is better (using the pogo type probes) onto test points.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 6 years ago in reply to ttt7

    I didn't know these were still sold : )

    If it is for one-off, personally I use individual probes (the kind that have a spring plunger since I rarely need to connect to so many pins simultaneously). If it is for production, maybe a test jig is better (using the pogo type probes) onto test points.

    • Cancel
    • Vote Up +3 Vote Down