RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum Freescale RD3803MMA7660FC review issues
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 2746 subscribers
  • Views 2360 views
  • Users 0 members are here
  • freescaleroadtest
  • accelerometer
Related

Freescale RD3803MMA7660FC review issues

gandrewstone
gandrewstone over 16 years ago

Hi 7660 reviewers,

 

I've been holding off on my review because I haven't had time to put the device in my own circuit.  Lack of code really is the issue isn't it?  I mean, frankly all that software they gave us and the USB->serial->i2c board is just a cute toy.  Or more realistically they probably made all that for marketing reasons and figured that it could be pawned off as a dev kit.


It would be pretty easy for them to give us a nice API that calls into an unimplemented I2C "underface".  What I mean is that they wouldn't provide the I2c implementation; all the uPs have those anyway... they just provide calls into a "prototypical" I2c library (read, write, etc) and you would translate their calls into your uP's I2C library.


I've been holding off on my formal review on my blog until I can get some code written.  But its interesting I kind of feel like they are getting free labor here... I mean its worth more then $35 bucks of my time to write that code.  But it bugs me that Freescale has clearly already written that code, but for some reason only released an incomplete header file (for example, it does not mention that the I2c address is 0x4c).  Ultimately Freescale is really losing out; the quality of our reviews would be much better and would come out much sooner if they had provided that code.

 

Here are my initial observations for you other reviewers, summarized.

 

0. No code: see rant above :-)


1. There seems to be no way to program the uP on the USB->Serial board.  So I can't change the code to try out my application.


2. The USB protocol is documented, so I could write my program to run on the laptop and use that protocol.  But that would be a lot of throwaway code, and not really test issues like whether my uP can handle the data stream.


3. Putting the chip on its own .1" daughterboard is great!  I can prototype with it.


4. You can buy that little daughter board separately for $35, vs $130 for the whole kit.  Since that's really the only valuable part for real engineering eval, that's what I would buy.


5. I have a handy 5v uP, other uPs have 1.8v.  Wouldn't it have been a lot more useful if their helper board did logic level conversion instead of USB to serial?


In sum, seems like a nice little chip, with a poorly conceived "development" toolkit.  I guess the magic of open source will eventually fix that, esp. if I get some time this weekend! :-)


If you have managed to upload code to the uP or solve any of these other issues, send me a message!

 

Cheers!

Andrew

  • Sign in to reply
  • Cancel
Parents
  • bbolo1
    bbolo1 over 16 years ago

    Now the details

     

    Here's the link where you can find all the necessary resources for building the JB16 BDM debugger (like in my case) http://forums.freescale.com/t5/OSBDM-JM60-Open-Source-BDM-for/USBDM-Version-2-JB16-Version/td-p/49363

     

    Thanks to pgo, the Freescale forum user who spent so much of its time having this neat thing working and being open source).

     

    As a personal advice please check the Freescale website for available samples. JB16 is still in sampling program so you can have a few chips of this kind. I personally got more than one and used some other in a small USB I/O expander project of my own. Quite a handy tool.


    I want to try to build the OSBDM version of the debugger since this kind of debugger supports some other families of Freescale uCs (HCS08, RS08, Coldfire V1 - V4, and the 56F series of DSCs). I think the idea of having a unified debugger is great!

    The OSBDM is based on the MC9S08JM60 uC, which is in sampling program as well. So, if you want a simple version of the debugger, go with the JB16 version. On the other hand the OSBDM is more versatile but the final decision on which one to start is yours.

    Being open-source, you have access to the firmware source code as well as the host DLLs. And there's support for Linux as well.

     

    Keep in touch

     

    Bogdan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bbolo1
    bbolo1 over 16 years ago

    Now the details

     

    Here's the link where you can find all the necessary resources for building the JB16 BDM debugger (like in my case) http://forums.freescale.com/t5/OSBDM-JM60-Open-Source-BDM-for/USBDM-Version-2-JB16-Version/td-p/49363

     

    Thanks to pgo, the Freescale forum user who spent so much of its time having this neat thing working and being open source).

     

    As a personal advice please check the Freescale website for available samples. JB16 is still in sampling program so you can have a few chips of this kind. I personally got more than one and used some other in a small USB I/O expander project of my own. Quite a handy tool.


    I want to try to build the OSBDM version of the debugger since this kind of debugger supports some other families of Freescale uCs (HCS08, RS08, Coldfire V1 - V4, and the 56F series of DSCs). I think the idea of having a unified debugger is great!

    The OSBDM is based on the MC9S08JM60 uC, which is in sampling program as well. So, if you want a simple version of the debugger, go with the JB16 version. On the other hand the OSBDM is more versatile but the final decision on which one to start is yours.

    Being open-source, you have access to the firmware source code as well as the host DLLs. And there's support for Linux as well.

     

    Keep in touch

     

    Bogdan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to bbolo1

    Hello,

     

    just wanted to point out that the OSBDM in its present form is "unified" only in hardware, but the firmware has to be reprogrammed every time you want to work on a different type of target.

     

    The USBDM by pgo has a single firmware that works for HCS08, HCS12, Coldfire V1 (CF1), but the OSBDM has to be reprogrammed with different firmware for each of these target families. And naturally you need some other BDM pod to do the reprogramming ...

     

    best regards,

    Robert