RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Help us select RoadTest kits
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 73 replies
  • Subscribers 2766 subscribers
  • Views 6726 views
  • Users 0 members are here
  • RoadTest
  • international
  • rectifier
  • freescale
  • matrix
  • avago
  • development
  • ir
  • maxim
  • national
  • hawkboard
  • kits
Related

Help us select RoadTest kits

awinning
awinning over 16 years ago
Hi,

We'd like to hear your thoughts on dev kits in the market just now. What  kits interest you, or would you maybe like to see on future RoadTests?  Are there any other type of products you'd like to see on RoadTest?  (before anyone suggests, there's no chance of an iPad appearing in the  near term future image )

To get the conversation started we've pasted 9 possible kits below. Tell  us which of these interest you the most and why? As a disclaimer, I'm  not promising to give away the most popular, but we'll certainly talk to  the manufacturers and your views will help us greatly!


1. National Semiconductor’s LM26420 evaluation board demonstrates the  company's LM26420 based solution.

2. International Rectifier's IRS2540 IRS2540/1 buck converter based  development board helps develop HB-LED applications

3. ST's STM3210E-SK/HT helps start development for the company's ARM  core-based microcontrollers.

4. Maxim's MAX9830A evaluation kit uses a filterless class D amplifier to  drive a mono bridge-tied-load speaker.

5. Matrix Multimedia's EB018 E-blocks CAN bus board allows investigation  of the CAN bus protocol.

6. Avago's HFBR-0410HFBR-0410 fiber optics evaluation kit allows first hand  experience with simple DC to 5MBd TTL compatible components.

7. Freescale's RD1986MMA2260DRD1986MMA2260D TRIAX 3-axis acceleration sensing demo  board combines demos available for accelerometer applications.

8. Microchip’s DM183026 mTouch capacitive evaluation kit helps develop  touch sense applications using PIC16F or PIC24F MCUs.

9. Innovate Software Solutions Hawkboard is an open community board with a  feature set based on the TI OMAP L138 processor.
  • Sign in to reply
  • Cancel
  • Zad
    Zad over 16 years ago

    An interesting selection there! Predictably, I would go with the herd. The smaller products (Class D amp for example) I can hack together quickly and cheaply anyway, the more complex / delicate systems are way too much hassle to mock up a 1-off just to see if it will work, so I nominate:


    3.  ST's STM3210E-SK/HT helps start development for the company's ARM   core-based microcontrollers.

    9. Innovate Software  Solutions Hawkboard is an open community board with a  feature set based  on the TI OMAP L138 processor.

     

    Last year I had a customer come to me with a product design that fitted the Beagleboard Hawkboard pretty closely. It would be interesting to see if I could resurrect it. Who knows! Difficult times out here for pitching new products without having at least a prototype to show.

     

    I would also like to add my weight to the suggestion of a relatively simple FPGA board, maybe one of those with a DIP40 header. Not especially for my use, but because I think it will help many of the technicians and engineers out there get into a product area that is likely to be even bigger business in the not too distant future. They are very difficult to get into at a simple level, yet most engineers only need something fairly basic to use, rather than an all-singing all-dancing box which has so much to offer that it gets in the way of actually using the FPGA. Being greedy, a Xilinx eval board would be top of the list, but there are many 3rd party manufacturers who produce FPGA kits.

     

    More personally, I would like to see Analog Devices boards, particularly DDS and ADC/DAC. The lower end DDSes are very easy to develop with, but the faster gear, and the faster/wider ADC/DACs are very demanding  and need professional dev boards.

     

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • julian.higginson
    julian.higginson over 16 years ago

    in order of what I'd most love to play with:

     

    option 3. ST's STM3210E-SK/HT - really keen to get my hands on an arm based dev kit.

    option 7. Freescale's RD1986MMA2260DRD1986MMA2260D - accelerometers are always fun!

    option 8. Microchip’s DM183026 - as would be capacitive touch sensors!

    option 4. Maxim's MAX9830A - class D  amp that works with no filtering sounds really interesting to  play with.

     

     

    thanks,

     

    julian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • danielw
    danielw over 16 years ago

    I'd like to try, the 3. ST's STM3210E-SK/HT as I'd like to start using ARM Cortex devices (My current Favourite is Atmels AVR) as some of my work requires a bit more oomph.(Though I do enjoy squeezing the AVR's and it has definately improved my programming skills!)

     

    I'd Ilso like to try the, Maxim's MAX9830.

     

    Dan.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    Hi,

     

    Thanks for asking.

    These would be my choices:

     

    8. Microchip’s DM183026 mTouch capacitive  evaluation kit helps develop  touch sense applications using PIC16F or  PIC24F MCUs.

     

    Anything from Microchip would be welcome.

     

    7. Freescale's RD1986MMA2260DRD1986MMA2260D TRIAX  3-axis acceleration sensing demo  board combines demos available for  accelerometer applications.

     

    In general, sensor applications, cheap and versatile human interfaces are in my interest.

     

    Regards,

    George

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • awinning
    awinning over 16 years ago

    Thanks very much for your responses, and I hope you had a great Easter break. There were some quite surprising responses. If FPGAs were included, they would have tied with IR, and I suspect if included they would have had even more votes.I think it shows how much they have moved into the mainstream of design now.

     

    1 Hawkboard

    2 Microchip

    3 ST

    4 Freescale

    5 IR

    6 Matrix

    7 Maxim

    8= Nat Semi and Avago

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    Hello,

     

    The Hawkboard really gets my interest due to its power, flexibility and the fact I've been wanting to play with the OMAP-L138! Coming a close second the STM3210E-SK/HT sounds quite intriguing.

     

    Regards,

     

    Al

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    For power supplies, rather than the LM26420 board, I would like to get my hands on a TI REG710-33 or REG711-33 test board. They might not be as new and shiny as the LM26420 but there are not many other devices claiming to produce a stable 3V3 from a supply that wobbles between 1V8 and 5V5.

     

    However, the thing I would most like to road test would be a USB PC-based mixed-mode oscilloscope. Any chance of doing a road test of a BitScope 325U? One of those would be lovely image

    Thanks,
    John.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cksd
    cksd over 16 years ago

    Hi Alistair,

     

    I am interested in the following Kits:

     

    5. Matrix Multimedia's EB018 E-blocks CAN  bus board allows investigation  of the CAN bus protocol

     

    because I am already using Flowcode 4 for PIC development. It is a quite very useful Platform which generates quickly good results.

     

    and:

     

    8. Microchip’s DM183026 mTouch capacitive  evaluation kit helps develop  touch sense applications using PIC16F or  PIC24F MCUs.

     

    because it is a nice Kit  for capacitive application testing.

    9. Innovate Software Solutions Hawkboard is an  open community board with a  feature set based on the TI OMAP L138  processor.

     

    because an open community projects such as this board is a good way to spread and share knowledge to and with a wide interesting group.

     

    Have nice day!

     

    Chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    Hi Alistair,

     

    I'd love to try out the Innovate Software Solutions Hawkboard. I think the OMAP L138 in combination with the open community will provide a great starting point to learn about DSP video processing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Thomas
    Thomas over 16 years ago

    Hi Alistair,

    My preference would be as follows;

    1.) IT's IRS2540 buck convertor development board for HB LED application, to be tried on outdoor LED display for public displays. I do see any of TDK units coming in for trial.

    2.) Maxim's MAX3210E-SK/HT eval kit for Class D amplifier, 2W output for my hobby projects.

    3.) LM26420 Eval board for dual output supply unit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>