RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Help us select RoadTest kits
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 73 replies
  • Subscribers 2766 subscribers
  • Views 6727 views
  • Users 0 members are here
  • RoadTest
  • international
  • rectifier
  • freescale
  • matrix
  • avago
  • development
  • ir
  • maxim
  • national
  • hawkboard
  • kits
Related

Help us select RoadTest kits

awinning
awinning over 16 years ago
Hi,

We'd like to hear your thoughts on dev kits in the market just now. What  kits interest you, or would you maybe like to see on future RoadTests?  Are there any other type of products you'd like to see on RoadTest?  (before anyone suggests, there's no chance of an iPad appearing in the  near term future image )

To get the conversation started we've pasted 9 possible kits below. Tell  us which of these interest you the most and why? As a disclaimer, I'm  not promising to give away the most popular, but we'll certainly talk to  the manufacturers and your views will help us greatly!


1. National Semiconductor’s LM26420 evaluation board demonstrates the  company's LM26420 based solution.

2. International Rectifier's IRS2540 IRS2540/1 buck converter based  development board helps develop HB-LED applications

3. ST's STM3210E-SK/HT helps start development for the company's ARM  core-based microcontrollers.

4. Maxim's MAX9830A evaluation kit uses a filterless class D amplifier to  drive a mono bridge-tied-load speaker.

5. Matrix Multimedia's EB018 E-blocks CAN bus board allows investigation  of the CAN bus protocol.

6. Avago's HFBR-0410HFBR-0410 fiber optics evaluation kit allows first hand  experience with simple DC to 5MBd TTL compatible components.

7. Freescale's RD1986MMA2260DRD1986MMA2260D TRIAX 3-axis acceleration sensing demo  board combines demos available for accelerometer applications.

8. Microchip’s DM183026 mTouch capacitive evaluation kit helps develop  touch sense applications using PIC16F or PIC24F MCUs.

9. Innovate Software Solutions Hawkboard is an open community board with a  feature set based on the TI OMAP L138 processor.
  • Sign in to reply
  • Cancel
  • espanholito
    espanholito over 16 years ago

    Hi Alistair,

     

    From the developments tools you refered i think that these are the most interesting:

     

    3. ST's STM3210E-SK/HT helps start development for the company's ARM  core-based microcontrollers.

    8. Microchip’s DM183026 mTouch capacitive evaluation kit helps develop  touch sense applications using PIC16F or PIC24F MCUs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mountaindude
    mountaindude over 16 years ago

    I'd suggest

     

    8. Microchip’s  DM183026 mTouch capacitive evaluation kit helps develop  touch sense  applications using PIC16F or PIC24F MCUs.

    ...because touch interfaces are becoming almost mandatory and expected by consumers. Would be great to try this out in an informal way.


    9. Innovate Software  Solutions Hawkboard is an open community board with a  feature set based  on the TI OMAP L138 processor.

    ...because it's a nice concept and a good processor. Should be interesting to try this out in various embedded applications.

     

    7. Freescale's  RD1986MMA2260DRD1986MMA2260D TRIAX 3-axis acceleration sensing demo  board combines  demos available for accelerometer applications.

    ...because sensors are hot and accelerometers enable a lot of itneresting consumer applications when used in everyday devices.

     

     

    /G

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago
    Hi all.
    My two votes are for:
    9. Innovate Software Solutions Hawkboard is an open community board with a  feature set based on the TI OMAP L138 processor.
    5. Matrix Multimedia's EB018 E-blocks CAN bus board allows investigation  of the CAN bus protocol.
    As stated by others before, any FPGA development kit would be welcome.
    Regards.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gordonmx
    gordonmx over 16 years ago

    In the near future, how about a ...

     

    10) PICkit 2 Development Programmer/Debugger with Flowcode

    Oh wait, that's coming up this Sunday!   8^)

     

    Have a Happy Easter

     

    Gordon Margulieux

    Salem, OR USA

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • amri_amin
    amri_amin over 16 years ago

    Alistair,

     

    It would be great to have some Microsoft .NET Micro Framework eval boards ( easy development language with many libraries + powerful 32 bits processor).

    This one from GHI electronics is my best:

    http://www.ghielectronics.com/product/128

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    Hi Allistair,

    for me the choice would be :

     

    #9: it is an open source based development and I would kill for it ...(hawkboard.org)  : i just had a look and already have the idea to add a LCD and can bus to extension port for a dashboard application for a plane ...

    #7: i really like sensor and would love to add some features to a RC helicopter...

    #3: ST is one leader of micro electronics and its product are really interresting (also they have good sensors ...)

     

    I have a look if i could help you to add some dev kits to the list.

    Thank you again for giving us these opportunities !!!

    Xavier

     

    PS: i read others proposals and i thought about a fantastic product from actel :

    Smartfusion (in one chip !!!):

    - FPGA

    - ANALOG

    - ARM M3

     

    they got a "low cost" (but not low features) eval kit A2F-EVAL-KIT (http://www.actel.com/products/hardware/devkits_boards/smartfusion_eval.aspx) with a A2F200M3F-FGG484  with ethernet, rs232, oled display, analog inputs and a big extension port ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    Hello!

    I think that this kit would be really usefull for everybody, who want to develop really modern devices:

    8. Microchip’s DM183026 mTouch capacitive evaluation kit helps develop  touch sense applications using PIC16F or PIC24F MCUs.

    I think, that it is time to forget about custom buttons and try to implement in our applications touch screens and touch buttons! I would be really happy to get this kit and understand the principles of mTouch.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    Hello,

     

    as was previously mentioned FPGA is the technology we would like to evaluate, but it is not so easy to do some board by yourself. Mainly because of FPGA manufacturer  obsession of GPIO pin number. Almost all devices are in BGA case style.

     

    I see a big potential with a connection FPGA core together with MCU core (Cortex-M3 as a best choice).

     

    There are two devices I would like to see in Road Test:

     

    1) Actel's SmartFusionTm Evaluation Kit

    http://www.actel.com/products/hardware/devkits_boards/smartfusion_eval.aspx

     

    2) Cypress PSoC 5 (when it will be released)

    http://www.cypress.com/?id=2233

     

    I know PSoC isn't exactly the same thing as I've described above, but it is similar and also interesting.

     

     

    W.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    Hi all,

    Personnaly, I'll prefer :

    9. Innovate Software Solutions Hawkboard  is an open community board with a  feature set based on the TI OMAP L138  processor.

    7. Freescale's RD1986MMA2260DRD1986MMA2260D TRIAX  3-axis acceleration sensing demo  board combines demos available for  accelerometer applications.


    and last

    6. Avago's HFBR-0410HFBR-0410 fiber optics  evaluation kit allows first hand  experience with simple DC to 5MBd TTL  compatible components.

     

    Is it possible to have test on Miwi/Zigbee ?

     

    Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    Hi Alistair,

     

    my all time favorite would be a small Kit for developing with FPGAs... one of the areas in electronics that you are not able to just solder together quickly a running solution. A device for the upper Low-segment would be great to be able to check out alot of different solutions (so most of the examples eg on opencores.com would run sufficiently... up to a little, self-implemented ARM-Core image ).

     

    Second the mentioned International Rectifier's IRS2540  IRS2540/1 board would be great... as HB LEDs will be the future in Lighting and some new solutions are outstanding. Here I also would suggest an old device image But in my opinion one of the most flexible ones and great to "play with" and to collect experience: National Semiconductor LM3445.... offline solution with the capability to be controlled over PWM or the integrated dim decoder (triac).

     

    Also the Microchip’s DM183026 mTouch capacitive  evaluation kit sounds very interesting... and would be useful as the PICs are very easily available and used in almost all devices anyways.

     

    One more device I would love to see a Kit of (not included in your list) would be for Ethernet over Plastic Optical Fiber (POF) like AVAGO AFBR 5978Z.

     

    Happy Easter to all image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>