RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Help us select RoadTest kits
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 73 replies
  • Subscribers 2766 subscribers
  • Views 6738 views
  • Users 0 members are here
  • RoadTest
  • international
  • rectifier
  • freescale
  • matrix
  • avago
  • development
  • ir
  • maxim
  • national
  • hawkboard
  • kits
Related

Help us select RoadTest kits

awinning
awinning over 16 years ago
Hi,

We'd like to hear your thoughts on dev kits in the market just now. What  kits interest you, or would you maybe like to see on future RoadTests?  Are there any other type of products you'd like to see on RoadTest?  (before anyone suggests, there's no chance of an iPad appearing in the  near term future image )

To get the conversation started we've pasted 9 possible kits below. Tell  us which of these interest you the most and why? As a disclaimer, I'm  not promising to give away the most popular, but we'll certainly talk to  the manufacturers and your views will help us greatly!


1. National Semiconductor’s LM26420 evaluation board demonstrates the  company's LM26420 based solution.

2. International Rectifier's IRS2540 IRS2540/1 buck converter based  development board helps develop HB-LED applications

3. ST's STM3210E-SK/HT helps start development for the company's ARM  core-based microcontrollers.

4. Maxim's MAX9830A evaluation kit uses a filterless class D amplifier to  drive a mono bridge-tied-load speaker.

5. Matrix Multimedia's EB018 E-blocks CAN bus board allows investigation  of the CAN bus protocol.

6. Avago's HFBR-0410HFBR-0410 fiber optics evaluation kit allows first hand  experience with simple DC to 5MBd TTL compatible components.

7. Freescale's RD1986MMA2260DRD1986MMA2260D TRIAX 3-axis acceleration sensing demo  board combines demos available for accelerometer applications.

8. Microchip’s DM183026 mTouch capacitive evaluation kit helps develop  touch sense applications using PIC16F or PIC24F MCUs.

9. Innovate Software Solutions Hawkboard is an open community board with a  feature set based on the TI OMAP L138 processor.
  • Sign in to reply
  • Cancel
  • icserny
    icserny over 16 years ago

    Hi Alistair,

     

    My top 3 choices are:

    1) Innovate Software Solutions Hawkboard  is an open community board with a  feature set based on the TI OMAP L138  processor.- This board looks very promising. I would like to try it as a central unit of an autonomous measurement control and data acquisition system in our electron spectroscopy laboratory.

     

    2) Microchip’s DM183026 mTouch capacitive  evaluation kit helps develop  touch sense applications using PIC16F or  PIC24F MCUs.- I am especially interested in this development kit of Microchip, because it is based on the MCUs I am working with presently. Touch sensing could help me to extend my applications with better human interface.

     

    3) ST's STM3210E-SK/HT helps start  development for the company's ARM  core-based microcontrollers. - ARM microcontrollers could be the next step toward the more CPU demanding applications, when the 8 or 16 bit MCU-s (which I am presently using) are insufficient. 

     

    Best regards,

     

    István Cserny

    Debrecen, Hungary


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    Hi,

     

    I woud tip in preference order for Hawkboard, ST's STM3210E-SK/HT and for the Freescale one.

     

    Murat

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    I would like to vote for 4), 7) and 8).

    Reason: I am intrested in sensing of accelerations (vibrations, tracking), capacitive user interface and amplifying sensor signals.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    My interests would run to:

     

    3. ST's STM3210E-SK/HT - ARM core

    7. Freescale's RD1986MMA2260DRD1986MMA2260D TRIAX 3-axis acceleration sensing

    9. Innovate Software Solutions Hawkboard - TI OMAP L138 processor

     

    Presently developing consumer devices with the STM32F101 (also various AVR's, and SiLabs 8051's).

    The STM32 primer2 has been very fun to experiment with - it would be interesting to test a different kit.

     

    Cheers,

       Robert.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    For sure my first choice is number 3, ST's STM3210E-SK/HT.

    But I think that also number 9 (Innovate Software Solutions Hawkboard) is really interesting!

     

    Thanks for the opportunity to give our opinion!!

     

    Davide Calusini

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ms_koster
    ms_koster over 16 years ago

    Hi Alistair,

     

    My preference:

     

    8. Microchip’s DM183026 mTouch capacitive evaluation kit helps develop  touch sense applications using PIC16F or PIC24F MCUs.

     

    Touch screen apps seem to trickle down into every application these days, so it would be interesting to get our hands on an implementation from a supplier that delivers affordable ucontrollers with it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mschwingen
    mschwingen over 16 years ago
    #9 Innovate Software Solutions Hawkboard 
    #3 ST's STM3210E-SK/HT
    because both seem to enable real hands-on experience, running your own code and 
    not just canned demos supplied with the board.

    It should be interesting to test open-source tools on these boards, aside from
    the vendor-supplied windows stuff - from a first glance, gcc + OpenOCD might support both.


    Michael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    hi alistar

    surely my favourite options are :

    2, International  Rectifier's IRS2540 IRS2540/1 buck converter based  development board  helps develop HB-LED applications

    because field of DCDC conveter is rapidly growing and there are lots of different good product especially from IR but also the

    high brightness LED field is a very interesting application


    9. Innovate Software Solutions Hawkboard  is an open community board with a  feature set based on the TI OMAP L138 processor.

    is very interesting because i have already use Beagle Board from TI and I think tha OMAP is an amazing microcontroller but at the same

    time I think Hawkboardis better than Beagle especially for the high number of peripheric like LAN, etc,,,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    Hi Alistair,

     

    I would be interested in the ARM platform.

    And also FPGA boards in general as Amine already mentioned.

     

    Thanks,

     

     

    Elias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    Hi Alistair,

     

    Kits 7 (Freescale accelerometer) and 8 (Microchip mTouch) seem very interesting, and would provide a learning tool with a new product area for me and most likely others in this group.  Thank you for all your effort!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>