Products
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
RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum PIC32 Ethernet Starter Kit review
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 2751 subscribers
  • Views 1033 views
  • Users 0 members are here
Related

PIC32 Ethernet Starter Kit review

tayken
tayken over 16 years ago

The PIC32 Ethernet Starter Kit is the 3rd version of a series of PIC32 starter kits. This  is not my first time for working with Ethernet enabled  microcontrollers  but a first for PIC32 family.

Package Content

The kit came in a black plastic box which resembles a DVD box. The contents were:

  • PIC32 Ethernet Starter Kit development board
  • USB Mini-B to full-sized A cable – USB debug cable to debug and power the board
  • USB Micro-B to full-sized A cable – PIC32 USB cable to communicate with the PIC32 USB port
  • RJ-45 CAT5 Ethernet patch cable – Ethernet CAT5 cable to communicate with the PIC32      Ethernet port
  • Software CD
  • Registration card

 

image

Package contents

 

Hardware

The PIC32 Ethernet Starter Kit board has the same form factor and expansion connector as the previous starter kits. It contains PIC32MX795F512L as the main microcontroller, a PIC32MX440F512H as the on-board debugger, a National DP83848 PHY for ethernet connection, a 120-pin Hirose connector for expansions  and three LEDs (green, orange and red) & three pushbuttons for user  interaction.

 

image

Top side, switches & LEDs highlighted

 

The board also has a USB Mini-B for debugger connection, a USB  Micro-A/B for USB peripheral and OTG applications, a USB full-sized A  for USB host applications and a RJ-45 jack for Ethernet connection.

 

image

USB & Ethernet Connectors

 

The board also has some unpopulated parts such as Y3, C15, C16 for  RTCC; R24 and R27 for USB-OTG voltage converter and C19-C24 decoupling  capacitors.

 

image

Top side, unpopulated parts highlighted

 

image

Bottom side, unpopulated parts highlighted

 

The microcontroller has the following specifications:

  • MCU Core: 80MHz, 1.56 DMIPS/MHz, 32-bit MIPS M4KRegistered Core USB  2.0 On-The-Go peripheral with integrated PHY 10/100 Ethernet MAC with  MII/RMII Interfaces; 2 x CAN2.0b modules with 1024 buffers; 8 dedicated  DMA Channels for USB OTG, Ethernet, and CAN; 5 stage pipeline, Harvard  architecture; MIPS16e mode for up to 40% smaller code size; single cycle  multiply and hardware divide unit; 32 x 32-bit core registers; 32 x  32-bit shadow registers; and fast context switch & interrupt  response.
  • MCU System Features: 512K flash (plus 12K boot flash); 128K  RAM (can execute from RAM;) 8 channel general hardware DMA controller  flash; pre-fetch module with 256 byte cache; lock instructions or data  in cache for fast access; and programmable vector interrupt controller.
  • Analog Features: Fast and accurate 16 channel 10-bit ADC,  max 1 mega sample per second at +/- 1LSB, and conversion available  during SLEEP & IDLE.
  • Power Management Modes: RUN, IDLE, and SLEEP modes; multiple switchable clock modes for each power mode, enables optimum power settings.
  • Debug Features: iFlow Trace: Non-intrusive Hardware  Instruction Trace port (5 Wires); 8 hardware breakpoints (6 Instruction  and 2 Data); 2 wire programming and debugging interface; and JTAG  interface supporting Programming, Debugging and Boundary scan.
  • Other MCU Features: Fail-Safe Clock Monitor – allows safe  shutdown if clock fails; 2 internal oscillators (8MHz & 31KHz);  hardware RTCC (Real-Time Clock and Calendar with Alarms); watchdog timer  with separate RC oscillator; pin compatible with 16-bit PIC MCUs; and  serial communication modules allow flexible UART/SPI/I2CTm configuration.

Software Installation

The software CD  in the kit is a bit outdated, but I installed it  anyway for the drivers. However, this caused problems with MPLAB IDE I  have (8.50), I couldn’t open the latest version installed on my system  and the version that was installed by the CD kept crashing each time I  tried to connect to the board. So I zipped the starter kit folder,  uninstalled it and unzipped so that I can use the demo files and other  documentation in these folders.

Driver for the Debugger

The installation manual gives the general idea about how to install  the device drivers. If you have a full installation of the latest MPLAB  IDE, it also comes with PIC32 Starter Kit debugger drivers, so you can  use either the drivers inside the starter kit bundle or MPLAB IDE.

Information

PIC32MX Starter Kit User’s Guide is the  ultimate document for this board. It contains hardware, software and  demo application information for all three starter kits. Each demo has a  description in this document and also all the starter kits have a block  diagram, board layout and schematic so you can use these to develop  your own hardware in the future. However, care should be taken as this  document contains some errors because of copy-paste effects.

Each demo contains an HTML file in their own project directory where  how to configure the board and how to use the application is explained.  It is crucial to read these files before trying the demonstrations so  that you do not try to find an error in the program when there are none,  as I did.

Initial Use

The PIC32 Starter Kit comes pre-programmed with the Simon Says game.  You try to mimic the light patters for as long as you can before you get  bored and move to the other demos.

Building Tutorial Projects

All the tutorials come as a project, so what you have to do is to  open the project file, compile the code and upload the hex code  generated into the flash memory of the PIC32. Of course you can use  another programmers/debuggers but it is really easy with the PIC32  Starter Kit debugger.

One warning: As there are hardware differences between different  starter kits, some demos have multiple project files. You have to open  and compile the appropriate project file, otherwise you get warnings and  errors.

All projects are to the point, with enough documentation and have  detailed comments. So you can use them as a basis for your own codes.

Conclusion

This is a goodly designed hardware that can show you the capabilities  of a PIC32 series microcontroller. It has a small form factor, lots of  I/O and lots of capabilities.

However, I really wished for some improvements, for example for  people who already have the latest MPLAB IDE, the software bundle  installation creates problems so I think having a zip archive with only  tutorials can be helpful for those people.

Also although this kit has awesome I/O capabilities, you are limited  to the USB & Ethernet connectors that are available.  The PIC32 I/O Expansion Board is a little expensive (72$, same price with the Ethernet Starter Kit)  for a simple project so a breakout board with only a Hirose connector  and some pins would be better for me. One of my professors wanted to use  the first starter kit for education but decided not to as the board  itself was not capable for the whole course and the expansion board  available was more expensive than the starter kit itself! So another  expansion board is a must in my opinion.

I didn’t had the chance to test this board with my Linux computer yet  but there are C32 compilers for Linux so I think it will be easy.

  • Sign in to reply
  • Cancel
Parents
  • tayken
    tayken over 16 years ago
    This is my review, if I can get my hands on some kind of an expansion board, I will write about them in my blog.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • tayken
    tayken over 16 years ago
    This is my review, if I can get my hands on some kind of an expansion board, I will write about them in my blog.