Products
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
RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Road Test Review: Agilent U1620A
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 2750 subscribers
  • Views 808 views
  • Users 0 members are here
Related

Road Test Review: Agilent U1620A

aemarconnet
aemarconnet over 14 years ago

First and foremost this is an amazing device at a great sales price considering how feature-packed it is. It has been a lot of fun, convenient, and very exciting to work with. It performs well across the board and is loaded with useful features. During my road test of this device it has been an invaluable asset easily worth the ~$3000 commercial cost. It has aided in dignostic and support work in the RF industry and performed well.

 

I hesitate to use such a subjective measurement as the "5 star review scale", but it seems to have become ubiquitous of the online market place. I would gladly award this device a 5 star review save for 1 problem that i experienced with RF coupling across channels (see the section on “Noise in output channels”). Taking that into consideration i believe that it still would deserve a 4 to 4.5 stars, and would re-award 5 stars if a work-around like the one I created was commercially available.

 

The U1620A is rugged, useful, powerful, feature packed, extreemely accurate and quite reliable.

 

With the above underlined statement, i would like to go into some of the problems, concerns, and limitations of the device.

 

INITIAL THOUGHTS

When I received the unit in the mail I felt like I hit the jackpot and rushed to open it, sadly, it needed to be fully charged prior to use, however I can say that my initial reaction was the following:

I was very impressed with the rugged exterior, the silicon buttons provided a good tactile response and the unit was surprisingly small and light considering how much technology must be crammed inside. The handle (fabric and Velcro) took a bit of getting used to.

It seems that the device is intended to be held with the right hand in the strap, supported by the left forearm. I would have liked to have seen mounting brackets for a right handed individual (so that the right hand is free to use probes and operate the unit). Regardless, after a few hours one becomes accustomed to holding it, and often I have the unit sitting on a ledge or table near my device under test.

 

DISPLAY

On the first day operating the product, I had a blast; I took it to every electrical source I could find in my facility. The display was very bright and clear, and the user interface was quite intuitive. I even took the opportunity to get it outside to see how the monitor looked in the sunlight. I was quite impressed by how readable the display was in the “outdoor” mode. Even on a bright sunny day text and scope measurements were quite clear.

 

NECK AND SHOULDER STRAPS

While examining the noise in the electrical system of my 2007 Toyota Highlander (with and without filtering capacitor) The Supplied neck-strap broke and the device fell 3 feet...there is some minor scuffing, however the rubberized case absorbed the impact well. I was rather dissatisfied that a $3000 piece of equipment was shipped with such a cheap strap; in addition to being physically weak (poorly designed seam between strips of fabric) it feels cheap compared to the actual handheld unit. On another note: I would have loved to see neoprene used to make the strap more comfortable, in an un-collared shirt it can chafe a good bit around the neck…while on the subject of straps the hand strap, when adjusted to accept a larger hand, does not have sufficient strength. On multiple occasions the velcro has released and thus i nearly drop the device.

 

PRECISION CONTROL - Lacking

From the very beginning, when taking measurements I longed for some form of precise input. The range, position, and time controls are all operated with up/Down +/- type controls. This method of controlling the input seemed too clunky and did not give me the control that I desired. I greatly missed having a knob-style input that is standard with desktop scopes. I understand that such a knob would compromise the ruggedness of the device, however a low profile solution could be found similar to the knobs seen in DJ Audio Equipment. Via software a single “universal” knob could easily be designated to control whichever button had been last used (eg if one were to tap the “time scale” to a longer span, then turning said dial would allow fine-tuning of that input)….along the same lines I would also like to see the addition of a num pad or mini-keyboard, it seems that the device has limited “USB On-The-Go” support, I would like to see USB support for a keyboard.

 

MEMORY SLOT NAMES

I work in a manufacturing facility and I manage multiple products. When I started saving data to the internal memory I was disappointed to find that these files were names solely based on the memory “Slots” and timestamps. Even saving to an external flash drive one is limited to the timestamp. This does not allow me to keep track my data, I have to keep a notebook to log when I was measuring what device.

 

SOFTWARE INSTABILITY (FIRMWARE UPDATE CORRECTED?)

During my first few days using the device I experienced multiple instances of a very similar software crash. This particular crash appeared as though the display froze and during a refresh cycle the majority of the screen was wiped to black. Leaving only small fragments of the Background grid still illuminated on the display…There was no real pattern behind this crash…I would simply be navigating the menu and suddenly it would occur…Later, I updated to the latest firmware, and since then have not experience this error.

 

!!!!!!!NOISE ON INPUT CHANNELS!!!!!!!!!

This following error is perhaps the most frustrating for me. Working with the high frequencies, high voltages, high noise (electromagnetic), and high powers associated with the RF industry I immediately took note of the poor isolation/shielding between channels.

To state it as simply as I can: when only one line of the scope was in use I saw amazingly clear plots of the waveform. However when the second channel was activated I began to see a great deal of noise, to the point where the waveform looked nothing like it should. In some instances I even noticed that the shielding channel 2 with my finger would wildly manipulate channel 1. Unfortunately I cannot provide images as the content is proprietary. However, I realized that by making the unit portable we sacrifice a proper ground, and to make it compact we sacrifice shielding: as such, both channels psudo-float at a potential and energy is able to somehow couple between channels. Especially when both inputs have a high frequency/power input, we see inductive(?) coupling of this energy to the other channel of the scope. In my experimentation I found that the trick to reducing noise is to provide a common ground. My initial testing was simply done with a paperclip: bent to contact the outer conductor  of each channel (CH1, CH2, Trig). This was very successful, but it was difficult to maintain a good connection with the paper clip, I plan to produce a better common ground using 3 coax elbows linked with wire. If hardware modifications are not made to the devices next generation to combat this problem, I would recommend that such a “grounding Compensator” be made commercially available.

 

BATTERY DISPLAY

Since upgrading to the latest firmware I have noticed that the battery life is not accurately displayed on the device. It will show the red low-power icon even when the display on the battery shows a full charge. I believe that the icon simply gets “stuck” as it no longer shows the “charging” icon either. This can be re-set by pulling the battery, simply power-cycling the unit does not always fix the icon.

 

LOGGER REFRESH RATE

During my experience with the device I found that that the fixed refresh rate of apprx 1 sample per second was insufficient. When working with some equipment it is important to be able to react quickly. To be able to see a trend and prevent a fatal malfunction that second can make a world of difference. I think that it would be nice if the user were able to change a setting to sacrifice some of the accuracy (decimal points) and increase the refresh rate to at least 2 Hz if not more. I am unsure if this could be done within the software/firmware, or if it would require a hardware change, but I believe that it is a feature that is well worth looking into.

 

LOGGER DISPLAY

When in the Data Logger mode this unit shows a plot of the measurement against time. As time progresses the unit automatically scales the division of time such that all time is displayed. This can make it hard to visually examine the rate of change. I believe fixed width (Rolling option) would be a worthy addition (eg trim to only show the last 30 seconds of data).

 

USB DAQ INTERFACE

I have done some experimentation, however I have been unable to configure the device for use as a Data Acquisition module via USB. I think that integration with labview or even excel could increase the utility of this hardware.

  • Sign in to reply
  • Cancel
Parents
  • aemarconnet
    aemarconnet over 14 years ago

    I would also like to mention that i would be happy to answer any questions privately or publicly about the device or my review. Please ask questions, or leave your thoughts.

     

    Regards

    Alex

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to aemarconnet

    Good review Alex, very informative.

     

     

    Regards,

     

     

    Elias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to aemarconnet

    Good review Alex, very informative.

     

     

    Regards,

     

     

    Elias