Products
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
RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum road testing the EFM32™︎ Zero Gecko Starter Kit - Part 3
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 2750 subscribers
  • Views 570 views
  • Users 0 members are here
  • RoadTest
  • review
  • zero_gecko_starter_kit
Related

road testing the EFM32™︎ Zero Gecko Starter Kit - Part 3

Jan Cumps
Jan Cumps over 11 years ago

part 2: unboxing and checking the demo applications, first debug cycle

 

I've checked the different energy modes.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Road Test 2: measure power consumption during various modes

 

The starter kit comes with several energy mode examples. I've tested two of them.

 

The energy example: this project switches between clock frequencies (7, 11, 14 and 21 MHz) every few seconds. It displays the voltage and currency stats of the USB supply on the LCD. The power monitor works exclusively when the PWR selection switch is in DEBUG position.

 

The emode example: this one prompt for the desired energy mode and keeps running in that mode once selected. This exercise is handy when you want to do measurements in a stable state. These options are available:

  • EM0 24MHz (primes calc): the processor goes into a loop to calculate prime numbers in energy mode 0 - a good mode to learn how the profiler displays energy use per function
  • EM1 24MHz: runs in energy mode 1 at full speed
  • EM2 32kHz: energy mode at low speed
  • EM3 and EM4: go to sleep modes 3 and 4 respectively
  • EM2+RTC: run in energy mode 2, activate on pulse counter interrupt
  • EM2 and EM3+RTC+LCD: wake up on pulse counter interrupt, update display and go back to sleep
  • User: full speed standard mode running in an endless for(;;) loop.
  • Sign in to reply
  • Cancel
  • Jan Cumps
    Jan Cumps over 11 years ago

    I monitor the current with the Energy Profiler and with a µCurrent. To be able to measure current, I desoldered R704 and populated P701 with male print headers.

    When not measuring, I bridge pin 1 and 2. When measuring, I put a current meter between pin 1 and 2.

    image

     

     

    Part 4: the tutorials