Products
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
RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Which would you get Rasberry PI 2 or Gizmo 2 and why?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 2751 subscribers
  • Views 2305 views
  • Users 0 members are here
Related

Which would you get Rasberry PI 2 or Gizmo 2 and why?

libernullmal
libernullmal over 11 years ago

Just curious between the two and I wanted to know what the pros and cons between the two?

  • Sign in to reply
  • Cancel
Parents
  • dtsartsanis
    dtsartsanis over 11 years ago

    Gizmo 2 is using a x86 processor which means that u can install windows.So if u are not familliar with Linux software and u can spend $199 go for it.

    Raspberry Pi 2 now is a complete pc in a compact size, with a lot documentation and tutorials from the community and it costs almost nothing.

    I choose Pi

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to dtsartsanis

    dtsartsanis I beg to differ. Linux software knowledge is not a prerequisite for Raspberry Pi. He could download and install Openelec. Start it and be in full screen without typing any Linux command. Openelec  turns the Raspberry Pi into a media center playing movies on USB or off the internet.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dtsartsanis
    dtsartsanis over 11 years ago in reply to clem57

    Yes i agree, but if u want to use it as a pc u have to install software through the command line or install Synaptic.And is not always easy for windows users to use the command line.

    For me Raspi is a great tool to learn and explore Linux and other great projects.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dtsartsanis
    dtsartsanis over 11 years ago in reply to clem57

    Yes i agree, but if u want to use it as a pc u have to install software through the command line or install Synaptic.And is not always easy for windows users to use the command line.

    For me Raspi is a great tool to learn and explore Linux and other great projects.