RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Clock problems on Basys 3
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 4 answers
  • Subscribers 2751 subscribers
  • Views 4015 views
  • Users 0 members are here
  • basys-3
  • fpga
  • vga
Related

Clock problems on Basys 3

nixiefairy
nixiefairy over 8 years ago

Hey everyone!

I have been busy working on the roadtest of Basys 3 entry level board for a few days now. Recently, I got stuck while implementing one of the projects.

I am trying run a snake-apple game on the Basys 3 using a VGA input monitor. Thing is I am getting an error saying that my refresh rate is incorrect. For a 640X580 display, pixel rate has to be close to 25Mhz. Even after setting up the frequency of the display, I am still hitting a wall. Any suggestions? Codes and error attached below (vga_tst is top module):

Attachments:
codes.zip
image
  • Sign in to reply
  • Cancel
Parents
  • nixiefairy
    0 nixiefairy over 8 years ago

    Okay so I got the solution to the problem : It was wrong implementation of the clock of the clock divider module. I've written a new one which can be used by the community for dividing their clock. Feel free to use it.

    module newClk(

    input master_clk,

    output reg op_clk,

    input num);

                                                  //usage: masterclk=100Mhz(say) so for op_clk=25Mhz, num should be num=4

    integer x=0;

    always@ (posedge master_clk)

    begin

    x<=x+1;

        if(x==num)

            begin

            op_clk<=~op_clk;

            x<=0;    

    end

    else

    op_clk<=op_clk;

    end

    endmodule

    Thanks everyone for your input!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 8 years ago in reply to nixiefairy

    I'm not a frequent user of Verilog but I don't think you need this last bit, op_clk is a reg so will keep its value - so you only need to drive it when it changes.

     

    else

    op_clk<=op_clk;

    end

     

     

     

    You may have issues with simulation because op_clk is undefined at start up so ~op_clk is undefined, so op_clk is always undefined. In hardware this doesn't matter - it must start up as something but the simulator may not see it that way.

     

    If you want op_clk defined as you come out of reset then you need a reset input to your module and to use that to pre-set op_clk.

     

    Xilinx argue strongly against resetting everything.

     

    Google ' xilinx synchronous reset verilog' to learn more than you ever thought possible about resets !

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 8 years ago in reply to nixiefairy

    I'm not a frequent user of Verilog but I don't think you need this last bit, op_clk is a reg so will keep its value - so you only need to drive it when it changes.

     

    else

    op_clk<=op_clk;

    end

     

     

     

    You may have issues with simulation because op_clk is undefined at start up so ~op_clk is undefined, so op_clk is always undefined. In hardware this doesn't matter - it must start up as something but the simulator may not see it that way.

     

    If you want op_clk defined as you come out of reset then you need a reset input to your module and to use that to pre-set op_clk.

     

    Xilinx argue strongly against resetting everything.

     

    Google ' xilinx synchronous reset verilog' to learn more than you ever thought possible about resets !

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • nixiefairy
    0 nixiefairy over 8 years ago in reply to michaelkellett

    Hey Michael,

     

    1) I am leaving op_clk<=op_clk cause you just don't know how it effects an FPGA. Better to have a safe run than having an error!

    2) Fair point on initializing op_clk. To be honest, I really didn't simulate it, other than using the ILA occasionally.

    3) I am leaving the clock signal asynchronous to the reset for the time being.

    Thanks for all the input you have given!