RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Clock problems on Basys 3
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 4 answers
  • Subscribers 2751 subscribers
  • Views 4015 views
  • Users 0 members are here
  • basys-3
  • fpga
  • vga
Related

Clock problems on Basys 3

nixiefairy
nixiefairy over 8 years ago

Hey everyone!

I have been busy working on the roadtest of Basys 3 entry level board for a few days now. Recently, I got stuck while implementing one of the projects.

I am trying run a snake-apple game on the Basys 3 using a VGA input monitor. Thing is I am getting an error saying that my refresh rate is incorrect. For a 640X580 display, pixel rate has to be close to 25Mhz. Even after setting up the frequency of the display, I am still hitting a wall. Any suggestions? Codes and error attached below (vga_tst is top module):

Attachments:
codes.zip
image
  • Sign in to reply
  • Cancel
Parents
  • nixiefairy
    0 nixiefairy over 8 years ago

    Okay so I got the solution to the problem : It was wrong implementation of the clock of the clock divider module. I've written a new one which can be used by the community for dividing their clock. Feel free to use it.

    module newClk(

    input master_clk,

    output reg op_clk,

    input num);

                                                  //usage: masterclk=100Mhz(say) so for op_clk=25Mhz, num should be num=4

    integer x=0;

    always@ (posedge master_clk)

    begin

    x<=x+1;

        if(x==num)

            begin

            op_clk<=~op_clk;

            x<=0;    

    end

    else

    op_clk<=op_clk;

    end

    endmodule

    Thanks everyone for your input!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • gecoz
    0 gecoz over 8 years ago in reply to nixiefairy

    Hi Eashan,

     

    Glad to hear you managed to solve the problem. I see now you have implemented a generic module-"num" counter. For the Basys 3 , have you used the 100MHz reference clock with mod-4 counter then? I'm asking because in your previous reply to my suggestion, you said that solution it didn't work, so I'm curious to know what worked.

     

    fabio

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nixiefairy
    0 nixiefairy over 8 years ago in reply to gecoz

    Hey Fabio,

    Yeah it was a great relief to finally have it working. I have put the project results in my review: FPGA Essentials: Basys 3 Artix-7 FPGA - Review .

    For my project I've used a 50Mhz signal coming from the FPGA. This was then passed to a clock divider module which then gave a 25Mhz clock signal. So yes, I used it as a mod-2 counter.
    It was something to do with the previous lines of code I was using.

     

    reg pixel_reg;

    wire pixel_next, pixel_tick;

     

    always @(posedge clk)

      pixel_reg <= pixel_next;

     

    assign pixel_next = ~pixel_reg; // next state is complement of current

     

    assign pixel_tick = (pixel_reg == 0); // assert tick half of the time

     

    Probably I didn't instantiate a separate module? Or probably I called this where my VGA sync signals were generating, I am not entirely sure.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • nixiefairy
    0 nixiefairy over 8 years ago in reply to gecoz

    Hey Fabio,

    Yeah it was a great relief to finally have it working. I have put the project results in my review: FPGA Essentials: Basys 3 Artix-7 FPGA - Review .

    For my project I've used a 50Mhz signal coming from the FPGA. This was then passed to a clock divider module which then gave a 25Mhz clock signal. So yes, I used it as a mod-2 counter.
    It was something to do with the previous lines of code I was using.

     

    reg pixel_reg;

    wire pixel_next, pixel_tick;

     

    always @(posedge clk)

      pixel_reg <= pixel_next;

     

    assign pixel_next = ~pixel_reg; // next state is complement of current

     

    assign pixel_tick = (pixel_reg == 0); // assert tick half of the time

     

    Probably I didn't instantiate a separate module? Or probably I called this where my VGA sync signals were generating, I am not entirely sure.