RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum What is the format to add to an Element14 Blog
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 2745 subscribers
  • Views 850 views
  • Users 0 members are here
Related

What is the format to add to an Element14 Blog

colporteur
colporteur over 6 years ago

What is the process to update a Blog? Are Blog posts individual CREATES or Add to Comments?

 

I'm a novice at using a Blog. I have started the following Blog on Element14 The Road to Raspberry Pi4B/ PoE Hat RoadTest Review (Introduction) and would like to post an update. Do just use the Add A Comment button at the bottom of the post or do I CREATE a new Blog enter using the same title and then add the material there?

 

I can see pluses and minus for both approaches but would like to follow the norms for blogging. Can anyone provide a recommendation?

  • Sign in to reply
  • Cancel
Parents
  • genebren
    0 genebren over 6 years ago

    Sean,

     

    It is possible to edit an existing blog.  On the righthand side of the screen is an actions list and in it is an 'Edit' button/link.  This allows you modify the blog.

     

    I have used this feature to add updates to an existing blog (as have others).  Depending on the amount of new material, I either append to the initial blog (small additions) create a new blog (large additions).

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • genebren
    0 genebren over 6 years ago

    Sean,

     

    It is possible to edit an existing blog.  On the righthand side of the screen is an actions list and in it is an 'Edit' button/link.  This allows you modify the blog.

     

    I have used this feature to add updates to an existing blog (as have others).  Depending on the amount of new material, I either append to the initial blog (small additions) create a new blog (large additions).

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • colporteur
    0 colporteur over 6 years ago in reply to genebren

    Thanks GB genebren . I'm trying to determine what constitutes a small or large change and then applying the criteria.

     

    If you just keep editing a Blog post, what prevents it from becoming a running toilet?

     

    I guess the decision points you choose to break posts. Hummm, I have to do some thinking about this.I'm trying to prevent the reader from endless scrolling. The Blog is on Pi4/PoE but I have a post on test criteria, another on cable specification, another on power requirements.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer