RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Comments for using RPi with SPI memory
  • Blogs
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 22 replies
  • Answers 2 answers
  • Subscribers 2715 subscribers
  • Views 4363 views
  • Users 0 members are here
  • ram
  • raspberry
  • microchip
  • pi
  • spi
  • sram
Related

Comments for using RPi with SPI memory

clem57
clem57 over 11 years ago

image

Here are my notes so far. Any comments or issues please let me know. I think I am on the right track.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago +1
    Why do you want to connect a tiny additional memory to your PI ? There is no reason why it couldn't work - it just seems a bit odd. MK
  • bbolo1
    bbolo1 over 11 years ago in reply to clem57 +1
    Here are a few examples of SPI RTC chips: ST M41T93 Microchip RTCs NXP PCF2123 Maxim RTC and another Maxim RTC as for the CS manipulation, here are a couple of pages ( 1 , 2 ) that might help you. You…
  • clem57
    clem57 over 11 years ago +1 suggested
    Ok! I have learned that I should use pins 24/26 as CE0/CE1 instead of pin15(GPIO 22) because this alleviates me writing extra code. I plan on using Python SPIDEV from GitHub... Thanks for Elektor Academy…
Parents
  • clem57
    0 clem57 over 11 years ago

    Ok,

         I picked this for the following reasons:

    • Learn how SPI will be used
    • Will add more chips to play with CS logic. Then I would like to use two GPIO for 4 chips with external TTL chip
    • Even more later, I will maybe use flash,EEPROM same interface ...

     

    The mad professor image

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 11 years ago

    Ok,

         I picked this for the following reasons:

    • Learn how SPI will be used
    • Will add more chips to play with CS logic. Then I would like to use two GPIO for 4 chips with external TTL chip
    • Even more later, I will maybe use flash,EEPROM same interface ...

     

    The mad professor image

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data