RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum What to do when a review doesn't go as planned
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 2756 subscribers
  • Views 4220 views
  • Users 0 members are here
Related

What to do when a review doesn't go as planned

scottiebabe
scottiebabe over 4 years ago

I am currently having an issue reviewing the MAX77714 EVK where the 32k XO isn't running. Its not really a hardware issue as I can get the XO to run just with the capacitance of 2 10x scope probes. The issue has to do with configuring the PMIC to enable its on die load capacitors for the 32k oscillator.

 

I can't even try to enable the load capacitors because the evaluation software doesn't have the correct register map for the PMIC. The evaluation tool locates the 32KLOAD bitfield in register 0x31:

image

 

When actually the bitfield is in register 0x30 (from the datasheet: https://datasheets.maximintegrated.com/en/ds/MAX77714.pdf ):

image

 

Actually as I write this, even if the 32KLoad register was addressed correctly in the evaluation software it is readonly so I still wouldn't be able to change it. So why isn't it booting with a value of 0b00 instead of 0b10? Wrong OTP config?

 

So, my questions is what do reviewers typically do in this situation?I don't want to write a scathing review over something so silly.

 

I suppose I will start by seeing if maxim will confirm the issue with the EVK and see if they can provide a software fix or want to send new hardware.

 

One of the uncertainties I had with my last review was determining if I am reviewing the silicon product or the evaluation platform. In this case, am I reviewing the MAX77714 or the EVK and software for the MAX77714? Or, a bit a both? Or, is it up to the reviewer?

 

Thanks

  • Sign in to reply
  • Cancel
Parents
  • navadeepganeshu
    navadeepganeshu over 4 years ago

    I too see the same thing happening wherein the register values are incorrectly mapped against the capacitance value choices. But I am curious, why that value needs to be changed/configured? Seems like internally it's taking default capacitance value and clocks fine. Simply for testing purposes? Alright.

     

    Apart, there are minor bugs where the whole 'register explorer' tab GUI minimizes when the configuration tray is pulled down(i saw it happening twice. now, not finding where exactly was it,......murphy is real)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • navadeepganeshu
    navadeepganeshu over 4 years ago

    I too see the same thing happening wherein the register values are incorrectly mapped against the capacitance value choices. But I am curious, why that value needs to be changed/configured? Seems like internally it's taking default capacitance value and clocks fine. Simply for testing purposes? Alright.

     

    Apart, there are minor bugs where the whole 'register explorer' tab GUI minimizes when the configuration tray is pulled down(i saw it happening twice. now, not finding where exactly was it,......murphy is real)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • scottiebabe
    scottiebabe over 4 years ago in reply to navadeepganeshu

    Don't let my experiences bias your review of the EVK. Its plausible your board is different from mine. I look forward to reading your review image.