RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum How Long Would It Take for You to RoadTest the Raspberry Pi 4 Model B (prep, testing and writing)?
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 2662 subscribers
  • Views 5575 views
  • Users 0 members are here
  • RoadTest
  • time to roadtest
  • raspberry pi 4 model b
Related

How Long Would It Take for You to RoadTest the Raspberry Pi 4 Model B (prep, testing and writing)?

rscasny
rscasny over 3 years ago

  • Sign in to reply
  • Cancel

Top Replies

  • fmilburn
    fmilburn over 3 years ago +4
    I did this Pi 4 Roadtest a few years back: /products/roadtest/rv/roadtest_reviews/685/roadtest_the_raspber I can’t remember now but would guess it took at least 24 hours.
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to robogary +3
    For that road test? A Lot. I'd say 80 hours at least. Most likely more. Not all of that time was efficiently used. Sometimes it was just fiddling around and see how things behaved. For the test gizmo…
  • robogary
    robogary over 3 years ago +2
    Ok, I'm the clown that voted more than 40 hrs. Know why ? Documentation is 50% or more of a road test. There is linux stuff to play with, python, pi hats, etc. I'd want to build a donkey car with it…
  • ntewinkel
    ntewinkel over 3 years ago in reply to cstanton

    Agreed, and if anything happens to not go perfectly - oops wrong software version, oops wrong pin, etc etc - then it’s easy to waste several hours just trying to figure out what is going wrong.

    A big mistake people tend to make when estimating time is that they only estimate things going right, not factoring in the time required for figuring out when things go wrong.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 3 years ago in reply to ntewinkel

    Agree. Often times testing means intentionally trying things that may cause problems to make sure they dont. I am a champion of breaking software at work, even when I'm not trying to. :-) 

    I anticipate that a product is fairly well tested before requesting a road test, unless it is clearly stated the product is an alpha or early beta release. 

    Most road tests seem to be Charlie releases, and that's why a supplier benefits from the experience diversity of the E14 community and some unique project ideas to try. Those unique ideas do take time to troubleshoot and blossom especially if they exercise functions that may not be tested well enough yet.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 3 years ago

    I did this Pi 4 Roadtest a few years back:  /products/roadtest/rv/roadtest_reviews/685/roadtest_the_raspber

    I can’t remember now but would guess it took at least 24 hours. 

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 3 years ago in reply to ntewinkel

    And even "oops I was tired and I transferred a 500mb file instead of a 1tb file, so that's why the numbers are off for the file transfer benchmark!" so you have to re-do the whole test again, for science.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to fmilburn

    The Pi4 was also a component in the Sound and Vibration Measurement Hat for Raspberry Pi.

    I didn't spend too much time reviewing the Pi, but it got used in anger while I focused on the DAQ hat. Using the Pi4 for the 1st time, with the Buster OS, was easy.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 3 years ago in reply to Jan Cumps

    What was total time for test, documentation,  and posting ? 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to robogary

    For that road test? A Lot. I'd say 80 hours at least. Most likely more.

    Not all of that time was efficiently used. Sometimes it was just fiddling around and see how things behaved. For the test gizmo I traveled to a makerspace and worked with balearicdynamics . 

    For the SCPI server and LabVIEW drivers and test flows, the hours are uncountable (and unaccounted for). Many of those hours were spent with shabaz  on chat. He was working on a MatLab integration.

    For the industry-relevant calculations and analytics, I worked with friend martinvalencia  from Peru, at (my) night. He taught me all the calculus, and what KPIs were critical for predictive maintenance in heavy industry (mining).

    I keep working on it (and blogging about it - although that goes unnoticed these days). Recently I tested a circuit (a good one !!) from michaelkellett on the road test kit. 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to Jan Cumps

    That was a great RoadTest, especially bouncing ideas off each other! It helped we are in the same approx timezone too. People can do a lot with such high-res data acquisition with Pi, it's a great combination.

    I've got a little list of features requests, waiting to submit them as soon as the site stability is there!

    One of them is that whenever anyone replies, they get a choice of 2 buttons: one will subscribe them (i.e. the button should be "Reply and Subscribe" which will subscribe to all notifications (i.e. edits to the blog and any replies) and the smaller button next to it should be "Reply" which will not affect the subscription/notifications). That way, those that want granular control as it is today, still have it, but everyone else can have the improvement. Similarly for Likes, when people click on it, there should immediately be a pop-up, to either confirm the like, or to confirm _and_ subscribe. It will slow down 'Likes' slightly, but I can't see that could be a problem, or there simply should be a another option, i.e. a "Like&Subscribe" button. Also, the site messaging remains the same, if the pop-up is in JavaScript or if there is a separate button and no pop-up.

    The latter could also encourage Likes because people will do that "Like&Subscribe' whenever they want to quickly be subscribed.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago in reply to ntewinkel

    How many wasted hours does the term "oops" cover? As in I took a job where the company folded after 6 months - oops Flushed 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 3 years ago in reply to dougw

    You sure are expensive :-)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<>