RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum ROADTEST POLL-- Which of These Boards Would You Likely Decide to Roadtest?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 2742 subscribers
  • Views 3468 views
  • Users 0 members are here
  • roadtest survey
Related

ROADTEST POLL-- Which of These Boards Would You Likely Decide to Roadtest?

rscasny
rscasny over 3 years ago

Here are a few more boards that I would like to get your feedback on whether element145 should offer them as roadtests. If you have a bit of time, I'd appreciate your vote.

seeed studiojetson nano

Seeed Studio Jetson Nano

Datasheet

cytron Maker Pi RP2040

Cytron Maker Pi RP2040

Datasheet

Avnet Maaxboard

AVNET Maaxboard

Datasheet

Arduino Nano Every

Arduino Nano Every

Datasheet

  • Sign in to reply
  • Cancel
Parents
  • ntewinkel
    ntewinkel over 3 years ago

    All of those are interesting choices.

    For me, the Maaxboard and the Nano Every are redundant - I have a Raspberry Pi, and I have several choices of boards that can (probably?) do for me what the Every does. So I'd be interested and happy to try them out, but not for the effort and commitment required for a proper RoadTest.

    The Cytron Maker is really cool, as it seems to have all the things I want for robot arms and robot cars - but I'm not familiar with Grove connectors as I have none of those, so I'm not sure if it would interface easily with my existing robot platforms (standard servo connectors, mainly).

    The Jetson Nano is also very interesting, and it looks like it would be a very nice replacement for a Raspberry Pi based server, given the 16GB eMMC, which for my tiny bits of data being collected should be plenty for a long while. My hesitation is whether it is compatible enough with Raspberry Pi to make those things easy - I'm guessing most likely the server parts can all install to whatever Linux system it uses in the same way as before, but can it run Python software that is intended for a Raspberry Pi ? (the sprinkler control software is very Pi biased). And the other "wish they included that" item is that the M.2 slot doesn't support SSDs. I'm not sure if that's important, given the eMMC?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ntewinkel
    ntewinkel over 3 years ago

    All of those are interesting choices.

    For me, the Maaxboard and the Nano Every are redundant - I have a Raspberry Pi, and I have several choices of boards that can (probably?) do for me what the Every does. So I'd be interested and happy to try them out, but not for the effort and commitment required for a proper RoadTest.

    The Cytron Maker is really cool, as it seems to have all the things I want for robot arms and robot cars - but I'm not familiar with Grove connectors as I have none of those, so I'm not sure if it would interface easily with my existing robot platforms (standard servo connectors, mainly).

    The Jetson Nano is also very interesting, and it looks like it would be a very nice replacement for a Raspberry Pi based server, given the 16GB eMMC, which for my tiny bits of data being collected should be plenty for a long while. My hesitation is whether it is compatible enough with Raspberry Pi to make those things easy - I'm guessing most likely the server parts can all install to whatever Linux system it uses in the same way as before, but can it run Python software that is intended for a Raspberry Pi ? (the sprinkler control software is very Pi biased). And the other "wish they included that" item is that the M.2 slot doesn't support SSDs. I'm not sure if that's important, given the eMMC?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mp2100
    mp2100 over 3 years ago in reply to ntewinkel

    It could definitely be used as a linux server. The os installation is debian based and can run python. It’s not a perfect RPi replacement for HATs, not all gpio pins work exactly the same as on the pi. You do get i2c and SPI though. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to ntewinkel

    The Jetson Nano's main USP is the processing cores that form its CUDA capability, ideal for things like AI or anywhere lots of data needs to be processed in parallel. As a Pi replacement it wouldn't be very good, since the CUDA cores would go unused. It's about the cheapest way to get that capability (many PCs may have graphics cards that support it too). Possibly the Maaxboard could be a closer fit to a Raspberry Pi (since the Pi is out of stock in a lot of places currently) but I've not looked at the Maaxboard details. 

    I like the Seeed cases they use... they fit both the Jetson Nano, and also the Raspberry Pi. I've been meaning to create a little LED strip for the Raspberry Pi enclosure, so that the LED flashes whenever there's a radio event (the Pi has a LoRaWAN card installed).

    image 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 3 years ago in reply to ntewinkel

    I'm rather curious to know why you think the Maaxboard is redundant. Personally, I quite like the NXP i.MX 8M Processor with Arm Cortex-A53 and the Cortex-M4F cores onboard. IMHO, this is nicely positioned for Industrial Edge devices. I believe this is same processor used in the Arduino Portenta X8, for example. At the moment I am pondering whether to get a Portenta X8 or go for the original Portenta H7. Still, one aspect to review is degree of flexibility you have with your Linux install (assuming you use something like yocto).

    The Nano Every is also a curious one and probably worth road testing, only to demonstrate if it still has value in it's target market. The form factor is liked, but the price makes it a hard sell compared to say Raspberry Pi Pico boards. Anyway there are not many SAMD11 M0+ processor boards around, so it may be a case of benchmarking against other similar M0 boards (e.g. RP2040).