RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum ROADTEST POLL: Would You Be Interesting in Roadtesting a Data Acquisition Learning Module?
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 40 replies
  • Subscribers 2559 subscribers
  • Views 5954 views
  • Users 0 members are here
  • roadtest survey
  • adalm2000
  • analog devices
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

ROADTEST POLL: Would You Be Interesting in Roadtesting a Data Acquisition Learning Module?

rscasny
rscasny over 2 years ago

adalm2000I'm planning a roadtest on this product. I'd like to gauge your interest in roadtesting it. 

Here's some information about the product:

ADALM2000 is an (M2K) active learning module is an affordable USB-powered data acquisition module that takes the capabilities of the ADALM1000 (M1K) active learning module to the next level. With 12bit ADCs and DACs running at 100MSPS, the ADALM2000 with the Scopy software, brings the power of high performance lab equipment to the palm of your hand, enabling electrical engineering students and hobbyists to explore signals and systems into the tens of MHz without the cost and bulk associated with traditional lab gear. The ADALM2000, when coupled with Analog Devices' ScopyTm graphical application software running on a computer, provides the user with the following high performance instrumentation.

Here are some of its features:

  • Provides access to real circuits and concepts used in an actual real-time engineering environment
  • Available online resources support educator, guide students to learn difficult engineering concepts
  • Hands-on activities stimulate interest and accelerate learning in fundamental engineering concepts
  • Helps to develop critical thinking skills needed for career development
  • 16-ch digital logic analyzer (3.3V CMOS and 1.8V or 5V tolerant, 100MS/s)
  • 16-ch pattern generator (3.3V CMOS, 100MS/s), 16-ch virtual digital I/O
  • 2 input/output digital trigger signals for linking multiple instruments (3.3V CMOS)
  • Digital bus analyzers (SPI, I²C, UART, parallel)
  • 2-ch oscilloscope with differential inputs, 2-ch arbitrary function generator, 2-ch voltmeter

Here are some docs:

Datasheet

Flyer

App Notes

Here's the poll question:

  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 2 years ago in reply to misaz +5
    Yes, there are a lot of tough choices to make when on a limited budget. You can use digilent's waveforms with a sound card to get an idea if this type of product would be useful. I have the OEM version…
  • anniel747
    anniel747 over 2 years ago +4
    Deleted
  • javagoza
    javagoza over 2 years ago in reply to anniel747 +4
    I agree, it would be great to be able to test ADALM2000 together with ADALP2000 . I have the ADALM1000 with the ADALP2000 and it's definitely a great kit to learn on.
  • misaz
    misaz over 2 years ago

    I have seen this device few weaks ago. Looks good for entry level device but it is quite a overpriced I think.

    ADALM family contains more devices. Look for exmaple at very interesting ADALM-PLUTO SDR which would be also nice device to RoadTest.

    • Cancel
    • Vote Up +2 Vote Down
    • Cancel
  • anniel747
    anniel747 over 2 years ago
    [deleted]
    • Cancel
    • Vote Up +4 Vote Down
    • Cancel
  • javagoza
    javagoza over 2 years ago in reply to anniel747

    I agree, it would be great to be able to test ADALM2000 together with ADALP2000. I have the ADALM1000 with the ADALP2000 and it's definitely a great kit to learn on.

    • Cancel
    • Vote Up +4 Vote Down
    • Cancel
  • shabaz
    shabaz over 2 years ago

    I bet this would be extremely popular! The ADALM1000 was a wonderful device but very version 1,0, but this newer ADALM2000 is supported a lot more with software and with educational material (complete training program!) as far as I'm aware. It is pretty much a lab-in-a-box, but surprisingly with enough performance and precision, within a voltage/current range, to do very detailed experiments, like really understanding semiconductors and various component networks, through to testing complete circuits with stimulus and measurements.

    • Cancel
    • Vote Up +2 Vote Down
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to misaz
    misaz said:
    but it is quite a overpriced I think

    That perhaps depends upon if you factor in all the training material they provide to go along with it.

    • Cancel
    • Vote Up +2 Vote Down
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to misaz

    Compared to the AD2, it looks reasonably priced to me

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to javagoza

    Yes definitely! 

    I tried an early predecessor of ADAPL2000 here:  Christmas Gift Ideas part 2 - Analog Kit 

    Very neat kit, I still use the predecessor version to experiment with (and I bought one for a family member too), and that is now a 9 years old kit! : ) The newer ADALP2000 looks much more comprehensive. It is basically a very large portfolio of AD components, but linked to an educational program too. I wish other manufacturers did the same.

    • Cancel
    • Vote Up +3 Vote Down
    • Cancel
  • dougw
    dougw over 2 years ago

    Very nice feature set, which of course means there are a lot of things to test in a road test.

    • Cancel
    • Vote Up +2 Vote Down
    • Cancel
  • tarna
    tarna over 2 years ago

    I would love to test something like this!

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • misaz
    misaz over 2 years ago in reply to scottiebabe

    Yes, but for 230 USD you can get low-end scopes with properly defined bandwidth, with display and without 3.3V logic restrictions. For example https://www.newark.com/multicomp-pro/mp720781-us/handheld-dso-40-mhz-250-msps/dp/25AK2940 or https://www.newark.com/multicomp-pro/mp720010-us/digital-storage-oscilloscope-50mhz/dp/10AH2393. Of couse it is not fully comparable becase ADALM have integrated logic analyzer and there are some other differences.

    I think ADALM2000 and Analog Discovery should be priced below these devices. 100 - 150 USD I consider good price for them.

    • Cancel
    • Vote Up +2 Vote Down
    • Cancel
>