RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum ROADTEST POLL: Would You Be Interested in Roadtesting an Open Source Single Board Computer?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 2742 subscribers
  • Views 4507 views
  • Users 0 members are here
  • roadtest survey
  • beaglebone play
Related

ROADTEST POLL: Would You Be Interested in Roadtesting an Open Source Single Board Computer?

rscasny
rscasny over 3 years ago

imageI have a couple of new BeagleBone SBCs that I'd like the community to roadtest.

This poll is to gauge the level of interest.

About the product:

BeaglePlay is an open-source single board computer designed to simplify the process of adding sensors, actuators, indicators, human interfaces, and connectivity to a reliable embedded system. It features a powerful 64-bit, quad-core processor and innovative connectivity options, including Wi-Fi, Gigabit Ethernet, sub-GHz wireless, and single-pair Ethernet with power-over-data-line. With compatibility with 1,000s of off-the-shelf add-ons and a customized Debian Linux image, BeaglePlay makes expansion and customization easy. It also includes ribbon-cable connections for cameras and touch-screen displays, and a socket for a battery-backed real-time-clock, making it ideal for human-machine interface designs. With its competitive price and user-friendly design, BeaglePlay provides a positive development experience for users.

Features

  • Multicore A53s with R5, M4s and PRUs processor, TI AM6254
  • WiFi/2.4G, MIMO/5G, SISO M2 1216, TI WL1807 Wi-Fi module, U.FL x2
  • TI BLE/SubG CC1352P7 M4+M0 with BeagleConnect firmware
  • 2GB(1Gb x 16)-1600MHz 3200Mbps DDR
  • Kingston 16GB eMMC
  • Gigabit Ethernet with RJ45 x1, single pair Ethernet and power over with RJ11
  • Power input with USB Type-C
  • HDMI Type-A supports up to Full-HD/1080P with 24-bit RGB
  • Support FPC 22pin CSI and FPC 40pin OLDI
  • 1x MikroBus connector, 1x USB Type-A, 1x micro SD socket, 1x QWIIC, 1x grove connector, 1x RTC

Documentation

Datasheet 
Getting Started 
For More Information

Polls

  • Sign in to reply
  • Cancel
Parents
  • mp2100
    mp2100 over 3 years ago

    I think this BB-P looks like an SBC with very interesting features.  I would like to test it, but when I look at the documentation available so far, it made me vote maybe.  The information is sparse.  I have tried almost all of the Beagles, but this reminds me of the BB-AI roadtest where many struggled to get progress  ( and to be sure, the clever people here achieved  results that got us an amazing amount of information from their hard work ) 

    At the top of my list for this board is trying the SPE - single pair ethernet, but I don't know any other devices that also use SPE.  I will have to search around.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mp2100
    mp2100 over 3 years ago

    I think this BB-P looks like an SBC with very interesting features.  I would like to test it, but when I look at the documentation available so far, it made me vote maybe.  The information is sparse.  I have tried almost all of the Beagles, but this reminds me of the BB-AI roadtest where many struggled to get progress  ( and to be sure, the clever people here achieved  results that got us an amazing amount of information from their hard work ) 

    At the top of my list for this board is trying the SPE - single pair ethernet, but I don't know any other devices that also use SPE.  I will have to search around.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Fred27
    Fred27 over 3 years ago in reply to mp2100

    I've been searching and I don't think you can buy any SPE devices - apart from a few impractically expensive specialist bits of kit. Also, it doesn't seem that RJ11 is a standard connector for SPE so it would also probably involve making up your own cables.

    I'd also like to play with SPE, but I don't think it's practical as part of a road test - unless it's between 2 BeaglePlays.