RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum When Is A RoadTest Review Too Much or Too Little?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 2752 subscribers
  • Views 4213 views
  • Users 0 members are here
  • roadtest reviews
  • writing a roadtest review
  • too much or too little
Related

When Is A RoadTest Review Too Much or Too Little?

rscasny
rscasny over 3 years ago

I have been spending more time reading (including proofreading) roadtest reviews. Some of our suppliers are reading your reviews and providing me feedback on them as well. One of the main reasons why a sponsor participates in the RoadTest program is to get feedback about the product, documentation, design tools, and so on. So, your reviews could be read by a variety of stakeholders within the sponsor's organization (engineers, business managers, marketing, etc.). Your reviews are highly visible. (So, make sure you do a spell check before you publish them, please!) While I have always said you don't be a superior writer to be a roadtester, roadtesters should try to spot basic errors and correct them. If you need help, please contact me.

One thing I have noticed recently as I read reviews is that some reviews cover a lot of things. Some have indexes to separate blogs that function as tutorials. I have also noticed that some are fairly short and don't "tell the story behind the review" visually to make a reader think "Wow" this is cool, incredible, etc."

So, when is a review too much or too little?

I do not desire to establish stringent max-word-count guidelines. I never will. After I choose you as an official roadtester, I need you to "take ownership" of the roadtest. I fully understand that people will write reviews differently. In fact, that is something I ponder when I go through the roadtest applications. I want to obtain different kinds of reviews, which in my mind represents different kinds of engineering minds and, yes, different kinds of customers.

But back to my core question: When is a review too much or too little?

There are some experienced roadtest reviews who can juggle gads and gobs of information and, like a conductor at a symphony, produce a multi-faceted, "perfect" review. These are great productions.

But there are also some reviewers who can easily perform the testing but when one reads the review it doesn't flow so smoothly and makes it a bit harder to read.

I personally think: don't forget the basics.

A review should (a) explain what you are going to do and why, (b) provide a background on the product because not all readers will be familiar with it, (c) conduct and describe the results of your tests (this can include an unboxing), (d) go through how you experienced the product and (e) draw some conclusions.

For some roadtesters, too much is when there are side information that bogs down the basics, so they never get to the basics. But for other roadtesters, they can add the side information to explain things that perhaps are not explicitly stated in the sponsor's documentation; these are skilled roadtesters. 

When is a roadtest review too little? The comments are a guide. If our members ask the roadtester a lot of questions, then maybe your review lacks something.

People learn a lot visually. Take a cartesian grid. One can learn more from a graph of a sensor temperature vs Time than just a table of temp data. When a review has no visuals that support what is being stated in the text of your narrative, it is probably too little. Finally, a just-the-right-length review is persuasive. Read the comments of a bunch of reviews. When you see comments like "nice review," you know you have hit a homerun.

Thank you for your time.

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • genebren
    genebren over 3 years ago

    As always, the devil is in the details.  Not enough information - then no value added.  Too much information - it will be really difficult to absorb or process the data.

    An example of a great review (not a roadtest), was a recent review written by shabaz ,  Working with the Renesas RA4M1 Microcontroller .  This was very concise and it did a great walk through of a new processor, working up to a real practical example.  This would have been a great roadtest review, given the value of the evaluation board.  It might have been a little shy of a worthy roadtest review of a $4000 Oscilloscope.

    I think the value of the product sets the scope for the appropriate amount of content that needs to be in the review.  The more features, the more content.  That being said, I really like a problem or project specific type of a review (like shabaz's example above), as this really drives home how easy or difficult it might be to use this device.  Also, a good summary, with pros and cons is a really valuable addition to a review.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to genebren

    Hi Gene,

    Thanks for the RA4M1 feedback! Incidentally that content was going to be even shorter: the content contains information on several peripherals, and I was going to publish that, but it felt incomplete without one more peripheral, namely USB. So from my perspective, it would have been a review that was too short without that peripheral.

    I figured that USB Serial was essential for usability/config/troubleshooting, and readers might feel cheated if it wasn't there, so I didn't publish it until I had tested USB and written that up too. That's why USB is the last example peripheral in that blog post, simply because it was written last. It read fine as the last peripheral example, so I didn't rearrange the text.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago in reply to genebren

    Hi Gene,

    Thanks for the RA4M1 feedback! Incidentally that content was going to be even shorter: the content contains information on several peripherals, and I was going to publish that, but it felt incomplete without one more peripheral, namely USB. So from my perspective, it would have been a review that was too short without that peripheral.

    I figured that USB Serial was essential for usability/config/troubleshooting, and readers might feel cheated if it wasn't there, so I didn't publish it until I had tested USB and written that up too. That's why USB is the last example peripheral in that blog post, simply because it was written last. It read fine as the last peripheral example, so I didn't rearrange the text.