RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum How You Would RoadTest a Power Entry Device with Wi-Fi/Bluetooth Connectivity to Report on Energy Consumption
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 2748 subscribers
  • Views 5970 views
  • Users 0 members are here
  • roadtest survey
Related

How You Would RoadTest a Power Entry Device with Wi-Fi/Bluetooth Connectivity to Report on Energy Consumption

rscasny
rscasny over 3 years ago

imageI am planning on roadtesting this product in the near future. It's a simple device, but with WiFi and Bluetooth connectivity and an energy consumption sensor, the product stands out from others.

I primarily wanted to get some ideas on how you would roadtest it. Do you only need the product or is there anything else that should be included in the kit?

Let me give you a few basic facts about the product:

  • The product can be operated with the following load: 85-305VAC @47-63Hz.

  • Standalone device with WiFi and Bluetooth connectivity

  • Measurement of energy data and integrated relay switch to generate additional value on the power input

  • Easy integration of smart IoT functionality into existing devices

  • Connected to the Internet via WiFi 802.11b/g/n and has an integrated energy meter senso

  • Data analysis and processing via SCHURTER Dashboard or SCHURTER App

  • Relay switchable via WiFi (Cloud)

  • Integrated energy live measurement with update rate up to 60 sec.

  • Low standby Energy consumption (<0.5W)

Here are links to the documentation for you to review:

Datasheet 
Web Page 
White Paper 

While I am interested to see how you would set up the product for a product, I have been hashing out some ideas with others. These ideas include:

1. Power a load via the DT31
2. Verify Energy Measurement
3. Ease of use of the Phone App
4. Identify use cases for devices and measurements.

imageHow would you test this unit? I'd appreciate your thoughts in the comments below.

Prospective RoadTester Polls





  • Sign in to reply
  • Cancel
Parents
  • charlieo21
    charlieo21 over 3 years ago

    I think that in order to test this an interlock cable would be needed. Also, if the software side, API, is intended to be tested a subscription for a pair of months would be needed as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • charlieo21
    charlieo21 over 3 years ago

    I think that in order to test this an interlock cable would be needed. Also, if the software side, API, is intended to be tested a subscription for a pair of months would be needed as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to charlieo21

    If your load currently has a "IEC 60320-1" style connector, you can just plug this unit in your device, and the existing power cord into this unit. It sits in-between.