RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum How You Would RoadTest a Power Entry Device with Wi-Fi/Bluetooth Connectivity to Report on Energy Consumption
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 2748 subscribers
  • Views 5975 views
  • Users 0 members are here
  • roadtest survey
Related

How You Would RoadTest a Power Entry Device with Wi-Fi/Bluetooth Connectivity to Report on Energy Consumption

rscasny
rscasny over 3 years ago

imageI am planning on roadtesting this product in the near future. It's a simple device, but with WiFi and Bluetooth connectivity and an energy consumption sensor, the product stands out from others.

I primarily wanted to get some ideas on how you would roadtest it. Do you only need the product or is there anything else that should be included in the kit?

Let me give you a few basic facts about the product:

  • The product can be operated with the following load: 85-305VAC @47-63Hz.

  • Standalone device with WiFi and Bluetooth connectivity

  • Measurement of energy data and integrated relay switch to generate additional value on the power input

  • Easy integration of smart IoT functionality into existing devices

  • Connected to the Internet via WiFi 802.11b/g/n and has an integrated energy meter senso

  • Data analysis and processing via SCHURTER Dashboard or SCHURTER App

  • Relay switchable via WiFi (Cloud)

  • Integrated energy live measurement with update rate up to 60 sec.

  • Low standby Energy consumption (<0.5W)

Here are links to the documentation for you to review:

Datasheet 
Web Page 
White Paper 

While I am interested to see how you would set up the product for a product, I have been hashing out some ideas with others. These ideas include:

1. Power a load via the DT31
2. Verify Energy Measurement
3. Ease of use of the Phone App
4. Identify use cases for devices and measurements.

imageHow would you test this unit? I'd appreciate your thoughts in the comments below.

Prospective RoadTester Polls





  • Sign in to reply
  • Cancel
Parents
  • Gough Lui
    Gough Lui over 3 years ago

    I'd certainly look at the security of the device - how is it provisioned, how does it speak to the cloud, how does the API work, is there any local access?

    I'd also look at the functionality in terms of whether it memorises state on power outage - as I can see this being a box targeted at remotely power cycling a computer/IT equipment/rack in case of trouble.

    It would be interesting to verify accuracy of energy measurement - a resistive load, variac and power analyser could do the job for a ~PF 1.0 load, but distorting loads could be interesting as well, using a phase-angle control dimmer (leading/trailing edge).

    I don't think a load test is entirely necessary - it's probably got a relay inside rated at the right rating for the job. But if one wishes to cycle it to check for welding of contacts due to inrush, the results are likely very dependent on the load.

    Instead, I'd rather check it for operating power consumption - this is something that's going to be switched on 24/7 and contributing to the power bill, so understanding its consumption would help you avoid silly ideas (i.e. plugging a mobile charger into one, as its standby consumption would be less).

    The outlet IEC C13 (plug) is no big issue - if you're like me, you'd probably lop it off and wire in a mains socket for a bit more versatility. For those who don't want the trouble, commercially available C14 (socket) adapter cables are available especially as some UPSes use the same scheme - e.g.

    • for the UK: https://au.element14.com/pro-elec/pel01253/power-cord-iec-60320-c14-mains/dp/3052547
    • for the US: https://au.element14.com/tripp-lite/p002-001-10a/power-cord-iec-c14-nema-5-15r/dp/2578461
    • for the EU (via third party): https://www.amazon.com/Eonvic-IEC-C14-Europe-adapter/dp/B015T1LM92
    • for AU (via third party): https://www.lindy.com.au/150mm-power-cable-10a-iec-c14-plug-to-3-pin-socket

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gough Lui
    Gough Lui over 3 years ago

    I'd certainly look at the security of the device - how is it provisioned, how does it speak to the cloud, how does the API work, is there any local access?

    I'd also look at the functionality in terms of whether it memorises state on power outage - as I can see this being a box targeted at remotely power cycling a computer/IT equipment/rack in case of trouble.

    It would be interesting to verify accuracy of energy measurement - a resistive load, variac and power analyser could do the job for a ~PF 1.0 load, but distorting loads could be interesting as well, using a phase-angle control dimmer (leading/trailing edge).

    I don't think a load test is entirely necessary - it's probably got a relay inside rated at the right rating for the job. But if one wishes to cycle it to check for welding of contacts due to inrush, the results are likely very dependent on the load.

    Instead, I'd rather check it for operating power consumption - this is something that's going to be switched on 24/7 and contributing to the power bill, so understanding its consumption would help you avoid silly ideas (i.e. plugging a mobile charger into one, as its standby consumption would be less).

    The outlet IEC C13 (plug) is no big issue - if you're like me, you'd probably lop it off and wire in a mains socket for a bit more versatility. For those who don't want the trouble, commercially available C14 (socket) adapter cables are available especially as some UPSes use the same scheme - e.g.

    • for the UK: https://au.element14.com/pro-elec/pel01253/power-cord-iec-60320-c14-mains/dp/3052547
    • for the US: https://au.element14.com/tripp-lite/p002-001-10a/power-cord-iec-c14-nema-5-15r/dp/2578461
    • for the EU (via third party): https://www.amazon.com/Eonvic-IEC-C14-Europe-adapter/dp/B015T1LM92
    • for AU (via third party): https://www.lindy.com.au/150mm-power-cable-10a-iec-c14-plug-to-3-pin-socket

    - Gough