RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum How You Would RoadTest a Power Entry Device with Wi-Fi/Bluetooth Connectivity to Report on Energy Consumption
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 2748 subscribers
  • Views 5953 views
  • Users 0 members are here
  • roadtest survey
Related

How You Would RoadTest a Power Entry Device with Wi-Fi/Bluetooth Connectivity to Report on Energy Consumption

rscasny
rscasny over 3 years ago

imageI am planning on roadtesting this product in the near future. It's a simple device, but with WiFi and Bluetooth connectivity and an energy consumption sensor, the product stands out from others.

I primarily wanted to get some ideas on how you would roadtest it. Do you only need the product or is there anything else that should be included in the kit?

Let me give you a few basic facts about the product:

  • The product can be operated with the following load: 85-305VAC @47-63Hz.

  • Standalone device with WiFi and Bluetooth connectivity

  • Measurement of energy data and integrated relay switch to generate additional value on the power input

  • Easy integration of smart IoT functionality into existing devices

  • Connected to the Internet via WiFi 802.11b/g/n and has an integrated energy meter senso

  • Data analysis and processing via SCHURTER Dashboard or SCHURTER App

  • Relay switchable via WiFi (Cloud)

  • Integrated energy live measurement with update rate up to 60 sec.

  • Low standby Energy consumption (<0.5W)

Here are links to the documentation for you to review:

Datasheet 
Web Page 
White Paper 

While I am interested to see how you would set up the product for a product, I have been hashing out some ideas with others. These ideas include:

1. Power a load via the DT31
2. Verify Energy Measurement
3. Ease of use of the Phone App
4. Identify use cases for devices and measurements.

imageHow would you test this unit? I'd appreciate your thoughts in the comments below.

Prospective RoadTester Polls





  • Sign in to reply
  • Cancel
Parents
  • kmikemoo
    kmikemoo over 3 years ago

    240v, 50Hz. Frowning2  That rules me out.  To demonstrate the operation, I'd put it on the Keurig.  That little beast cycles on and off during normal business hours - just in case we need caffine.  "Just in case..."  Who am I kidding?  WHEN we need caffine.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to kmikemoo

    Hi Mike,

    I'm not sure, but I think it's likely a webpage mistake, because the "250V 10A" text may just mean the relay and the IEC cable rating, because there's nowhere in Europe that has such a voltage system either (nominal is 230V, not 250V). The 50 Hz doesn't make any sense alongside that. Or they might have meant 10A/230V 50Hz. Either way there's a mistake, but I don't know which they meant.

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago in reply to kmikemoo

    Hi Mike,

    I'm not sure, but I think it's likely a webpage mistake, because the "250V 10A" text may just mean the relay and the IEC cable rating, because there's nowhere in Europe that has such a voltage system either (nominal is 230V, not 250V). The 50 Hz doesn't make any sense alongside that. Or they might have meant 10A/230V 50Hz. Either way there's a mistake, but I don't know which they meant.

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rscasny
    rscasny over 3 years ago in reply to shabaz

    Schurter just told me this: 

    The product can be operated with the following load: 85-305VAC @47-63Hz.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 3 years ago in reply to shabaz

    Hi shabaz .  I wondered if that might not be the case - Marketing working with the data they had.  But I also wondered if they sensing electronics might not be frequency specific (timing circuits, et al).  Another interesting thought would be to power it from a generator and see how it likes imperfect frequency.  It wouldn't be the first time I ran a generator just to make coffee. Laughing

    • Cancel
    • Vote Up +3 Vote Down