RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Would You Be Interested in Roadtesting a Current Mode Control DC/DC converter with Fast Transient Response?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 2748 subscribers
  • Views 3162 views
  • Users 0 members are here
  • roadtest survey
  • rohm
  • BD9G500EFJ-EVK-001
Related

Would You Be Interested in Roadtesting a Current Mode Control DC/DC converter with Fast Transient Response?

rscasny
rscasny over 3 years ago

imageI will be roadtesting this product in September. I'd like to get your feeedback, thoughts and interest in this product.

Here are a few facts about the product:

The BD9G500EFJ-EVK-001 uses BD9G500EFJ-LA to output 5V from a 48V input voltage. The input voltage of the BD9G500EFJ-LA is from 7V to 76V and the output voltage is configurable from 1V to 0.97 x VIN V with external resistors. The operating frequency is configurable between 100 kHz and 650 kHz with an external resistor connected to RT pin. This is a current mode control DC/DC converter that provides fast transient response performance and simple phase compensation setup.

Here are a few features of the DC/DC Converter:

  • Wide Input Voltage Range
  • Integrated High-Side MOSFET
  • Current Mode Control
  • Adjustable Frequency
  • Soft Start Function
  • Over Current Protection (OCP)
  • Under Voltage Lockout (UVLO)
  • Thermal Shutdown Protection (TSD)
  • Over Voltage Protection (OVP)
  • HTSOP-J8 package

Here are some documents from the manufacturer:

Datasheet: 

User Guide: 

Manufacturer's Page: 

For More Information

Roadtester Polls


I am considering adding an adjustable DC Power Supply to the kit, Bench Power Supply




  • Sign in to reply
  • Cancel
Parents
  • dang74
    dang74 over 3 years ago

    I was thinking of using a switching regualtor to serve as a poor man's substitute for a bench top power supply.  The wide operating range of this product in terms of both input and output voltages sounds pretty promising.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • anniel747
    anniel747 over 3 years ago in reply to dang74
    This reply was deleted.
    • Cancel
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to anniel747

    It's a power electronics design. Also goes to several amps. May get hot. It's part of the trade.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to anniel747

    which one?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • anniel747
    anniel747 over 3 years ago in reply to Jan Cumps
    This reply was deleted.
    • Cancel
    • Cancel
Reply
  • anniel747
    anniel747 over 3 years ago in reply to Jan Cumps
    This reply was deleted.
    • Cancel
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to anniel747

    which one?